We’re Giving away 10 Intel Genuino 101 Dev Boards - Review

View table of contents ...  

RoadTest: We’re Giving away 10 Intel Genuino 101 Dev Boards

Author: jdlui

Creation date:

Evaluation Type: Independent Products

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: Arduino Uno

What were the biggest problems encountered?: Some issues with library installs, even triggering anti-virus. Due in part to the several 3rd part software that are usually suggested to start running demos with this unit.

Detailed Review:

Hi folks,

I completed a review of the Intel Genuino 101 as part of the element14 roadtest. My apologies that this review is coming late, the device unfortunately arrived at a pretty tough time (November) in my master's degree studies and Christmas holidays.

 

I am reviewing this from the perspective of someone who is fairly amateur in electronics and microcontrollers. I just got started with Arduino back in 2015 when I completed my first element14 review. At that point, I didn't even know how to program a microcontroller or hook electronics up to it. During this review and in some small subsequent projects, I learned how to work with these boards a little better.

 

Enter the Intel Genuino 101 board. This is a lovely little board, which is very similar to the Arduino Uno in many ways. However, it is very notably different in several key ways, including introduction of Bluetooth BLE and a 6 axis accelerometer/gyroscope. Also different, this device operates on 3.3V but is tolerant on 5V, which is something very convenient if you're finding yourself stuck between the two scenarios.

 

First Impressions

Here is the Genuino in all its newfangled glory. It arrives crisp and clean, just like the Arduino Uno and Yun did.

image

 

Notably missing when you open the box is the lovely stickers that came with the Arduino Uno model. It's rather insignificant but it always brought a bit of extra joy to opening these guys.

image

 

Let's take a look at the board itself! Honestly my first impressions on the layout were somewhat disappointing. Things I noticed:

  • Header pins on the digital side do not line up well. This could be a concern if your stacking shields onto this thing. This is slightly noticeable on the analog pin header side as well, but not as bad.

image

Here is another shot of the header alignment being off.

image

On the bottom side, I see a lot of leftover gunk on this board. I assume that most of these is not super hazardous material, but the board arrives quite frankly filthy.

image

Some more shots of the gunky board. Not sure what it is, leftover flux material? I never thought I'd be so pick with this (especially since I received the board for a review), but I think my hang-up with the cleanliness of these electronics is that they're now being marketed and popularized to younger and younger generations as they get into the maker space. If this is something we encourage, we should ensure a standard on cleanliness and manufacturing so we know contaminates are being left on the boards.

image

 

 

Setup

Setting up the Genuino 101 was generally pretty straight forward, even for a newbie like me. I've documented some of the steps below. The setup for the Genuino 101 requires installing some libraries, and was well documented by in his setup.

 

Step 1: Go into Arduino IDE, and select Board Manager.

 

image

 

Next step: Install Intel Curie Boards package.

image

 

Next up, your machine prompts you to allow installation of your hardware.

image

image

After this, you should see this as a proper device in Device Manager and as a Board entry in Arduino IDE. Looks like we're good to go!

image

 

First steps

Firsts steps with this board are not too difficult because there is already a decent amount of tutorial documentation out there for this board. For a great first demo, I followed the orientation visualizer tutorial. This demo uses the data from the onboard accelerometer and gyroscope and performs some math (Madgwick filter algorithm, which was developed by Sebastian Madgwick during his PhD in 2010) to integrate this data and obtain quarternions which can represent the orientation of an object in free space. This is a pretty big deal mathematically because this is usually fairly hard to compute quickly and efficiently. With this algorithm, we can take velocity and acceleration data and integrate to obtain position data and represent this in real time. The tutorial makes it pretty easy for anyone to get started. You basically load up their Arduino script, ensure you install and include the Madgwick library, and then run some additional code in an open source software called Processing so that you can see the orientation data in real time.

 

The result is shown below in pictures.

 

image

 

image

 

I've also demonstrated the orientation visualizer in action in a video here. Note what I mention in the video is a drift in yaw orientation data. This is something that is generally unavoidable, because we are integrating acceleration data to obtain position and orientation data. The result is that when the device is in motion we really get more accurate readings. But if we keep the device essentially stationary, the double integration from acceleration to position will take the smallest noise measurements and misconstrue this into actual movement data, hence why my device is rotating in yaw axis over time. This error in integration accumulates overtime when we do dead reckoning using gyroscope.

 

 

I think this is amazing that we can so quickly get orientation visualization running on this device. This is a definite boon over something the Arduino Uno, even though it should not be so daunting to buy and connect 4 wires to an IMU to get some accelerometer and gyro data. The fact the IMU is built into the Genuino 101 enforces consistency and hence allows great example code and libraries to be put in our hands, allowing very quick learning. This makes this device a great candidate for someone who is new to microcontrollers, but quickly wants to use an Arduino type MCU for a robotics, wearables, or fashion project. No need for time to be wasted learning about, researching, and integrating an IMU if you have a school project or something to worry about. This is actually very similar to how I applied the Genuino 101 in my research, because I needed to quickly test out an IMU hypothesis for a medical device prototype I was designing, but didn't want to worry about buying an IMU and testing it out.

 

Other tests

Tried out a few other Arduino standard tutorials for Genuino, including the tap detector. These tutorials are great because they can really help you see into the insight of the code and also start generating ideas on how to use the Genuino 101 board. Maybe you could use it to detect if someone is knocking on your door? Or track if someone is mishandling your package using tap count or shock detection?

 

The step counter tutorial was also excellent because it could again help a novice user (like me) to very quickly get the footing required to design, test, and prototype a custom wearable device. I didn't end up needing step counting for my Master's thesis work so I didn't delve into this script in detail. It looks like the step detection is probably triggered by a movement exceeding a threshold g force and this could be configured by using a command like the below.

 

CurieIMU.setDetectionThreshold(CURIE_IMU_SHOCK, 1500);

image

 

Trying to integrate this into my research

I'm completing a master's of engineering and wanted to try integrating this into some of my hardware prototyping in place of the standard Arduino Uno. The Genuino 101 functions like the Uno in most respects but I ran into some isues when trying to run some Arduino code I built to take readings from the Omron pyroelectric sensors.

 

Omron

 

Because of the sensors create so much data, the standard Wire.h buffer is apparently not big enough for reading the sensor data via I2C, so some people have taken the approach of using a custom version library called WireExt.h. However when I tried to compile my script that contained WireExt.h, the compile would crash because it was trying to include avr/io.h but it couldn't find anything. I guess this is because Genuino 101 is Intel Curie and ARC based instead of Atmel and AVR based. I didn't really have the intuition and know where to search for a solution, but I bet if I posted in the Arduino forums, someone would likely have a pretty easy work-around that I could attempt. That said, this was where I hit a roadblock in using the Genuino, and had to put it away for the time being and switch back to Arduino for my project.

 

image

 

Conclusion

Overall the Genuino 101 is a delightful little board with several features that make it pack a real punch. For most people I think it's an amazing starter board to pick out and would enable several more projects than the Arduino Uno can offer out of the box. The new focus on maker culture and general plethora of good Genuino 101 tutorials allow you to really run before you walk. That said, there is still some places where the standard Arduino Uno still holds dear to my heart.

 

So is this an Arduino Uno replacement? To some, yes it can be. Personally, I'm divided. The Uno still holds a very useful niche. However when the Genuino 101 basically retails for the same price as the Arduino Uno now, I think it's a no-brainer on which one you should select!

 

Thanks for reading!

Jordan

 

Evaluation

Application used in:

Attempted integration into biomedical graduate research and basic Arduino tutorial completion.

Was everything in box? Yes

Comparable products: Arduino Uno

Product performed to expectations:     10

Specifications were sufficient:     10

Demo software was good quality     10

Demo was easy to use     10

Support material available     10

Price to performance was good     10

Total score     60/60

 

My caveat is that hardware quality is not really in this rating criteria at all. I considered the build quality to look very poor and as a result I really would wonder about the manufacturing standards and long term durability of this hardware.

 

Biggest problems:  Some issues with library and file installs, and one of the tutorials was hard to follow and even triggered my anti-virus. Maybe a long term version of the Genuino will come with a larger software suite so we aren't installing as many random 3rd party pieces of software.

Anonymous
  • Randall,

    Thank you for the kind words and excellent feedback.

    I'd like to say a big thank you to the element14 community for the learning that I have gained in this community. I still remember when introduced me to element14 in November 2014. I didn't even know what an Arduino or a trim pot was. This community has truly connected me to many amazingly talented individuals and really accelerated my learning in the area of electronics and micro controllers. image

     

    Cheers,

    Jordan

  • Jordan,

     

    Thanks for a fine review (and reposting it to the official review form).

     

    Your approach to the review can be a model for other new reviewers. You start out with an overview, and unboxing, giving the reader more detail as you go. Then you enter into the experiments phase of your review. And you wrap up the review with the "insights" section. I like the section on how you were trying to integrate it into your research. While perhaps not complete (RoadTests will never be) you give some nuggests of information that can help people along to some degree.

     

    In summary for other roadtesters, his review was broken into:

     

    • Overview (unboxing Set up, etc)
    • Experiments
    • Insights

     

    This three phase approach is simple, streamlined and effective. An approach worth emulating.

     

    Randall

  • I suspect the gunk is flux that has remained after an attempt to clean it.

    One issue with residual flux like that is that it can absorb moisture and then cause issues.

     

    If you don't have access to commercial products, an old toothbrush and either methylated spirits or isopropohol alcohol will remove it.

     

    The modern libraries seem to always call various other bits of code.

    In this case the AVR/io is being called in the accompanying part of the library.

    http://fenrir.naruoka.org/download/autopilot/external/camera_breakout/arduino_library/WireExt/WireExt.cpp

     

    You could try commenting it out on your library.

     

     

    Mark

  • DAB,

    I'll contact the vendor directly and see what they think. Good point - someone would like to hear about these things.

     

    I'm still not quite sure about the workaround for my issue with the lack of support for the custom wireext.h library.

     

    I had a slightly different but related issue where reading too many of these sensors was maxing out the allowed size of a JSON object buffer, which I was writing to before I transmitted the data out from Arduino via Bluetooth. In that case, I stored data to a variable before emptying the buffer and continuing. I wonder if this type of approach would allow me to devise some sort of fix.

     

    In summary - I have more questions than answers on the sensor issue.  Hoping I can find a rainy Sunday to look at this in depth image

     

    Jordan

  • Nice review.

     

    I agree, no vender should send out a board that looks like that with the gunk still on it.

     

    Did you contact the vender about the board to see if they had any comment?  I have helped other manufacturers track down quality issues like this and they were very receptive.

     

    Did you ever resolve the IR sensor data rate issue?

     

    I wonder if there is a command you could have sent that would slow the data output.

     

    DAB