RoadTest: Tiva C Series TM4C1294 Connected LaunchPad
Author: refaqtor
Creation date:
Evaluation Type: Independent Products
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?:
What were the biggest problems encountered?:
Detailed Review:
This Texas Instruments Launchpad has proven as easy to get going on, especially considering the myriad of features including internet connection configuration. Conveniently, all the jumpers were set correctly by default to power up with the included USB cable. The "out of box" demo proceeded without a hitch according to the information sheet included in the box. I particularly appreciate the color-coded header pin function map also seen here: Energia Reference - Stellaris LaunchPad. While the web site suggested in the informational sheet brings you directly to the technical datasheets and documentation, I found this workshop site very informative : Creating IoT Solutions with the TM4C1294XL Connected LaunchPad Workshop - Texas Instruments Wiki . This site : Tiva C Series Connected LaunchPad (EK-TM4C1294XL) also had more information on other resources in their ecosystem. Of particular note is that Energia is supporting an increasing number of TI Launchpads, including this one : Energia Reference - Introduction. Arduino users will find Energia comforting and familiar.
Exosite Demo Site
Following the demonstration sheet in the box got me set up quickly and logging data to the website, as you see here-- very easy. Exosite limits the number of devices you can connect for free, but it is quite easily configurable may well be worth it for your application.
TivaWare - C Code Composer Resources
From the TI links noted above (and in the box) you can download Code Composer, TI's very nice free development environment based on Eclipse. You will also download TivaWare-C resource package, as you can see in the Resource Explorer of Code Composer, where you'll find the "qs_iot" pre-loaded demo example code.
Texas Instruments Code Composer
Code Composer is a capable IDE that makes it easy to find example resources and documentation. Connectivity to devices has always been painless, and a dynamite debugger makes it easy to step through code and really see how things work.
Tiva - C PinMux
Note: the part on this Tiva-C Launchpad is TM4C129x and the particular part is TM4C129NCPDT. The part number is on the chip itself, but I find that difficult to read if the paint label gets rubbed off.
There are many more peripherals in a Tiva than can be simultaneously enabled or accessed through the external pins. The permutations are myriad, as is the potential for conflicts. TI makes a tool to help you successfully configure the peripherals by giving you a useful graphical user interface that provides alerts to conflicts. It will also generate the appropriate code based on your selections to past into your own code. Tiva™ C Series MCUs PinMux Utility - TM4C_PINMUX - TI Software Folder
Tiva PinMux Produced Initialization Code
Here is an example of the code generated by the Tiva PinMux utility - simple, but voluminous. I enjoy knowing that, at least, all the initialization and port configuration is handled properly.
Energia (Arduino clone) interface for the Tiva-C launchpad
Finally, for those who just want to bang something out quickly there is really convenient access through Energia.
In conclusion, if you need to get something connected to the internet quickly, there is plenty of easy potential in the Tiva-C Launchpad, at a good price.
Top Comments
Yes you absolutely can, I have been for a little while now but it is limited as to how much of the hardware you can leverage with it as the hardware abstraction is permitting all the basic "Arduino" and…
-
mcb1
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Comment-
mcb1
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Children