TI C2000 InstaSPIN™-FOC LaunchPad w/ Motor Driver - Review

Table of contents

RoadTest: TI C2000 InstaSPIN™-FOC LaunchPad w/ Motor Driver

Author: Anonymous-237891

Creation date:

Evaluation Type: Evaluation Boards

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?:

What were the biggest problems encountered?: Nothing yet apart finding a suitable motor. The example code for the Piccolo board was just fine, but it is missing examples for the expansion board. Sad.

Detailed Review:

Unpacking and first impressions


My package arrived a bit late, I hope I won't be banished from road test just because of some delay in shipment.

Anyway I was super happy to crack the thing open, but I got disappointed when I realized this kit doesn't include a blcd motor.

I'm not involved in quadcopter making and this sort of things so I don't have any of those laying around.


The box came with everything need to get started (apart from the motor image) but the usb came with it so, I'll call it a "nice touch".



image


Installing the software


The software needed to code the board is all free and UNLIMITED that's really nice from ti (big thumbs up).

The two software need are:

CCS(code composer studio): http://processors.wiki.ti.com/index.php/Download_CCS

ControlSuite: controlSUITE - CONTROLSUITE - TI Software Folder


After install CCS should look like that

image

And ControlSuite like this

image

The drivers (thanks god) got installed with CCS but to make sure they work as intended, I just double check my computer/manage/devices.

image

(Yes sorry my Windows is configured in French)



Playing with the demo application


As explained in the quick start guide (http://www.ti.com/lit/ml/sprz413/sprz413.pdf) you can run the two demo allready programmed on the board.

The first is the very mainstream blinky led application. But the second one is much more fun to play with, it does measure the internal temperature of the chip and the send it over serial.

To do this they recommend using Putty (PuTTY Download Page) wich i did. (with the following settings)

image

And then You get the temp on a terminal (nothing fancy but still rewarding)

image

The board also show you on 8 bit the delta temp measured with the starting temp of the microcontroller. Sorry for the blur on the picture my camera doesn't like those LED that much.

image

 

Here I am again...

I haven't make anything turn yet but I am not giving up with this, I will someday.

 

For now I have learn how to download code onto the board, I am quite proud of this and I also experimented around with the board to get better with it.

 

Downloading the exemple code was not that hard.

image

And the debugging tool was just fine.

image

You have access to all needed register ect... Basic stuffs here.

I was quite disappointed though not to find any example code related to the expansion board, which is quite a shame because other expansion board are supported with example code and all the good stuffs.

But anyway the output of the terminal leaved a good impression of the board.

image

 

I will finish the review once I get the motor to spin ... Hopefully I will make it to that point image

Anonymous

Top Comments

Parents
  • Nice start to your review, I like that you won't let the board or lack of motor get you down image. I am in teh same road test and the issues you are haviong sound very fimiler. I am finishing up another project and hope to get on this one ASAP. If you want to colaborate (two brains are sometimes better than one, I would be happy to compare any notes we may have to see if we can progress through this board at a nice pace.

     

    Kas

  • hi,

    Thanks a lot for the compliments...

    In fact, I just followed the basic demos and tutorials to have something to show for the review until I get something to work.

    The hardest part was to be able to flash code on the board from ccs, I had hard time figuring out you had to Debug to get the code flashed onto the target device.

    That is wierd, very different from Keil and AVR studio which separate the flashing tool from the debug mode.

    And configure the target board was akward, I didn't noticed the board was an "experimenter's kit", I choosed the debuging chip as the target device at first and got a bunch of errors that didn't explain what was going on.

     

    But unfortunately I am back to the start because my computer had a fatal crash yesterday. I whyped everything out to get a clean reinstall of windows.

     

    I would love to share everything I can with you. If you get stuck I would really enjoy helping you out (if I can).

    I'm no expert, just a random motivated student.

     

    For my "notes" I am confused since I lost everything apart from the picture which appears to be sync with my dropbox image

     

    Sorry for the crappy english. (I do speak French a lot better though)

     

    -Ben

Comment
  • hi,

    Thanks a lot for the compliments...

    In fact, I just followed the basic demos and tutorials to have something to show for the review until I get something to work.

    The hardest part was to be able to flash code on the board from ccs, I had hard time figuring out you had to Debug to get the code flashed onto the target device.

    That is wierd, very different from Keil and AVR studio which separate the flashing tool from the debug mode.

    And configure the target board was akward, I didn't noticed the board was an "experimenter's kit", I choosed the debuging chip as the target device at first and got a bunch of errors that didn't explain what was going on.

     

    But unfortunately I am back to the start because my computer had a fatal crash yesterday. I whyped everything out to get a clean reinstall of windows.

     

    I would love to share everything I can with you. If you get stuck I would really enjoy helping you out (if I can).

    I'm no expert, just a random motivated student.

     

    For my "notes" I am confused since I lost everything apart from the picture which appears to be sync with my dropbox image

     

    Sorry for the crappy english. (I do speak French a lot better though)

     

    -Ben

Children
  • Hey Benjamin Bonnal,

     

    I see you where able to get code to load into the C2000, would it be possible to explain what you did. I am constantly getting errors. I have tried CCS v5 and v6 with no success. The Errors I am getting are:

     

    CCS v5

    Can't Initialize Target CPU:

    **Error**: Serial Communication failed at port: COM65, baud rate:9600!

    To use serial monitor, please ensure the following prerequisites are satisfied:

    1. Make sure the cable is plugged into both the target and the host on the right COM port.

    2. Make sure a compatible target side serial monitor is loaded and running on the target device.

     

    - For this error I'm not sure about port 65 as it does not exist in the device manager...

     

    Source Lookup: unable to restore CPU specific container - expecting valid source container id value

     

    - Not sure what this error means...

    CCS v6

    Missing new Target configuration (not exact error)

    - I tried fixing this by suggesting the uC being used and the connection (TMS3208027 - UART Connection)


    After fixing the COM port to the correct number I get a new error:

    C28xx: Flash Programmer: Warning: The configured device (TMS320F28027), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.

    C28xx: GEL: Error while executing OnTargetConnect(): Could not read register ST1: Execution state prevented access at (ST1&~(0x0100)) [f28027.gel:272] at C28x_Mode() [f28027.gel:80] at OnTargetConnect() .

    C28xx: Failed CPU Reset: Unsupported GTI Function.

     

    I haved also seen this with v6
    Can't Initialize Target CPU:

    **Error**: Serial Communication failed at port: COM65, baud rate:9600!

    To use serial monitor, please ensure the following prerequisites are satisfied:

    1. Make sure the cable is plugged into both the target and the host on the right COM port.

    2. Make sure a compatible target side serial monitor is loaded and running on the target device.

     

    All the demo codes compile the issue is getting them to run on the launchpad, any help in moving to this next step would be very much welcomed.

     

    I will also try post these questions on the TI forum as well to see if I can get something working here...

     

    Thanks

    Kas