RoadTest: EFM32™ Zero Gecko Starter Kit w/ Sensor Card
Author: migration.user
Creation date:
Evaluation Type: Independent Products
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: Arduino Uno R3 which I already own a clone of. I was comparing the functionality with that board.
What were the biggest problems encountered?: The IDE was really hard to handle and not much Linux support was found.
Detailed Review:
I received the board about a week ago, the shipping time was a little bit long but it came from the UK and I am in Canada so it was to be somewhat expected.
My favorite part of this board is the fact that it comes with onboard features so you can immediately start working with it. It has a low memory LCD screen, 2 pushbuttons, 2 capacitive touch buttons and with the sensor kit that comes with the program includes a Humidity, Temperature and Light level sensor as well as a few more headers so you can add things to it later on.
My least favorite part about this board is the IDE itself. The IDE is based on / modeled after Eclipse and I have never liked Eclipse, so there is a level of personal preference here. Also though in terms of functionality, I experienced a lot of problems with the IDE crashing or refusing to start. When I started my first program, the IDE basically broke and refused to ever start again. Even after uninstalling the IDE and trying again, it kept trying to load the program and it crashed again. It refused to import "display.h" as well for some reason. I was hoping that there was good support for the IDE in Linux because I use it on all my laptops, but it's in the beta phase (though it feels more alpha) and there are a lot of bugs and problems with it there. The IDE is SimplicityStudios.
The reason I wanted this board is because I have a lot of fun with the Arduino Uno R3 and I have always been fascinated by these controllers. I am trying to learn C and this is the best way I can think of to do it, hands on and with a purpose.
Overall the board is great, it's sturdy, it's quality built and full of features. The IDE, for me, however, limits the functionality of the board itself and has cause me many a problem. Once I get that straightened out it will be a wonderful project-base and a great tool to learn with. I rate the experience of owning it so far: a 7/10. There is very limited documentation on how to use some of the features and I am not knowledgeable enough to know it off the bat, and that is why I am here. To learn!
Thank you RoadTest and Silabs for providing me with the EFM32 Zero Gecko, I really will enjoy it.
-Jonah