TI HDC1000EVM Sensor Evaluation Module - Review

View table of contents ...  

RoadTest: TI HDC1000EVM Sensor Evaluation Module

Author: wymand

Creation date:

Evaluation Type: Evaluation Boards

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: null

What were the biggest problems encountered?: Lack of communications protocol or software for applications

Detailed Review:

NOTE!!! After 7 months the sensor has died.

The first symptoms were very erratic readings

which could be corrected by unplugging and

restarting the sensor that worked for a while but it is now dead. 

Sorry but I will stick to the cheap ones that have worked for years.


The location for this road test is a small homestead on the side of Tiger Mountain in Washington State USA.

The place is wooded with many predators. So the coop is outfitted with a Raspberry PI and cameras.

image

The Raspberry Pi sends data to a MySQL database and the data is available on a web page

As you may see, the Raspberry Pi controls exterior lights and the coop door.  The lights come on for

5 minutes if the PIR detectors see something.

image

Also available are daily and weekly graphs of the temperatures recorded by a DHT22. 


imageimage


The intent of the road test was to compare these temperatures with the temperature of a nest box to see if a hen is brooding.  With a brooding hen

on the nest, that temperature will rise while she is on the nest.

I wrote a Python3 program to record the temperature and humidity and call it as a cron job on the Raspberry.

The deadline for submitting the report was coming up and fate and chicken temperament stepped in and they tore up the

nesting boxes for rebuilding of the nests which they do every now and then so the following comparison chart is ambient

temperature. The DHT22 as I have it in the coop has a large thermal mass while the TI is much more sensitive to fluctuation

as this comparison chart shows:

image


Below is the Python3 code


#!/usr/bin/python

# coding=latin-1

import serial

import binascii

import httplib2

ser = serial.Serial()

 

 

#ser.port = "/dev/ttyUSB0"

#ser.port = "COM4:"

#ser.port = "/dev/ttyACM1"

#ser.port = "/dev/serial/by-path/platform-bcm2708_usb-usb-0:1.2:1.0"

ser.port = "/dev/serial/by-id/usb-Texas_Instruments_MSP430-USB_Example_E89A816F1C000500-if00"

ser.baudrate = 115200

ser.bytesize = serial.EIGHTBITS #number of bits per bytes

ser.parity = serial.PARITY_NONE #set parity check: no parity

ser.stopbits = serial.STOPBITS_ONE #number of stop bits

ser.timeout = 2              #timeout block read

ser.xonxoff = False     #disable software flow control

ser.rtscts = False     #disable hardware (RTS/CTS) flow control

ser.dsrdtr = False       #disable hardware (DSR/DTR) flow control

ser.writeTimeout = 2     #timeout for write

humidity = None

temperature = None

try:

    ser.open()

except Exception as e:

    humidity = None

    celsius = None

if ser.isOpen():

    try:

        ser.flushInput() #flush input buffer, discarding all its contents

        ser.flushOutput()#flush output buffer, aborting current output

                        #and discard all that is in buffer

        ser.write(serial.to_bytes([0x4C,0x33,0x01,0x00,0x03,0x40,0x00,0x02,0x87]))

        response = ser.readline()

        tmpval = (int(response[7])*256) + int(response[8])

        celsius =  str(("{0:.2f}".format(((float(tmpval)/float(65536)) * 165) -40)))

        fahrenheit = str(("{0:.2f}".format((((((float(tmpval)/float(65536)) * 165) -40) * 9) / 5) + 32)))

        print(str(("{0:.2f}".format(((float(tmpval)/float(65536)) * 165) -40))) + str("°C"))

        print(str(("{0:.2f}".format((((((float(tmpval)/float(65536)) * 165) -40) * 9) / 5) + 32))) + str("°F"))

        ser.write(serial.to_bytes([0x4C,0x33,0x01,0x00,0x03,0x40,0x01,0x02,0x92]))

        response = ser.readline()

        tmpval = (int(response[7])*256) + int(response[8])

        humidity = str(("{0:.2f}".format((float(tmpval)/float(65536)) * 100)))

        print(humidity + "%")

    except Exception as e1:

        print ("error " + str(e1))

 

 

if humidity is not None and celsius is not None:

    h = httplib2.Http()

    myStr = 'Nest Temp = ' + fahrenheit + 'F ' + celsius + "c Humidity =" + humidity + "%"

    print(myStr)

    myStr = myStr.replace(' ','%20')

    resp, content = h.request("http://192.168.0.159/wd-db.php?sqlcmd=UPDATE%20WD_Master%20SET%20Char_Value%20=%20'" + myStr + "',Last_Active%20=%20NOW()%20,LastCheck%20=%20NOW()%20WHERE%20Equipment=%20'Coop_RPI'%20and%20System%20%20=%20'Coop_Temp_Nest'", "GET")

    #print ("http://192.168.0.159/wd-db.php?sqlcmd=UPDATE%20WD_Master%20SET%20Char_Value%20=%20'" + myStr + "',Last_Active%20=%20NOW()%20,LastCheck%20=%20NOW()%20WHERE%20Equipment=%20'Coop_RPI'%20and%20System%20%20=%20'Coop_Temp_Nest'")

    reqstr = "http://192.168.0.159/wd-db.php?sqlcmd=INSERT%20INTO%20Environment%20(`Sensor`,%20`datetime`,%20`Temperature`,%20`Humidity`)%20VALUES%20('2',%20NOW(),%20'" + format(str(fahrenheit)) +"',%20'" + str(humidity) + "')"

    resp, content = h.request(reqstr , "GET")

    print(reqstr.replace("%20", " "))

else:

    h = httplib2.Http()

    print ('Failed to get reading. Try again!')

    resp, content = h.request("http://192.168.0.159/wd-db.php?sqlcmd=UPDATE%20WD_Master%20SET%20Char_Value%20=%20'Fail_to_Read',Last_Active%20=%20NOW()%20,LastCheck%20=%20NOW()%20WHERE%20Equipment=%20'Coop_RPI'%20and%20System%20%20=%20'Coop_Temp_Nest'", "GET")


When the module was originally received, I had to write code to read the device.  I have done most everything on the RPi in Python so I loaded the pyserial

module and realized that there was no documentation on the communications protocol with the module.  Reviving my intercept lust, I pried into the

way the demo program communicated with the module.  I found that the series of bytes to send the module to recover the temperature was


        ser.write(serial.to_bytes([0x4C,0x33,0x01,0x00,0x03,0x40,0x00,0x02,0x87]))


The two bytes of temperature are returned in bytes 7 and 8 of the response.  Using those two bytes the temperature can be displayed or stored with

        response = ser.readline()

      tmpval = (str(binascii.hexlify(response[7])) + str(binascii.hexlify(response[8])))

        print("      Temperature: " + str(("{0:.2f}".format(((float(int(tmpval,16))/float(65536)) * 165) -40)))+ u"\u00B0" + "C")

        print("      Temperature: " + str(("{0:.2f}".format((((((float(int(tmpval,16))/float(65536)) * 165) -40) * 9) / 5) + 32)))+ u"\u00B0" + "F")

 

To read the humidity register send

 

        ser.write(serial.to_bytes([0x4C,0x33,0x01,0x00,0x03,0x40,0x01,0x02,0x92]))

 

The same two bytes 7 & 8 return the hex values of the humidity register and can be displayed or stored with

 

        response = ser.readline()

        tmpval = (str(binascii.hexlify(response[7])) + str(binascii.hexlify(response[8])))

        print("Relative Humidity: " + str(("{0:.2f}".format((float(int(tmpval,16))/float(65536)) * 100)))+ "%")


  There was enough available for the roadtest report to be of value so I offer it and the code in my blogs on the subject.

HDC1000EVM Python code for Raspberry Pi


Texas Instrument has a good device here.  I would rather the i2c of the RPi be available for other duties and use this TI device. 

From the looks of the protocol it would seem that more than one

i2c device might well be connected to this.  I hope TI publishes the complete protocol soon.


Thanks to Element14 for allowing me to take part in this.)

Anonymous
Parents
  • <Blush>Please note:  I am new to Python so there is a lot of changing between strings and int values in the Python2 code that is not necessary.

    I will try and clean it up and post an update </blush>


    I have edited the road test and hope to do so again when the nest is quiet and the device can be used as planned

Comment
  • <Blush>Please note:  I am new to Python so there is a lot of changing between strings and int values in the Python2 code that is not necessary.

    I will try and clean it up and post an update </blush>


    I have edited the road test and hope to do so again when the nest is quiet and the device can be used as planned

Children
No Data