SIMPLE SWITCHER®: LM46002PWP EVM by TI - Review

View table of contents ...  

RoadTest: SIMPLE SWITCHER®: LM46002PWP EVM by TI

Author: Robert Peter Oakes

Creation date:

Evaluation Type: Evaluation Boards

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: Richtek EVB_RT7275GQW Evaluation Board

What were the biggest problems encountered?: Having a DC Load to test the Board with :)., a project for the summer :)

Detailed Review:

So right off the bat I would like to say this board definetly performed to exectations reaching over 90% efficient in some tests and exceeded the rated 2 Amps as well, I was able to push the board to 3Amps given the right input and still maintained low noise and ripple although it got pretty hot at those loads

 

All my testing was performed with the jumper installed to push the output to 5V (It would be 3.3V withut the jumper installed)

 

So performing this review I was always thinking of how it compared to the Richtek EVB_RT7275GQW Evaluation Board i reviewed in a previous road test and at the end of the day I think it was better due to the improved efficiency I was able to acheive and the increased input voltage range it was able to handle (60V vs 18 with the Richtek)

Here are the tqo bards side by side

imageimage

Here is a comparison of the efficiency charts at various loads

 

The TI:

image

The Richtek

image

and for Load variations here is the TI (the current scale is 10* so it shows on he graph)

image

 

OK, so there is not much to actually show with this device, its all about how well it can keep its output stable through large swings of input volts or output load, based on the testing using a rudimentry DC Load it seems to perform very well and indeed exceeds the boards ratings. Though during this part of the test the board and particularly the Choke got quite hot so I would not feel confident running at this level for extended periods of time. Knowing it is able to handle over 50% more load intermittently though would be a comfort to anyone using this device in a critical project.

 

BOM (Bill of materials)

lets look at the schematics for the two

First up the TI

image

Now the Richtek

image

 

OK, I have not counted them but to me this looks like a tie, the TI is unsing a much larger inductor though at 10uH vs the Richtek 1.4uH

 

I have recorded several videos of the testing and will now include them as part of the review, In the videos I go through various scenarious testing output vs input voltage changes, Efficiency vs Load changes and finally a quick tour arround the various test pins on the board

part 1, the Input line regulation test

 

Next up, Load regulation tests

 

And finally the view of the various test pins on the board (The ones that where doing anything, this is while I was hammering the board with the load square wave

 

And here are some screen shots of the various test pins around the board


This is the response to a load change of about 2Amps, as you can see it recovered extreamly quickly and only dipped by about 200mV

image

This is the PG Pin while the above load profile keeps hammering away at the board, there is a lot of noise but I do not think all of it is comming from the board, I need to find what is generating this in my lab image, the blue trace is the current switching in the load

image

This is the ground connection on the board while this load is being applied, see what I mean about the noise!

image

 

So the writeup looks short and sweet but there is a good few cups of coffee went into the videos so enjoy. I was very impressed with the performance of the TI switcher and this is not the first time, one of the very first requies I performed for Element 14 was on the TI Battery Booster Pack and it too had a couple of switching regulators, in this case, "buck boost" capapable and they too performed very well. Yes there where issues with the actual board but the chips where up to par in my book. TI yet again presents a niec roduce that can be applied in a variety of situations and if you check out their site, you can find plenty of information and even design tools allowing you to quickly design your board and figure out your BOM.

 

SIMPLE SWITCHER | Power Converter | Power Module | TI.com

http://www.ti.com/lit/ds/symlink/lm46002.pdf

Anonymous
Parents
  • Hi Peter, I enjoyed your road test. Did you get a chance to check out the DC/DC Book of Knowledge that RECOM posted on the site a couple weeks ago? I felt it had some good information. I have a question about evaluation boards in general. Do they serve any purpose other than to give the engineer a chance to gain some familiarity with a new chip?

  • if you have the room in a project case, they can be used for a longer term install as there fully functional, though I think the primary purpose it to evaluate the actual chip, if your designing your own boards then it works out cheaper to buy the chip and integrate it rather than get the eval board, I'm thinking 7$ish vs 20-30$ for the eval board

Comment
  • if you have the room in a project case, they can be used for a longer term install as there fully functional, though I think the primary purpose it to evaluate the actual chip, if your designing your own boards then it works out cheaper to buy the chip and integrate it rather than get the eval board, I'm thinking 7$ish vs 20-30$ for the eval board

Children
No Data