AVNET MicroZed SOM 7Z010 + Carrier Card - Review

View table of contents ...  

RoadTest: AVNET MicroZed SOM 7Z010 + Carrier Card

Author: bartokon

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: Other Microzed and Picozed SoM's, Ultra96, Kria.

What were the biggest problems encountered?: Latest example designs were from year 2016. Microzed documentation on pinout is professional, for example I couldn't find easily pinout for pins that are connected to PL side of Microzed.

Detailed Review:

RoadTest outline

My goal for this roadtest is to create a custom microcontroller written in Verilog, implement it on Microzed, and connect Microzed to Minized by PMOD and send instructions with VIO debug interface.

 

What are we RoadTesting?

Microzed is a System In Module,  that can be connected to one of ready to use carriers or custom carrier with compatible microheaders. Microzed hearth is a ZYNQ chip, that means beside an FPGA it contains a hardened dual-core ARM processor that is capable of running embedded Linux distributions like Petalinux. Microzed have access to 1Gb of RAM memory, uSD card slot, that is SoM "hard-drive", USB connectors and Ethernet.

{gallery} Microzed Gallery

Microzed block diagram

IMAGE TITLE: Microzed Block Diagram

Microzed TOP-View

IMAGE TITLE: Microzed Top-View

Microzed Bottom-View

IMAGE TITLE: Microzed Bottom-View

Example designs - Getting started

As in others *zed family development boards, Avnet provides example designs, bad thing is all these examples are pretty outdated:

image

But, it is not that bad. If you are willing to download 2015-2016 Vivado versions, you could probably follow these tutorials and learn some core Vivado development flow, on the other hand older versions of Vivado will differ in GUI!

 

Let's talk about more interesting things, like bsp support. As the example designs are outdated, I can't say the same about Avnet GitHub scripts. These scripts provide you a starting point for yours designs, just git-clone bdf, hdl, petalinux repositories, and you are good to go imageimage

Let's try to build some projects. As Microzed is based on ARM architecture, we can build our own linux based system with Avnet make files or just Vivado project.

image

Based on script description, this script will build design for MicroZed I/O Carrier and Zed Display kit. Starting from 2020.2 we have at our disposal clean "base" scripts, which I think is much better, but I can't test these because of disc space needed for all these Xilinx tools image and 2021.1 branch is not ready yet. I think mz7010 should have some extra scripts for dedicated carrier board much like Picozed. PS. build failed... I hope it is fixed in 2020.2 image

image

The constraints file is general. If you need to connect some pin from MicroZed to external board, search for pinout documentation.

For my purpose, let see... I would like to connect JM1, JM2, PL-PMOD from carrier to Minized. Let's search in .xdc JM-1, JM-2, PL-PMOD, nothing... only JA, JB, JY. But where all this J* point to? SoM have unnamed Pmod on board. Let's try search in proper documentation.

 

According to Microzed carrier hardware user guide page 13, I have found JM and page 16 PL-PMOD connections.

{gallery} Constrains_gal

image

IMAGE TITLE: Microzed JM2

image

IMAGE TITLE: MicroZed PL-PMOD

So, sum this up and create new constrains file we could use in our project for PMOD.

image

Microcontroller project

Let's create new Vivado project using Microzed board, import source files.

Create new block design with Microcontroller hierarchy.

image

In this block design, VIO is used as a logic analyzer, uC reset and enabler. From external pins, "program_data_address" and "clk" comes from Minized. Normally, when uC is implemented in one chip, it uses 15 bit "program_data_address" port from control_unit to make jumps in address memory. In this roadtest I will do jumps manually by using VIO to control logic directly image. So what does the uC look like inside? It is made from 3 general blocks.

Control_Unit - interprets program_data instruction at "posedge clk" and sends instructions to ALU and memory block at "negedge clk".

image

ALU - takes instructions from control_unit, and makes calculation like add/sub, and also perform comparator functions. For example, if A input is bigger than B input, the A_bigger flag goes to logic "1" etc...

image

Memory - general memory block, takes data from program memory → control unit or directly from ALU. You can save data to general_registers or compute_unit_ram. You can use a multiplexer to send new data to the output port to control for example another logic block.

image

Program_memory - Contains hardwired program memory.

We can program this block by using pseudo machine code:

image

  Or macros that act as assembler for example:

imageimage

As this Minized-Microzed implementation is not autonomous (program_data[] won't increment itself) we will act as program counter and select what instruction uC should execute by VIO. Let's jump to Minized project.

 

Minized project

Let's create another Vivado project targeting Minized, create new block design and modify .xdc file from Avnet GitHub.

image

Minized constrains:

image

 

Hardware connection:

Connect Minized and Microzed together via PMOD_1 and PL-PMOD. I have used some free lying cables and pins to create connection between these systems image

image

Generate bitstreams for these projects and program both development boards.

Use Vivado hardware manager to interact with VIO debug cores, interact with Minized output ports and control uC in Microzed fabric.

 

So after some time spend testing, there is a bug in uC design! It seems that regardless what we do, VIO reads "0" from accumulator, what could be the cause?

Let's take a few steps back...

 

Reimplementing design

Let's connect VIOS/ILA's differently.

image

I think that the issue can be in three places:

-One, you can't possibly variable from load memory, so in the control unit.

-Two, accumulator is somehow broken.

-Three, memory bridge is bugged.

 

Let's Work on ALU unit. Right click on wires/buses and run connection automation to add VIO/ILA cores to system. The next step is implementing design and running it on Microzed.

image

Remember what our project does. It reads instructions from "program_memory" and execute command, after the execution the "program_data_address is incremented". Starting from "0" address.

image

We are seeing some activity in "program_data_address", it seems that "Overflow" flag is not up and program gets stuck.

image

 

Data out, ports stayed at "0" all time, so ALU isn't getting any operand to work on!

image

 

Clear all previous debug ports and mark new ports from memory hierarchy for debug, run connection automation to connect system ILAs.

image

 

image

Generate bitstream and program device.

image

Click "+" on trigger setup and add trigger on "program_memory_0_program_data"

image

In "value" type "1101_0000_0001_0000" binary vector. This should trigger ILA when constant "1" is loaded from program memory.

image

Now arm ILA and restart system manually with VIO. The new waveform should be visible in "hw_ila_1" window.

image

Focus our attention on CU_RAM, mark more debug ports if necessary.

image

So, in my opinion, I have found the bug. Instruction nb[3] loaded from program memory, that means nb[2] is executed. I think it reads "0" not "1" (look at "register_write" and "micro_outpt" ports)

image

 

Meanwhile in behavioral simulation:

image

Summary

Agile workflow doesn't work in FPGA's, before writing any code you should thoroughly think about the way you are implementing the actual hardware. There is no, quick re-write, re-compile whole project. Fixing a simple bug in memory bus could take days!

Even if design is working in simulation, that doesn't mean that it will work in real implementation! This was an interesting project. I have learned a lot about Verilog and designing hardware. This was, I could say, my first Verilog-type project from scratch, and it was quite challenging.

 

What about dev-board Microzed? It is like an old trusty car. Old design that is working, maybe there is a new paint, but it is a little outdated. I like that this board can work in stand-alone mode aka SoM  or with a carrier board, if you get bored with basic functionality or are interested in developing your own hardware, you could create your own carrier board. What about other similar boards? If you have the extra ~20 dollars, there is Ultra96, or new Kria SoM, which is based on Ultrascale architecture, but you do not need it if you are learning the basics.

Anonymous