RoadTest: Agilent U1620A 200MHz Handheld Oscilloscope
Author: migration.user
Creation date:
Evaluation Type: Independent Products
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?:
What were the biggest problems encountered?:
Detailed Review:
Hi all,
I'll start my review as usual with the basic hands on and package content with some photos included, I will continue later on with more usage details etc.
Here is the first view of the nicely packed box after it arrived.
I do always prefer to have the contents padded on each side but the package was marked fragile so it should be safe.
Product box itself opened, neatly packed and the meter is very well cushioned.
The paperwork, calibration certificate is included.
Overview of the rest of the box contents. The powercable is old UK/South Africa style if I'm not mistaken and not very usable here, but as it is a standard 3-prong cable that is not a problem.
The heart of the box itself in it's comfortable cradle... First impression: It's bigger than I expected
The meter on hand, the strap is quite comfortable.
Look of the buttons, nicely placed, not too crowded. The buttons feel good, they can be pressed from any angle and work fine. Plus they make a comforting "click"-sound when pressed so you really feel that the button was actually pressed
View of the top connectors, the trigger input is also used for calibrating the probes.
Side port cover and locking cable hole.
Rear of the meter
The rear of the meter with the stand "leg" out. The latch that holds the leg is quite stiff, the leg bent quite a lot until it lets go properly. Probably it will get looser in use.
The meter with the stand open. Sits in a good comfortable angle.
The view with the stand open.
The hand-strap tightening system, easy to use for sure and well adjustable.
The side USB and power connectors under the cover, well protected by the thick rubber.
The power supply, hefty piece.
Instructions for the power supply
BNC to probe adapter for adjusting the probes.The thickness of the ground side is a bit too much for the ground alligator-clips of the probes so it easily slips off.
DMM side test leads
Package opened. Everything is plugged with good quality banana connectors and the wires are nice and flexible, good quality stuff.
Two packs of 1:10 probes wer included.
Package opened, again very good quality.
And parts put together.
And paperwork of the probes, first side.
Second side.
Clip from the manual (http://cp.literature.agilent.com/litweb/pdf/U1610-90040.pdf):
Before using the handheld scope for the first time, fully charge the
battery for at least 5 hours, with the handheld scope turned off, using
the AC/DC adapter provided.
The power key will turn constant yellow when the battery is fully
charged.
Looks quite green to me.
Ok that's the first part, more to follow of course with the actual usage part of the review.
Elias
Update: Problems with the USB connectivity were on my PC side, now it works perfectly. The meter mounts as a windows mobile device, which was quite unexpected, the ScopeLink works perfectly and basically shows realtime screen from the meter!
Update2: Rest of my review is on hold unti further notice as the meter broke down. I was measuring a simple crystal when the screen went blurry all of a sudden. I tried to reboot with the same result, except this time the meter couldn't be turned off either. Removing the battery shut the device down but when trying to turn it on now only the power button lights up, nothing else happens. I contacted Agilent and they told be to contact Farnell for a replacement. So the meter is officially bricked. I'm currently waiting for info from Christian.
Update3:
I just had a conversation with a very nice guy from Agilent, going through the specifics of the issue.
A replacement will be arranged so I can continue my review within couple of weeks or so.
Alltogether very good communication from Agilent so I can only recommend them as a company, as after-sales services are working very well.
Though it wasn't really a planned part of the review, this has also now been tested and I can give 10/10 to Agilent in that area
Part 2:
Hi everyone. Sorry for the delays, damn work taking time...
I have done some usage testing and have no major complaints, I like the way the scope and the software work in general.
The biggest shortcomings are in the logging capabilities as I think the functionality is not enough to have good data to analyse.
The attached image shows the logged waveform, realtime data and the logging window.
Image of the scope itself in use:
So it seems we can't just log raw waveform but only statistics of the measurements that are set in the measure menu, when using the scope itself.
With the scope link software one can save a snapshot of the waveform but it is just the current view and nothing else, also, I didn't see any way of doing measurements with the saved waveform so it is more or less a screenshot but can be adjusted a bit.
On the other hand I do like that you can fully remote control the scope with the software so it is definitely handy.
The screen clarity is very good with each of the display modes so I have nothing to complain about that.
After about 30min of usage I measured about 41 degrees celsius on the back side of the scope, so it definitely needs the internal fan to keep the running temperature in spec. After 1.5h hours of continuous use the max temperature on the back side has reached 50 degrees celsius.
All in all, the only negative sides I have found that the logging capabilities are more dumbed down then was expected, and that the battery runs out when the scope is not used. Plus that it mounts a WindowsCE device and drive to my computer
Thanks again to Agilent and Element14 for the opportunity, I will keep updating the review if something new comes up!
Regards,
Elias
Top Comments
Hi Peter,
I appreciate your inquiry as to making Oscilloscopes more usable for the disabled.
From my perspective I can lay out some general requirements that would aid myself and others struggling to continue…
i have had the oppertunity to try bolth the fluke scopemeter 190 and tektronix ths3000, while these are bolth 4ch scopes neither had the option of ext trigger, or an actual dmm input.
if your looking for…