Wolfson Audio Card for Use with Raspberry Pi - Review

View table of contents ...  

RoadTest: Wolfson Audio Card for Use with Raspberry Pi

Author: malakai

Creation date:

Evaluation Type: Evaluation Boards

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: null

What were the biggest problems encountered?: Incorporating the necessary files into Raspbian by default is still being worked on.

Detailed Review:

Full Run

 

Short Run

 

 

Grab the Jasper image from their website

 

 

Jasper | Documentation

 

 

Copy the image to the SD Card boot Pi. Run the configuration utility.

 

sudo raspi-config

 

expand rootfs, set localization, keyboard, and time.

 

 

reboot the Pi then update Raspbian

 

sudo apt-get update && sudo apt-get upgrade -y

 

Get Ragnar Jensen's kernel originally posted setup Re: Re: Wolfson modified Noobs raspbian zipped img  Cannot unzip new download

 

File name is kernel_3_10_25_wolfson.tgz

Size is 17MB

https://drive.google.com/file/d/0BzIaxMH3N5O1RnJfcGVpdmY1T1E/edit?usp=sharing

md5sum dec8d63b3c42846e54082c7c6ff1834f

 

 

 

To install:

 

 

Become root: sudo -s

Go to root directory: cd /

Untar the archive: tar xvzf /path/to/where/you/saved/kernel_3_10_25_wolfson.tgz

 

Add the line

  kernel=kernel_wolfson.img

to the file /boot/config.txt

 

 

·         Reboot

 

 

If it doesn't work, you can revert to your original kernel by just removing the "kernel=kernel_wolfson.img" line from/boot/config.txt

 

  • Grab Wolfson img

 

wget http://www.element14.com/community/servlet/JiveServlet/download/104303-128960/wolfson_drivers.tar.gz

 

Extract the patch software into the home directory

 

 

tar -zxvf wolfson_drivers.tar.gz

    A.  Configuring the Jasper Client

 

 

Install Jasper Client

 

 

In the home directory of your Pi, clone the Jasper source code:

 

 

git clone https://github.com/jasperproject/jasper-client.git jasper

 

§  Jasper requires various Python libraries that we can install in one line with:

 

 

sudo pip install –upgrade setuptools

 

 

sudo pip install -r jasper/client/requirements.txt

 

 

Run crontab -e, then add the following line, if it’s not there already:

 

 

@reboot /home/pi/jasper/boot/boot.sh;

 

 

Set permissions inside the home directory:

 

 

sudo chmod 777 -R *

 

 

I run the script anyways as it doesn't always go right on reboot.

 

/home/pi/jasper/boot/boot.sh

 

sudo reboot

 

 

Restart your Raspberry Pi. Doing so will run boot.py, which generates the languagemodel.lm file in the client/ folder.

 

 

Using Ragnar Jensen’s .asoundrc file is the key to getting it to work

 

 

Backup the existing file

 

cp ~/.asoundrc .asound.backup

 

rm ~/.asoundrc

 

sudo nano ~/.asoundrc

 

Paste the contents of the modified ./asoundrc file listed below.

 

 

Getting Jasper to play requires that you can play a wav file using aplay with no arguments. Once that works, you want to remove the aplay hardware references(-D hw:x,x) in /boot/boot.py and /client/mic.py

 

 

 

Try this file:

 

aplay /home/pi/jasper/static/audio/jasper.wav

 

 

If you get it to play you have setup your system correctly and are good to go.

 

You may need to test the Wolfson files for the correct connection:

 

 

 

 

./asoundrc file contents modifications made by Ragnar Jensen

 

#######################################################################

#

# Use libsamplerate instead of internal resampler.

# You might have to: sudo apt-get install libasound2-plugins

# Or just comment out the next line if the internal one is good enough for your needs.

# defaults.pcm.rate_converter "samplerate"

 

 

######################################################################

#

# Wolfson Audio Card for Raspberry Pi

#

pcm.wolfson_pi_soundcard {

    type hw

    card sndrpiwsp

    device 0

}

# Create a Master volume control

pcm.softvol {

    type            softvol

    slave {

        pcm         "pduplex"

    }

    control {

        name        "Master"

        card        0

    }

}

 

 

pcm.!default  {

    type           asym

    playback.pcm   "plug:softvol"

    capture.pcm    "pduplex"

}

 

 

#####################################################################

#

# Mixing and resampling goodness :-)

#

# Several clients can record and play back simultaneously.

# The dmix and dsnoop plugins operate at 48kHz by default, i.e. the sound card will be kept at 48kHz at all times.

# All playback streams are converted to 2 channels/48kHz/16bit.

# All recording streams are converted from the card's 2 channels/48kHz/16bit

# to the requested number of channels, sample rate and bit depth.

 

 

# We define one pcm device called "playmixer" for playback.

pcm.playmixer {

        ipc_key 140324  # Any number will do, as long as it's unique in the system.

        ipc_key_add_uid true

        type dmix

        slave.pcm "wolfson_pi_soundcard"

}

 

 

# Define another one called "recmixer" for capture.

# The sound card will run at 48kHz and input is resampled to the requested rate.

pcm.recmixer {

        ipc_key 140325

        ipc_key_add_uid true

        type dsnoop

        slave.pcm "wolfson_pi_soundcard"

}

 

 

# Define a duplex device, with both in- and outputs.

pcm.duplex {

        type asym

        playback.pcm "playmixer"

        capture.pcm "recmixer"

}

 

 

# Add a "plug" plugin for the above "duplex" device.

# This is where all the converting takes place.

# Sample rate, number of channels, bit depth.

# By the way, who thought that "plug" was a good name for a plugin?

#

# Use this device for all your playback and recording resampling needs.

pcm.pduplex {

        type plug

        slave.pcm "duplex"

}

 

 

# A ctl device to keep xmms happy

ctl.pduplex {

        type hw

        card 0

}

 

 

# A DSP to keep the alsa-oss layer happy:

pcm.dsp0 {

        type plug

        slave.pcm "duplex"

}

 

 

ctl.mixer0 {

        type hw

        card 0

}

 

 

image

Anonymous