CEL Robox 3D Printer - Review

Table of contents

RoadTest: CEL Robox 3D Printer

Author: dougw

Creation date:

Evaluation Type: Independent Products

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: Ultimaker 2 - it also gets good reviews, but it cost twice as much.

What were the biggest problems encountered?: The software is simple to use compared to competing products, but still not entirely intuitive - more detailed step by step instructions or a more detailed tutorial would help to get first time users up and running. Action icons should have text explanations that pop up when hovering over the icon of what they do when clicked. It would be great if there was a "Feed Error" indicator to flag when the filament is not fully fed in. Clear PLA would be a great addition to the available accessories. [updated comment: Note the software is continually being improved and the manufacturer already seems to have responded with new versions that address all the issues I was having. This printer is more automated and less fuss than most others I have seen.]

Detailed Review:

Mine was one of the lucky proposals selected to participate in the road test of the fantastic Cel Robox 3D Printer.

I will be documenting my initial experiences here, but I will be using the printer in many future projects and will try to update the links here along with other links associated with this road test.

Links:

Cel Robox 3D Printer Road Test page: http://www.element14.com/community/roadTests/1354

My proposal: http://www.element14.com/community/roadTestApps/14932

Robox road test discussion group: http://www.element14.com/community/inbox/dm/185299?et=notification.direct.message

My first attempt at 3D design and printing: Tangible Badges - The 3D Tangible Badge Project

My Heart Reactor & Crown Tools design challenge project: Sudden Impact - Crown Tools and Heart Reactor - updates 1-39

My vibration sensor project: Tis The Season For Arduino

My illuminated star project: Tis the Season for 3D Printing

My phone rescue mission: Robox to the rescue

Arc Reactor: Wearable Interactive Arc Reactor

Trophy: Interactive Trophy

Maple Leaf: LED Road Test - Maple Leaf Christmas Decoration - Blog 13 Dec 24

Space Ship: The Starship Enocean Voyager - Pi IoT Blog 4

Heart Reactor: Sudden Impact - Crown Tools and Heart Reactor - updates 1-39

Dodecahedron: Dodecahedron Light Fixture

Phaser: 3D Printed Phaser

 

Unboxing

I was a bit clueless when unboxing, which is partly the point of the following video. The value is in the comments and followup video below.

The package includes a USB memory in a credit card sized USB dongle, where the USB connector flips out on a pivot.

The USB memory contains the AutoMaker software package, but I had already downloaded the latest version from the Cel Robox web site since it is free.

imageimage

The AutoMaker software can load .stl files and slice them up into a printer command steam that downloads to the printer, even as the printer is operating. Once the print file is downloaded the USB connection is no longer needed and the printer can complete the job unattended.

Setup

It took a couple of hours of messing around trying to figure out what to do before I got my first print underway.

I had not fed the filament in properly even though the feeder seemed to have gripped the filament and because of this there was no "Print" button. It wasn't obvious to me what was wrong - It took a lot of scouring of the internet to even deduce what the "Print" button looked like and where it should appear. My model was loading fine, but there was no obvious way to proceed - no error flags, no diagnostic menus, nothing in the setup screens to indicate what the problem was. Eventually after a few tries at feeding the filament it properly grabbed the filament and auto-fed in about 10 inches of filament.


Printing

Since getting the printer running, it has run essentially non-stop for 20 hours on 7 jobs and it will continue for the whole weekend because I have a long backlog of things I want to print, and I can design them faster than I can print them.

My first effort was the design challenge "WINNER" badge linked above. It was not able to print the text section of the badge, possibly because the text was too small or possibly because the heat was not optimal. I tried it at both normal and fine resolution with white PLA, but neither worked well. It will take some investigation to see if it is possible to print at that size successfully.

My third print turned out perfectly, but I was hoping the 2 inch dome I was printing in white PLA would turn out more translucent since it will be illuminated from inside by an LED.

Since I couldn't get Robox PLA reels in clear, I bought a reel of clear PLA from a third party and rigged it to feed from an external axle (because the hubs are incompatible). This worked well as you can see in the video below.

Here are some closeups of the filler webbing set to 40% to conserve plastic and the overhang stranding in the interior plus a shot of the exterior finish - this was a normal finish, not fine.

image

image

image

Click image for a demo.

Note that this material is "clear" PLA which shows a lot more structure than the opaque PLA materials.

One of the projects I proposed to work on with this printer was enclosures for Enocean sensors:

image

Click image to view video.

Note the clear PLA allows light to reach the solar cells while completely enclosing the sensors.

 

Another project that I proposed was to make a case for the clock version of the Henrietta Project.

This case took over 8 hours to print because I printed it with a solid 100% fill (I wanted to drill and tap screw holes and that works better in solid fill)

However, the printer performed flawlessly and you can see the results below.

image

Click image to view video.

image

Here I replaced the clear acrylic faceplate with a printed PLA faceplate to see if it looked better. It is great to have a 3D printer so things like this can be tried on a whim.

Conclusions

The Cel Robox 3D printer is phenomenal. It makes a huge difference in transforming my projects from crude and boring rectangular black boxes into aesthetically attractive and interesting systems. The learning curve is well worthwhile and this machine has been designed to keep it to a minimum. So far I have not had to think about or learn about calibration - I just import an STL file and start printing. As far as cost goes, for most of my work this machine effectively replaces a whole machine shop full of far more expensive equipment. The results are far superior to any other home-made solutions both in aesthetics and functionality, and although the printer can take hours to complete a print, the labour of designing the item is actually less than the labour involved in manually hacking some other enclosure together with appropriate mounting and cutouts (both time-wise and physical effort-wise).

One general note is that clear PLA is an important material in many applications where lighting effects or internal illumination are desired and it also allows you to see internal hidden fit and tolerance of finished parts.

If I had known how strong the plastic was and how easy it is to get decent results, a 3D printer would have been much higher on my wishlist. It is already hard to imagine how I could ever get along without a 3D printer. I do dozens of projects every year and this printer will feature in most of them, so stay tuned for future blogs.

 

Update: The Robox has been running for 2 years now - it runs every week, sometimes several objects per weekend. It has lasted amazingly well - I have been through many kg of pla. I am still extremely happy with the printer and now find it to be an indispensable tool. It has dramatically changed how I do things and greatly improved my performance.

Anonymous
Parents
  • Hi Doug! Wow. Impressive that it's been running for so long, I half-expected there to be issues with that, e.g. due to bits overheating perhaps. Is it designed for 24/7 use if required?

    It's also great that it is fully enclosed, I'm guessing it also prevents hot plastic smell : ) and keeps noise down?

    I've never used a 3D printer, so curious to hear more about the finish, in the video your printed items looked pretty smooth!

  • The noise level is about the same as my laser printer, not as quiet as an UltiMaker 2, but that machine cost twice as much. I have it operating in my living room right now and it doesn't interfere with TV audio in the next room. I can work fine on my computer with it grinding away in the same room.

    It does a good job of accurately controlling the temperature of the nozzles, the bed (which it keeps at 65 degrees), and the air in the enclosure. All 3 temperatures are reported continuously and they are settable. The bed does not need glue, my prints stick to the bed until the bed cools down - really slick - I was expecting more issues with parts not sticking to the bed.

    The PLA doesn't give off much smell at all, although I think I have a slight allergy to it. Not enough to stop me printing however.

    I will update the review to include high res pictures of the finish, although I am not doing much work at the finest finish setting as the normal setting is good for me.

Comment
  • The noise level is about the same as my laser printer, not as quiet as an UltiMaker 2, but that machine cost twice as much. I have it operating in my living room right now and it doesn't interfere with TV audio in the next room. I can work fine on my computer with it grinding away in the same room.

    It does a good job of accurately controlling the temperature of the nozzles, the bed (which it keeps at 65 degrees), and the air in the enclosure. All 3 temperatures are reported continuously and they are settable. The bed does not need glue, my prints stick to the bed until the bed cools down - really slick - I was expecting more issues with parts not sticking to the bed.

    The PLA doesn't give off much smell at all, although I think I have a slight allergy to it. Not enough to stop me printing however.

    I will update the review to include high res pictures of the finish, although I am not doing much work at the finest finish setting as the normal setting is good for me.

Children