CEL Robox 3D Printer - Review

View table of contents ...  

RoadTest: CEL Robox 3D Printer

Author: thundersqueak

Creation date:

Evaluation Type: Independent Products

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: I am familiar with printers such as the makerbot 2x which I have used at my place of employment for production of enclosures and other parts for use in the oil fields of Alaska.

What were the biggest problems encountered?: The initial unit failed, the system itself would overheat drastically and it also was extremely loud. The second unit is about the same loudness level as your average ink jet printer. The item being printed does not always stick to the build platform and when you print some items that are thin, there will be curling of the part as the ends lift up from the print bed.

Detailed Review:

The printer first arrived, the initial one and I was excited.  It was right before Christmas.



image

 

 

Pre-Production Model:


 

I know what you are thinking, this review is long overdue.  This is partially true, but only comes this late as I had to send the unit back.  It was shipped to Element 14, then to the U.K. then back to Element 14, then back to me.    When I first contacted Cel about the issues I was having, they were willing to help me out with some basic troubleshooting.  It turns out that some mosfets in the unit had failed and that it was drastically overheating.  There was also a huge issue with the extreme loudness of the unit.  The fans would run at full speed.



image

 

 

 

Production Model:


 

Upon receiving the unit back however, I was pleasantly surprised.  Cel had included a bag to lift the printer out of the box, this was a very nice touch.  The new printer is also much quieter.


 

I immediately began to print new items.  First, I went and tried to print part of a project I had been working on, a DIY VR head mount display.  Part of this process included a large flat piece and this was the perfect test in order to see how much curl shows up during the print.  In order for there to be minimum curl the temperatures of the build platform and chamber have to be correct during the entire print process.  The Cel reels contain a chip that supplies this information for each material and then sets the printer up accordingly. 

 

image

image

 

The lens holder that I printed did shrink a bit, but that is the nature of ABS.  It would be nice if the software would automatically compensate for this and size it up slightly with perhaps a checkbox.  As you can see there is some curl and twisting of the piece.


 

To check the resolution I printed some miniatures used in table top gaming.  This is a good test as there is often a lot of detail in such figures.  I set the printer up as high as it would go and after loading an image hit print. 


The first print required support and the software did give the option to include it by setting it to auto.


image

 

One feature I wish was included would be the ability to preview the support structure before printing.    I have concluded that the auto support material feature works the majority of the time, with one exception where the printer attempted to print part of a figure in mid air about 2 hours into the print.

 

 

image


After some fiddling with the controls and some calibration, here are the results.  If you examine the gun,  the printer would cause slight misalignment to the print job as it continued on the figure.  Conclusion, the printer has a hard time doing extremely small parts or fine detail.  Even when a support structure is printed with the object, it tends to move the object just enough to throw things off. 


image

 


Next, a figure that does not require a support structure.

 

image

image

image

 

There is very little I can say about this, it came out better than I had expected!  The figure is smooth to the touch as the layering of the print was set to fine (about 30 microns).  I took this figure with me to the local makerspace and there was a lot of excitement over the resolution that this printer managed to achieve on this scale.

 


Printing Moving Parts:


 

For the this print I selected the NASA wrench.  Unfortunately I was forced to stop the print as it became disconnected from the print bed.

 

The fill pattern is clearly visible, they opted for a crosshatch pattern instead of some other method.  This results in very strong parts.


 

image

 


Some of the material did not adhere to the print surface.  This seems to be the norm with this unit, smaller components do not stick to the print bed by default.  Larger items with a high surface area contact do however manage to stay firmly attached to the bed until it cools, upon which the item is released with minimal force.


 

CCx76qyUsAAd6pZ.jpg

 


Next up, I switch the printer over to PLA.  After extruding the printheads using the purge function in the software I printed the following.

 

image

 

The resolution is very fine and I much prefer printing with this material over ABS.   I also had fewer issues with the print becoming dislodged from the build platform.  There was a very slight lifting in the corners however but nothing serious.  I give the Cel Robox printer + PLA  a huge thumbs up! 



Pros:

  • Easy to set up, simply remove it from the box, install the software and plug the printer into the USB. 
  • Self leveling bed, this makes life a LOT easier for the beginner and the veteran alike. 
  • The build chamber heats up and maintains a proper temperature for the material being used.
  • The bed becomes tacky when it heats up, hopefully negating the need to use hairspray or blue tape.
  • The new unit is very quiet, about the same decibel level as a standard inkjet.
  • Relatively fast prints when compared to other leading printers on the market in this price category.
  • You can pause a print in progress.
  • Software is easy to use with lots of options, although for some you may have to go digging.
  • Small form factor with a very large selection of material to choose from. (only PLA and ABS were tested in this review as that is what the unit is shipped with).  The unit specification as of this writing also lists HIPS, Nylon, PC, and PVA.
  • Good size print volume (210 x 150 x 100mm or for Americans 8.3 x 5.9 x 3.9”).



 

CONS:

 

  • The items being printed do not always stick to the bed.  This was especially true for small components that had very little surface area with the bed.
  • No option in the software to print a “raft”, Brim was included but does not always give enough surface area.
  • Once you pause the print, you cannot open up the build chamber to fix something.  Doing so aborts the entire job.
  • No preview in the software to show support structure before it is printed.
  • Software does not compensate for the shrinkage that ABS suffers as it cools.
  • When printing items, the edges tend to curl as the material lifts from the bed.


 

Would I recommend buying this printer?


 

Yes, simply put, this is one of the easiest printers to use that I have ever seen.  Within about 10 minutes of taking it out of the box you can be printing.  Even with the few shortcomings, many that plague all 3D printers, you will not find a more newbie friendly product on the market. 


 

The Cel Robox team were very receptive to my inquiries  when the original unit began to fail.  It should be noted that the original unit was never intended to be sent out for review as it was a pre-production model.    The unit, after being shipped to the manufacturer took about 2 months to get back to me for this review.  Was I comfortable with dealing with them? Absolutely yes.  They handled the situation in the best possible way.

 

This printer now has a permanent place in my tool kit.  It is the perfect size to sit on the desk and has all the required capabilities you would expect in a 3D printer.


 

image

 

UPDATE July 2, 2015

 

I decided that I wanted to show these images, it is of how well a part that was printed on the Cel Robox held up under months of stress in a wire spooler.  This particular spooler winds everything from silver satin to LMR-400 onto wooden spools, and I must admit, the part held up a LOT longer than I thought it would.  After 1 month of service it finally quit and you can see the failures in the image below.  This is a testament to the quality of part that this printer is capable of.  The part was printed using standard "normal" settings with a 40% infill.

 

 

image

imageimage

Anonymous