RoadTest: Amphenol Air Quality Engineering Dev Kit - Industrial Sensing
Author: vannystick
Creation date:
Evaluation Type: Independent Products
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: gp2y1010au Sharp dust sensor
What were the biggest problems encountered?: OLED screen failed following a few drops, assembly of sensors to shield is not very positive, humidity probe wire is very stiff
Detailed Review:
I have used this kit in a real world situation for several months and it has proven to be not only a useful tool but incredibly educational. The range of the sensors within the kit make it an excellent choice as a starting point for understanding air quality measurements. The kit offers extremely good value compared to buying the parts individually and is supported by clear, well documented and considered code for the Arduino. There is some room for improvement but my use of this kit is far from over!
This has been a great experience and I would like to thank neilsroberts for providing the kits
Let see how I got on. . .
Background and Application
I have been working in the automotive sector for ten years, and my company have been asked by a customer to investigate opportunities for improving air quality in the cabin. This is especially important in China where air quality monitoring is as common as checking for rain in the UK. My electronics (hobby) background gives me a good basis with Arduino, metrology and sensor kit design and packaging.
I am well experienced with cabin temperature and humidity and have a good understanding of what creates ‘comfort’ but my experience of air quality is a little limited. I expect to improve my understanding of typical cabin air quality and how it changes during a drive cycle. I will compare this against the air quality of the building I work in. I will explore the effect of some basic changes to improve cabin air quality with before and after evaluation of the changes. If time allows, I will compare the readings of the sensors against metrology systems commonly in use within the automotive.
You can read more about my back ground here Begin at the beginning. An Introduction.
Expectations
The EPA Air Quality Index is a great place for acceptable limits of substances in the air.

Unboxing and First Use
Hardware Observations
Recommendations
Arduino Code
The Sensors
Temperature and Humidity
The T9602 temperature and humidity sensor is an excellent package size for use in the cabin. Typically I would use a much large probe which is intended to be used outside the vehicle and becomes quite clumsy inside the cabin, so the T902 is a really good solution for me in every day testing. Operating range and accuracy for humidity is right where I need it to be for my application, although a temperature operating range of -20c and +70c would probably cause me issues. I regularly see cabin temperatures exceeding these limits (real world) which suggests the sensor is geared at indoor measurements only (despite being IP67 rated).
One issue I did find, repeatedly, with this sensor was the cable. It was far too stiff for the way I wanted to use it and I wanted to measure temperature and humidity in the same air stream as the dust sensor, this became quite a problem. Ultimately I resorted to a spot of carpentry to wrestle the cable under control.
Dust Sensor
The SM-PWM-01C dust sensor is a far superior looking sensor to many of the cheaper rivals, perhaps simply because of the black PCB or neatly arranged components with clear and contracting silk screen. It has very good performance to match. While more than double the price I have paid for an older designed Sharp sensor, GP2Y1014AU0F, the SM-PWM-01C reading was more stable and consistent perhaps simply because it is digital.
Like the temperature and humidity sensor, the dust sensor is also specified to be used indoors in a more controlled environment than I would normally test in. An operating temperature between -10 and +60c just won’t cut it in an automotive application. I have now tested at -20c in a controlled environment without issue, although I have no reference sensor to test against. It is also not clear how the sensor would react to sudden temperature changes. I suspect the readings might be out if condensation forms on the reflector mirror or IR sensor.
Without an aspirator fan, the dust sensor must be located in a vertical position and directly in the flow of air to be measured. For an automotive application this simply won’t be possible to package, so it is likely that that an aspirated version from a competitor will be required.
Despite the limitations for application, the learning derived from this sensor has been significant and invaluable as we will see below. I suspect a laser version of the sensor would potentially overcome many of the limitations.
CO2 SENSOR
The T6713 carbon dioxide sensor is truly remarkable and the part of the kit that I have most enjoyed working with. To think that so much information can be gleamed from such a small package is astounding. Again operating and storage temperatures would cause concern for automotive application, but the potential for this sensor in the cabin makes me think this limitation could easily be overcome. I’ll come back to this sensor later.
OLED Screen
Okay, the 128 * 64 OLED is not a sensor, but it is a significant part of the package. I’m used to using Arduino with screens and have plenty lying around, but to include it really does make the kit a full and complete package. I like the colour combination and it is very clear in all ambient lighting conditions.
Unfortunately in my case, a few unexpected trips around the foot well of the car didn’t do the screen any good and it failed. It actually took some time before I found this out as I had only been running with the logger and not the display output.
~$20 from many sources
Value for Money
I've put the DigiKey current prices in to show how good the value of the kit is compared to buying individual sensors is.
Total price for sensors alone is $181, the Digi-Key price for the whole kit is just $143.55, and the includes the shield and Arduino compatible with great source code to go with it!
Baseline Testing
For an initial test, I set the kit up on my desk and let it record for a day. I expected to see nice stable conditions as the desk is far from any doors (or windows) and well-conditioned. I wasn’t disappointed, the logger worked well, the traces are relatively flat and the spike in CO2 around 3000s can be attributed to a desk based meeting of minds (or lunch).
The two spikes are caused by movement rather than a bad sensor.
The values meet previously defined expectations giving good initial confidence in the readings.
Vehicle Testing
At the time of writing I have logged over 50 hours of data in car with the sensor mounted between the head rests of the car (yes that is a stick and cable tie assembly).
I don't intend to bore the reader with a graph of every single trip, but I thought it would be interesting to see some of the real world testing
The graph below shows a typical drive cycle, short town traffic followed by highway (60 to 70 mph) for 40 minutes. At initial look it would appear that dust level is proportional to speed, but further data analysis has shown that the other vehicles on the road at the time have a bigger influence. For example if I follow a couple of lorries then the dust level is far higher than if I am on an empty highway. I put this down more to up-draft of dust from the road surface than vehicle emissions.
It can also be seen that the climate control system is doing a good job of managing the temperature and humidity of the cabin.
For similar driving conditions, with AC off (compressor disengaged) we see a notable increase in humidity as the air is not being dried.
Again for similar driving conditions, with the climate system locked in re-circulation mode, we see a steadily growing CO2 level which reaches levels consistent with poor concentration, loss of attention etc. This is not a surprise as the cabin air is not being replenished, but does offer an opportunity to improve cabin air quality by limiting the duration the system can stay in recirculated air mode for example.
It is clear in all of these traces that the CO2 level starts quite high and drops down. The technical note for the sensor does specifically note that the sensor takes 5 minutes to warm up and give a stable reading.
Sensor Accuracy
I don't have access to a calibrated CO2 or dust monitor, comparing the AAS dust sensor to the Sharp sensor while comparable levels the AAS sensor gave a more robust value (not cutting out) with far less noise on the reading making it more reliable for making decisions from.
I was able to use a calibrated Testo meter for temperature and humidity, the results where very pleasing, the AAS sensor having slightly more noise but both well within measurement error.
I would like to compare against calibrated or reference air sample in the future.
What is Next?
Well I have by no means completed the testing I want to do on this kit, it will continue to run in the vehicle for a good while yet. It is also likely that my company will look to buy another set of kit to use in our overseas development centre. Personally I would like to get a case designed and made and have this series of sensors as a standard part of our instrumentation list.
Top Comments
Pleased you like the kit, as you say it is principally designed to evaluate sensors in industrial applications, and is not designed as a product per se, interestingly we are working on something that is…
Very good Road Test Report.
You did a great job of reviewing the device and showing use data over time.
Well written and you clearly made your points about the device and software.
Well done.
DAB
Excellent real world use case.
Well done and your observations about the CO2 level, and dust could be something worthwhile in future cars.
I do like the KISS style mount used.
Mark
-
vannystick
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Comment-
vannystick
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Children