Getting Started With RX23EA, A Solution Starter Kit

View table of contents ...  

RoadTest: Enroll to Review the Renesas Solution Starter Kit for RX23E-A

Author: meera_hussien

Creation date:

Evaluation Type: Connectors & Cable

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: Other part that is comparable to this product is the NXP FRDM-K64F Freedom Development Board

What were the biggest problems encountered?: Not the biggest but the problem which i faced is finding the right resources to get started with the kit since there were a lot of references available.

Detailed Review:

Getting Started With RX23EA, A Solution Starter Kit

Introduction

The Renesas Solution Starter Kit for RX23E-A is an evaluation board that allows you to quickly and easily evaluate the RX23E-A microcontroller. The kit includes the RX23E-A microcontroller, peripheral circuits for sensor measurement, a K-type thermocouple, and a GUI-based PC tool program. This makes it easy to evaluate the measurements of thermocouples, RTD, and strain gauges, which are typical sensors in industrial equipment.

Here are some of the key features of the Renesas Solution Starter Kit for RX23E-A:

  • Evaluation board with RX23E-A microcontroller
  • Peripheral circuits for sensor measurement
  • K-type thermocouple
  • GUI-based PC tool program
  • Easy to evaluate the measurements of thermocouples, RTD, and strain gauges
  • Shortens the development period and brings products to market quickly

Getting Started

Unboxing

To get started, I have referred to the quick start guide. Upon opening the kit, below are the items which I received.

Below are the terminals and jumper on the RSSKRX23E-A board.

Powering Up The Device

To power up this device there are two ways, either using the system power supply or USB Bus Power supply. By default, the power supply setting is "System Power Supply". I have decided to power up the device using the USB Bus Power supply. To achieve this I have followed the following configuration.

 

The table below shows the power selection methods.

Once the jumper is set to this position, the board is ready to power up. But before that, need to download the PC tool program. This program can be downloaded from here. After downloading the file, extract it to a folder and the below files should be listed. Click the file pointed by the arrow in the figure below to launch the PC tool program.

PC Tool Program

During the first try, I could not get any reading even though the connection was successful. Later after some tweaking, I was able to get the reading. The video shows the result.

Conclusion

Overall, I personally feel that this board has a lot of potential to be explored. The test which I have done is merely very little. There are many different types of tests that can conducted using this board for different applications and purposes.

Anonymous