Beaglebone Bundle: BBB, Wireless Cape & Display - Review

Table of contents

RoadTest: Beaglebone Bundle: BBB, Wireless Cape & Display

Author: gsgill112

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: Raspberry Pi 3 With 4.3" LCD HAT

What were the biggest problems encountered?: Unable to get the Wireless Connectivity Cape Working

Detailed Review:

BBB IoT Bundle RoadTest Review

Gurinder Singh Gill

 

NOTE : OFFLINE VERSION AVAILABLE TO DOWNLOAD AS ATTACHMENT

 

Introduction

First of all I want to Thank Element 14 and Ti for selecting me in this wonderful RoadTest.  One fine Morning I got a crushed parcel from Element 14 image Hmm.. I wonder What’s inside ?  

Lets unbox it to see ! Its Element 14 so definitely there may be something interesting image ;P  

 

Unboxing

So unboxing was darn simple, just RIP it apart ;D and as expected some BIG Bubble Wrap image Well thats just what electronics need image 

 

 

imageimageimageimage

 

Getting rid of all the BIG Bubble wrap unfolds three beautiful packages . Its Mesmerising .. .. One Moment please .. .. ..

 

image

OK, so moving forward,   

 

imageimageimage

It was indeed a beautiful unboxing. So, Lets now Focus on the Actual Review image

 

Review will be divided into FIVE (5) subsections :

1. The Beagle Bone Black

2. Wireless Connectivity Cape

3. 4.3” LCD Display Cape

4. Battery Modification to the Black (I am Not Racist !! was referring to the Beagle Bone)

5. Progress update and Video Review

I will cover the rest 2 in a separate Blog !!

 

Beagle Bone Black or just BBB or Black or Bone ##$$@@

Beagle Bone Black is one of the most feature rich SBC’s I came across and has a bunch load of GPIO’s. It is not exactly designed for kids to play with but it is pretty easy to use and have fun with.

 

If you have a Specific project you are working with, be rest assured you can get a million things done just with this SBC without any so called “HATs” (Opps.. I never said anything !).

 

The add-on boards which can extend the functionally to the board are referred to as “Capes” (I am not sure Who thought of a Dog, then Giving him a Bone and then putting a Cape on him sending him to outer space ??? I mean it is a Dog after all $$%%^##@@ WTF !!)

 

Ok, moving on The board is really easy to use for those trying to shove it in your dog’s mouth!! (B.T.W. Don’t Do It !!). Just plug in a USB HUB then plug the Keyboard and Mouse in it and an MICRO HDMI to HDMI Female Connector and then the HDMI cable and finally a 5V Power Adapter and you are all set up image Just like a champ !! After complete Booting (VIDEO LINK) which takes about 80 sec you will be presented with a wonderful LXDE interface to play with image image

 

For those of you who don’t have the MINI HDMI adapter, you can just connect the Ethernet to the Bone and you will have a wonder full Node.JS based Cloud 9 IDE to get started with Bone. <local_ip_addr:3000>

 

The bestsellers in the bone

  • 2 Programmable Realtime Units : They are just High performance RISC Processors running at 200Mhz with 8KB instructions RAM and 8KB Data RAM.
  • 1 GHz ARM Cortex A8 RISC Processor with NEON SIMD Coprocessor 256KB L2 Cache
  • Option for Bare Bone programming using TI SDK & CCS or Linux ports (There are a ton of them)
  • OPEN SOURCE Hardware Design and Software (Not like any of the Pi’s or oranges or banana or OREO’s image ;P )

 

The Not So bestseller in the bone

  • USB and Micro HDMI slots are Extremely near. I have personally shaved plastic from one of the cheep mini to HDMI connector and have barely managed to get them plugged together.
  • Once a Cape is attached, It doesn’t want to come out that easily (Apparently Dogs love Capes ??^^$$## )
  • My Thinking HAT is On ;  Will Update once I find more flaws in the cute DOG imageimageimage

 

Wireless Connectivity Cape

OK , So a Bit Disappointing One..

 

Well The specs of the Cape is like WoW.  But Instructions on How to get it working is like  Errr .. ..

imageimage

CLICK HERE for Specs.

 

As on date I am not able to get the board working !! Few details I can share:

  1. The Board is a power Beast and may consume up to 1.2-2 Amps easily So if you have a standard 5V 2Amp supply .. Get a New Charger rated at least 3Amps.
  2. It is very difficultly to get the board  out as the cuts just perfectly match the Bone’s cutout. So If you plug the cape all the way in bone, It’s gonna stay there for a while !!
  3. Planning to use a Li Battery using the on board PMIC !! Whann Whann Whann imageimage Big NO as the PMIC wont support the power with default configuration.

 

imageimage

 

4.3” Display Cape

OK, So After a Break , I went on with the 4.3” LCD Display Cape. And Damn the display is awesome. It is a 4.3” 470x272 RGB Resolution Display with Capacitive Touch . Yup It has Capacitive touch None of those Resistive Touch Rubbish !!

 

imageimage

image

Moreover It also has an On Board EEPROM with Kit Identity So Bone recognises it like Men recognise Women image image  You just need to plug the Display Cape, Connect the LCD using the connector,Flash the latest Debian IMAGE on to your Bone and You are Good to Go.

 

Click Here for The Full Booting Video

 

Coming to some Details

1. The display is quite Easy on Bone with a current consumption of about An Amp

2. With the Battery solution apparently the Display works just fine wit the PMIC getting a bit Heated but I have ran the system for about an hour on Battery and everything seems to work fine.

3. The Board had some flux residue on the connector pins ??? Hmm.. see Pic below.

imageimage

4. This should have been the first point :: BUT the display connectors are fragile and can break very easily. Plus the connectors on the Interface board is also not reversible so it fits exactly the way in the photos.

5. The display is Manufactured by Rocktech Displays (Pic Below for Part No)

imageimage

6. This Display uses a Ton of GPIO’s and Has Known Issues of WIFI and BLE not working Issues if using in conjunction with the above cape or with Beagle Bone Wireless. It uses the 24 BIT LCD bus

imageimage

Few More Pictures just for fun

 

 

 

So on an Final NOTE It was an Interesting Review and A tone is wet to be done.

A sneak peek of Whats Coming is given Below

 

imageimageimage

 

CLICK HERE FOR THE FULL VIDEO REVIEW

 

REFERENCES :

  1. Getting Started Guide
  2. Beagle Bone 101 Guide
  3. Beagle Bone Black TI PAGE
  4. Beagle Bone Black E14 Page
  5. TI AM335 Datasheet
  6. Beagle Bone Black eLinux Page - You can get all INFO on everything about Bone
  7. My Video Channel
Anonymous
Parents
  • Nice overview, are you going to set it up in an application to show extended use?

     

    DAB

  • YES, My original plan was to have a OnDesk IoT enabled Information Hub, that would be able to control your home devices as well as show meaningful information as widgets on screen. But doe to misfortune of the Wireless connectivity cape not working the plan has delayed, As of now I Have the project on hold as I am out station, will resume working on it next month.

     

    Agenda would be

    1. To get the Basic UI working

    2. Get data from Internet over Ethernet

    3. If possible get everything integrated with WCC

     

    Regards,

    GS Gill

Comment
  • YES, My original plan was to have a OnDesk IoT enabled Information Hub, that would be able to control your home devices as well as show meaningful information as widgets on screen. But doe to misfortune of the Wireless connectivity cape not working the plan has delayed, As of now I Have the project on hold as I am out station, will resume working on it next month.

     

    Agenda would be

    1. To get the Basic UI working

    2. Get data from Internet over Ethernet

    3. If possible get everything integrated with WCC

     

    Regards,

    GS Gill

Children
No Data