Arduino Nano R4 Review

View table of contents ...  

RoadTest: Apply to Test the Arduino Nano R4!

Author: neerajrd82

Creation date:

Evaluation Type: Evaluation Boards

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: STM32F373CCT6,MK40DX256VLK10,ATSAM4LC8C,EFM32GG11B420F2048GL64

What were the biggest problems encountered?: Complete USB failure – Board not detected (no COM port), blocking normal development via Arduino IDE Ineffective standard recovery methods – Bootloader reset and typical Arduino fixes did not work Complex root cause – Clock misconfiguration impacting USB initialization required deep MCU-level analysis Limited low-level documentation – Insufficient clarity on register-level configuration and clock dependencies for debugging such failures Shift to hardware-level debugging – Required use of SWD + J-Link, full chip erase, and reflash to recover the system

Detailed Review:

Section: Unboxing, Initial Setup & Failure Analysis – Arduino Nano R4

image

1. Unboxing & First Impressions

The Arduino Nano R4 was received in standard Arduino packaging with the board securely enclosed in an anti-static cover.

Package Contents:

  • Arduino Nano R4 board
  • Berg strip headers (unsoldered)

Initial Observations:

  • Compact Nano form factor retained
  • High-quality PCB finish
  • Clearly labeled pinout
  • USB Type-C interface for modern connectivity

The inclusion of unsoldered headers allows flexibility depending on application (breadboard vs embedded use).

2. Header Soldering Procedure

To prepare the board for testing, the supplied Berg strip headers were manually soldered.

Tools Used:

  • Temperature-controlled soldering iron
  • Lead-free solder wire
  • Flux (for clean joints)

Procedure Followed:

  1. Headers were aligned with PCB through-holes
  2. Board was placed on a flat surface to maintain perpendicular alignment
  3. Each pin was soldered carefully to ensure:
    • Proper wetting
    • No cold joints
    • No bridging between adjacent pins

image

Result:

  • Clean and mechanically stable solder joints
  • Board ready for breadboard and test setup integration



3. Initial Power-Up & Arduino IDE Detection

After soldering, the board was connected to the system using a USB Type-C cable.

Expected Behavior:

  • Automatic USB detection
  • COM port visibility in Arduino IDE
  • Board ready for programming

Observed Symptoms:

  •  No COM port visible in Arduino IDE
  •  Device shown as “Unknown USB Device” in Windows Device Manager
  •  Upload attempts failed completely
  •  No LED indication of bootloader activity

 At this stage, the board appeared non-functional and inaccessible

4. Initial Diagnosis Using Community Reference

To investigate the issue, the following troubleshooting resource was referred:

  • Element14 Community guide on USB detection issues on this link: 
    https://community.element14.com/products/arduino/b/blog/posts/arduino-uno-r4-minima-troubleshooting-unknown-usb-device

Key Insight:

  • USB failure is commonly caused by:
    • Improper firmware initialization
    • Clock misconfiguration
    • Bootloader not executing

Engineering Interpretation:

Since USB depends on correct timing:

Any misconfiguration in system clock or startup code can completely disable USB communication.

5. Attempt to Restore Bootloader Mode

Method Used:

  • Double-press reset button to force bootloader entry

Expected Outcome:

  • Board should enumerate as a valid USB device
  • COM port should reappear

Actual Result:

  •  Bootloader entry was inconsistent
  •  USB remained unstable or undetected

6. Bootloader Recovery Attempt Using Official Procedure

Next, the official Arduino recovery guide was followed:

  • Arduino Nano R4 Bootloader Flashing Procedure on given link: https://docs.arduino.cc/tutorials/nano-r4/bootloader-flashing/

Intended Goal:

  • Reprogram bootloader
  • Restore USB functionality
  • Re-enable Arduino IDE connectivity

7. Practical Challenges Encountered

 No Active Communication Interface

  • USB stack was non-functional
  • No serial interface available

 Result:

  • Bootloader flashing could not proceed

 Limited Hardware Access

  • No exposed SPI/ISP interface (unlike classic Arduino)
  • SWD/JTAG not readily accessible

 This prevented low-level recovery

 Documentation Limitations

The official guide assumes:

  • Functional USB connection
  • Arduino IDE workflow

It does not fully address:

  • Bare-metal firmware corruption
  • Complete USB failure scenarios

8. Root Cause Analysis

Based on experimentation, the failure was attributed to:

 Clock Misconfiguration

  • Incorrect system clock setup disrupted USB timing

 Bootloader Interference

  • Custom firmware may have overridden bootloader execution

 USB Stack Failure

  • USB requires precise timing → deviation leads to “Unknown Device”

9. Key Engineering Insight

The Arduino Nano R4 behaves like a professional MCU platform, but without equivalent recovery infrastructure.

Parameter Observation
USB dependency High
Recovery ease Limited
Bare-metal tolerance Sensitive
Debug accessibility Restricted

10. Lessons Learned For those Engineers who use Arduino IDE without any other options: 

  • Avoid modifying critical startup configuration without validation
  • Preserve bootloader region
  • Maintain backup firmware


11. Switching over to SWD debug access to recover the target chip R7FA4M1AB3CFM mounted on Arduino Nano R4 board:  

Now, i would like to refer to official schematics of Arduino Nano R4 given on this link: 
https://docs.arduino.cc/resources/schematics/ABX00142-schematics.pdf

image
Here are 3 important observations about above picture are given below required for SWD bebug access: 

1. MD pin of MCU given on JP1 connector pin no 13. -> This pin should be connected with SWCLK pin of debugger.

2. RESET pin of MCU given on JP2 connector pin no 3. -> This pin should be connected with RESET pin of debugger.  

3. VUSB pin of MCU given on JP1 connector pin no 12 -> This pin should be given +5VDC from debugger USB power supply.  
image

Here are some important observations about above picture are given below required for SWD bebug access: 

1. P108_SWDIO & P300_SWCLK are required to connected with any compatible debugger -> Jlink / CMSIS-DAP / Renesas made Emulator  

2. Very-very important point :  P300_SWCLK & MD pin of MCU given on JP1 connector pin no 13 should be shorted with each other & connected to SWCLK line from debugger side.  

Again by chance, i already possess this evaluation kit made by renesas: 

image  

This board already have onboard Jlink OB lite debugger mounted on this kit. So, i decided to connect this debugger to Arduino Nano r4 while totally disconnecting on board target chip. 

Now, referring to schematics of this kit which are found in ek-ra2l1-v1-designpackage.zip , these are important points everybody needs to consider for connections given below: 

Please! download ek-ra2l1-v1-designpackage.zip from Renesas website.

Now, given below is important section of debugger to get connected with external target chip  

 


image 

Important Note: all jumpers shown in this diagram needs to taken out totally, to cut off the onboard target chip for debugger connections.

 image

J13 connector shown above is not populated in actual kit, so all the connector pads are exposed which were directly soldered for debugger connection with Arduino Nano r4 board. 

image

In above picture, 5V power supply can be easily seen which was connected with Arduino Nano R4 board to get power up using debugger USB power supply. 

J-link Commander after getting correct connection from debugger will give below message corresponding to Arduino Nano R4 board:  

Device "R7FA4M1AB" selected.

Connecting to target via SWD
InitTarget() start
Identifying target device...
SWD selected. Executing JTAG -> SWD switching sequence...
Initializing DAP...
DAP initialized successfully.
Low power mode detected. Waking device from low power mode.
InitTarget() end - Took 14.5ms
Found SW-DP with ID 0x5BA02477
DPIDR: 0x5BA02477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x24770011, ADDR: 0x00000000)
AP[1]: APB-AP (IDR: 0x44770002, ADDR: 0x01000000)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Found Cortex-M4 r0p1, Little endian.
FPUnit: 6 code (BP) slots and 2 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7
[0][1]: E0001000 CID B105E00D PID 003BB002 DWT
[0][2]: E0002000 CID B105E00D PID 002BB003 FPB
[0][3]: E0000000 CID B105E00D PID 003BB001 ITM
[0][4]: E0040000 CID B105900D PID 000BB9A1 TPIU
[0][5]: E0041000 CID B105900D PID 000BB925 ETM
[0][6]: E0042000 CID B105900D PID 002BB908 CSTF
[0][7]: E0043000 CID B105900D PID 001BB961 TMC
[0][8]: E0044000 CID B105F00D PID 001BB101 TSG
Memory zones:
Zone: "Default" Description: Default access mode
Cortex-M4 identified.

So, SEGGER J-FLASH LITE was able to program Arduino Nano r4 board successfully, below picture demonstrates that:  


 image

So, SEGGER J-FLASH LITE was able to erase Arduino Nano r4 board successfully, below picture demonstrates that:  

image

 

I m showing the picture of actual physical connections with debugger & Arduino Nano R4 board given below: 
 

image


Important observation noted: I was able to recover original preloaded program which was actually loaded in Arduino Nano R4 at time of arrival using jlink debugger. 

12. Switching over the development of  target chip R7FA4M1AB3CFM mounted on Arduino Nano R4 board from Arduino IDE into Keil MDK ARM :  

Here you have to use Renesas smart configurator with Output configured for Keil MDK ARM.

Select the clock settings given below in Renesas smart configurator in given screenshot: 

image

Select Board : Custom User board (Any Device) as shown in screenshot given below: 

image

Pin function select is shown in given screenshot :


image

BSP options are shown in  below screenshot:

image

In bsp options, just select bare metal & No RTOS to include. Also select "Generate Project option" option to generate Blinky program in this configurator as shown below:

image

Below given picture demonstrates the output given by Renesas smart configurator for Keil MDK ARM: 

 image

To run this program correctly, Please! do the following steps: 

Search & comment  this line given below: 

FSP_HARDWARE_REGISTER_WAIT(R_RTC->RCR2_b.RESET, 0);   -> This line is found in bsp_clocks.c

Important observation: Debugger gets stuck on above line. 

Update on 31/03/2026: 

Keil screenshot on C/C++ tab: 

image

Keil screenshot on Asm tab:

image
 

Keil screenshot on Linker tab:

image

Configure the below settings in Flash download of keil as shown screenshot given below: 

image 

Apply the above settings, then follow the below given steps:


Generate the hex file.

Completely erase the chip.

Then program the chip using download button in keil.

Expected result: You should be able to RGB LED as single white LED glowing brightly but without blinking.

Now, after resolving settings issues, renesas flash programmer is also working, screenshots are given below: 

image

Programming messages by Renesas Flash Programmer are given below: 

Loading File (E:\Arduino-nano-r4\led.hex) CRC-32=8D56F9F1

Target device : RA

Connecting the tool
J-Link Firmware: J-Link OB-S124 compiled Dec 10 2025 15:52:46
Tool : J-Link (SEGGER J-Link-OB-S124), Interface : SWD
Connecting to the target device
Connecting to the target device
Communication speed : 6.0 MHz
Signature:
Device: RA
Device Code: 00160447

Erasing the selected blocks
[Code Flash 1] 0x00000000 - 0x0003FFFF size : 256 K
[Data Flash 1] 0x40100000 - 0x40101FFF size : 8 K

Erasing the selected blocks
[Code Flash 1] 0x00000000 - 0x0003FFFF size : 256 K
[Data Flash 1] 0x40100000 - 0x40101FFF size : 8 K

Writing data to the target device
[Code Flash 1] 0x00000000 - 0x0003FFFF size : 256 K
[Data Flash 1] 0x40100000 - 0x40101FFF size : 8 K
[Config Area 1] 0x01010008 - 0x01010033 size : 44

Verifying data
[Code Flash 1] 0x00000000 - 0x0003FFFF size : 256 K
[Data Flash 1] 0x40100000 - 0x40101FFF size : 8 K
[Config Area 1] 0x01010008 - 0x01010033 size : 44
Setting the target device

Disconnecting the tool
Operation completed.

Important observation: This tool should be used to production programming rather than for development.   

 

13. Build the whole project in keil bypassing Renesas smart configurator   

 If you do not want to use code generated by Renesas smart configurator -> then it is still long learning curve, but some how i managed to reduce the number of files to taken from smart configurator & managed to write in register direct format. Also i have followed the steps given just above this section.

End result of above exercise is shown below screenshot: 

image    

Of course, result was fabulous: I was able to blink RGB LED & AMBER LED independently bypassing the HAL library as mandated by Renesas.

Final Verdict: 


When the Arduino Nano R4 loses USB functionality due to low-level firmware issues, recovery becomes complex and not be achievable using standard Arduino tools alone.

It requires the assistance of JLINK/ CMSIS DAP / Renesas EMULATOR to recover from all types of firmware issues.

Also this board requires the erase of whole chip to prevent the hang-up. 

The Arduino Nano R4 delivers powerful Renesas-based performance, but its recovery mechanisms need significant improvement to support advanced embedded development workflows.

Renesas flash programmer is not reliable at all, it does not connect with Jlink reliably to sense the chip. 

There is steep learning curve for bare metal development on register direct access bypassing HAL layer by Renesas.

Renesas needs to improve on all these parameters. 

MY SINCERE THANKS FOR ELEMENT 14 Community to give me to chance to test the arduino nano R4 board.   

Anonymous
Parents
  • Hi,

    thank you for your fine review.

    This helps me a lot, if I have troubles with my own Nano R4.

    You use the Keil MDK ARM, (item 12):

    can I use the community, free version as well, or do I need the full version?

    Best Regards 

    Gerald

    --- 

Comment
  • Hi,

    thank you for your fine review.

    This helps me a lot, if I have troubles with my own Nano R4.

    You use the Keil MDK ARM, (item 12):

    can I use the community, free version as well, or do I need the full version?

    Best Regards 

    Gerald

    --- 

Children