RoadTest: RoadTest Review a Raspberry Pi 3 Model B !
Author: gpolder
Creation date:
Evaluation Type: Independent Products
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: The Pi rules!
What were the biggest problems encountered?: an old NOOBS card from a Pi B (not the B+) didn't work.
Detailed Review:
The topic I promised to discuss in my roadtest application is heat dissipation related to use of the Pi 3 for home automation.
There were some rumors on the net that the processor temperature can be as high as 100 degrees celsius at 100% CPU.
Currently I'm running an home automation system using a Pi 2 model B, which controls the lights in the house, measures temperature and also a connected camera detects intruders.
For monitoring the system itself I have a temperature sensor in the cabinet and also monitor the CPU temperature.
Here is a picture of the webpage which shows me the graph of the current month:
You will see the temperature of the power supply (green), the case itself (purple) and the CPU (top one).
You can see that it follows the ambient temperature, including day/night rhythm.
So I was curious about the heat transmission is om the Pi 3. I saw some tests on the internet who states that the CPU under 100% load can go higher than 100 degrees celsius. (http://www.gizmodo.com.au/2016/03/the-raspberry-pi-3s-quad-core-cpu-can-hit-a-toasty-100c-under-load/ )
For home automation I don't need a lot of computing performance, while power dissipation is much more important.
First I did a CPU test using sys bench, on three types of the Raspberry Pi, my current home automation system (Pi 2), a Pi B+, and the Pi 3 from the roadtest.
Here is a picture of the Pi B+ (left) and Pi 3, laying on my desk.
sys bench can be installed using: sudo apt-get install sysbench
For monitoring the temperature I used RPiTemperature from: http://www.roylongbottom.org.uk/Raspberry_Pi_Stress_Tests.zip
wget http://www.roylongbottom.org.uk/Raspberry_Pi_Stress_Tests.zip unzip Raspberry_Pi_Stress_Tests.zip cd Raspberry_Pi_Stress_Tests/ chmod +x RPiTemperature ./RPiTemperature passes 700, seconds 2 &
Here is the result of sys bench on all three boards. Of course I know that --num-threads=4 doesn't make much sense on the Pi 2 and Pi B+, but I don't expect it influences the results a lot.
pi@zolderpi ~/stres_test $ sysbench --num-threads=4 --test=cpu --cpu-max-prime=20000 --validate run
sysbench 0.4.12: multi-threaded system evaluation benchmark
Running the test with following options:
Number of threads: 4
Additional request validation enabled.
Doing CPU performance benchmark
Threads started!
Done.
Maximum prime number checked in CPU test: 20000
Test execution summary:
total time: 1329.8390s
total number of events: 10000
total time taken by event execution: 5318.6407
per-request statistics:
min: 351.47ms
avg: 531.86ms
max: 1132.11ms
approx. 95 percentile: 551.17ms
Threads fairness:
events (avg/stddev): 2500.0000/0.00
execution time (avg/stddev): 1329.6602/0.13sysbench 0.4.12: multi-threaded system evaluation benchmark
Running the test with following options:
Number of threads: 4
Additional request validation enabled.
Doing CPU performance benchmark
Threads started!
Done.
Maximum prime number checked in CPU test: 20000
Test execution summary:
total time: 293.8832s
total number of events: 10000
total time taken by event execution: 1175.3010
per-request statistics:
min: 117.00ms
avg: 117.53ms
max: 160.74ms
approx. 95 percentile: 118.04ms
Threads fairness:
events (avg/stddev): 2500.0000/11.02
execution time (avg/stddev): 293.8253/0.04
pi@pi1pi3test ~/stress_tests/Raspberry_Pi_Stress_Tests $ sysbench --num-threads=4 --test=cpu --cpu-max-prime=20000 --validate run
sysbench 0.4.12: multi-threaded system evaluation benchmark
Running the test with following options:
Number of threads: 4
Additional request validation enabled.
Doing CPU performance benchmark
Threads started!
Done.
Maximum prime number checked in CPU test: 20000
Test execution summary:
total time: 246.9762s
total number of events: 10000
total time taken by event execution: 987.6050
per-request statistics:
min: 96.08ms
avg: 98.76ms
max: 214.33ms
approx. 95 percentile: 97.46ms
Threads fairness:
events (avg/stddev): 2500.0000/54.59
execution time (avg/stddev): 246.9012/0.02
During the tests I logged the temperature with a 2 seconds interval and plotted the results using plot.ly. Below you will see the results.
I also made some thermal images when running the tests simultaneously on the Pi B+ (left) and the Pi 3 laying on my desk.
My conclusion is that I continue to use the Pi 2 for my home automation, and use the Pi 3 for more demanding tasks, such as software defined radio.
During my experiments A Comprehensive Raspberry Pi 3 Benchmark was added to Element14 by cstanton
I hope my findings above will contribute a little bit to that.
Do not hesitate to contact me when you have some questions.