By Invitation Only - Minode Kit - Review

View table of contents ...  

RoadTest: STEM micro:bit - Minode Kit

Author: lorrainbow

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?:

What were the biggest problems encountered?: There is no simple how-to guide on how to use this kit.

Detailed Review:

The mi:node kit is a really attractive looking kit. Each sensor has it's own slot in the box and the colour scheme is colourful and friendly.

 

It comes with a small booklet but this doesn't specify where to go to find out more. The element14 page that sells the kit also doesn't have any links to lesson plans or code blocks.

A quick google gives you a comprehensive booklet from Farnell: http://www.farnell.com/datasheets/2551715.pdf?_ga=2.160216059.7971154.1520321820-521448588.1473107271

It's really thorough but not very child-friendly. I think a non-computing parent would be pretty stuck on what to do with this kit without ideas/sample projects to look at.

 

The sensor boards could do with some more formatting. On the back of each board, it says the name of it. But in some cases, this isn't obvious what it does, e.g. DHT11 ??

On the front of the light sensor it has a switch - what does the switch do?!

 

Also, some boards only go into specific slots of the connector board - this could have been specified on them as well as in the booklet.

 

There's a lot to do with this kit. Plenty of sensors and outputs to play with. It comes with:

  • Light Sensor
  • Speaker
  • Temperature and Humidity Sensor
  • Sound Sensor
  • Mini Fan
  • Relay
  • Rotary Angle
  • PIR Motion Sensor
  • Switch
  • RGB LED
  • Orbit Fan
  • DC Motor

 

Kids love the mini fan. When it starts, they just get so excited!

 

All the sensors can be easily slotted into the connect board and a micro:bit also slots easily into the middle of the board. The whole setup is very neat and compact. It comes with plenty of connecting wires to connect multiple devices. It also comes with a micro USB cable which is very useful. Physically, it's very easy to use.

 

This is a brilliant kit for young children and novices with no electronics skills. The connectors are very easy to use and are really solid. It would be difficult to break one. It's great that someone with no electronic skills can use all of these sensors without having to wire them up/add resistor/use a breadboard.

 

The only sensor I don't like is the Relay. With no example projects, this looks like a pointless connector! You can use it to control high voltage devices but that's not clear in the kit and obviously, one is not included!

 

Using the kit I made the following:

- the fan turns on when the temperature went over a certain level

- the speaker makes a noise when the sensor is breached

- the RGB light comes on when it gets dark

 

As I'm familiar with the micro:bit and can do programming I was able to create these using the farnell guide above. If you're a programmer but know nothing about electronics you'd really like this kit. It really needs a more user-friendly guide for schools with example projects.

 

 

Cost wise:

While there are a lot of parts to the kit I don't think the price reflects the value for money. It's very expensive. It doesn't include a micro:bit so that's an added expense.

Anonymous
Parents
  • Essentially, I agree with DAB. To be honest, I am not a judge but expressing my personal opinion it is not a road t st at all. Inacceptable because I think impossible:

    • That you never read a product review somewhere else
    • That you was not able to make some photos of what you have done, at least with a smartphone
    • That you have never read, at least bcause curious, how roadtest here are done
    • That you have not read the plenti of recommendations on how to make and write a road tto st and what is the minimum required to do so

    frankly this is a very sad result, IMHO

    Enrico

Comment
  • Essentially, I agree with DAB. To be honest, I am not a judge but expressing my personal opinion it is not a road t st at all. Inacceptable because I think impossible:

    • That you never read a product review somewhere else
    • That you was not able to make some photos of what you have done, at least with a smartphone
    • That you have never read, at least bcause curious, how roadtest here are done
    • That you have not read the plenti of recommendations on how to make and write a road tto st and what is the minimum required to do so

    frankly this is a very sad result, IMHO

    Enrico

Children
No Data