We’re giving away 5 BBC micro:bits! - Review

View table of contents ...  

RoadTest: We’re giving away 5 BBC micro:bits!

Author: dougw

Creation date:

Evaluation Type: Independent Products

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: N/A

What were the biggest problems encountered?: The only problem was the micro:bit introduction was delayed by months, so the road test device was not available for months.

Detailed Review:

After about a nine month suspenseful wait for a micro:bit to arrive, I finally get to test one for myself.

The BBC micro:bit is a phenomenal initiative to introduce youngsters to the world of electronics and computing. I would love to see the initiative spread to other countries, like Canada, where I live.

In this road test / review I would like to do a little engineering analysis and explain how to interface the micro:bit to other electronics.

But first a few comments on the significance of this platform as a free give-away to students.

Back in 1981 the BBC commissioned development of the BBC Micro for the BBC Computer Literacy Project and it eventually made its way into about 80% of schools in the UK due to a 50% procurement subsidy from the government. This initiative was a phenomenal success in launching UK students into the computer era. It even has a fairly direct connection to development of ARM technology which is so ubiquitous today.

The BBC micro:bit launching this year, with the goal of providing a free micro:bit to every 7th grade student in the UK, is intended to help address the expected severe shortage of technical expertise in the near to medium future. It is a spectacularly forward thinking initiative that is sure to have far reaching and positive consequences.

The table below compares the capabilities of the BBC micro:bit to the original IBM PC and the original BBC Micro.

CategoryIBM PC (1981)BBC Micro (1981)BBC micro:bit (2015)
Size1,760 cubic inches, 25 lbs.439 cubic inches0.5 cubic inches, 0.018 lbs.
Power120 v. AC, 63 Watts220VAC < 50Watts3V DC, 0.1 W
CPU8/16 bit, 8088, 4.77 MHz8 bit, 6502A, 2 MHz32 bit ARM CortexM0, 16 MHz
Memory40K ROM, 16K RAM 32K ROM, 16K RAM128 K FLASH, 16 K RAM
SoftwareBIOS, DOS, BASICBBC BasicTouchDevelop, uPython,
JavaScript, Block Editor
DisplayMonochrome
- 25 lines x 80 char
External monitor 11.5" screen, (17 lbs. 2,310 cubic inches)
640 x 256 x 8 colours
External monitor/TV
25 LEDs, external terminal
SensorsExternal IBM 83 key keyboard74 key keyboard
3 buttons, 3 axis accelerometer,
3D magnetometer
Non-volatile memory 5¼" diskette drive
160KByte/disk, 20Kbits/s
300 Baud cassette
Tape ~ 100 Kbytes
128 Kbyte Flash, 256 Mbits/s
CommunicationsRS-232C, 115.2 KbaudRS423, 19.2KbaudUSB, Bluetooth, > 2 Mbaud
Price$1565 ($4100 today)
(£2644 today)
£235 (£764 today)
Free

 

Clearly the micro:bit is a platform with extensive computing potential and the shear number of them will ensure many great applications get developed for it.

I think it would be interesting to port BBC Basic to the micro:bit to perform a more direct comparison.

I had designed some interfaces for the micro:bit 8 months ago based on information available at the time. Some of the documentation has changed since then, so be careful when using old information on this product.

Here is an unboxing video to get started with the road test:

The micro:bit is a nice pocket sized computer, but perhaps a little fragile for pocket transport. Maybe your first project should be to make a protective case for it.

Next just a quick note about making the LEDs a bit more legible for some applications:

The next video shows the demo firmware that comes installed on the micro:bit:

Before getting into programming, I want to show how to create a low cost breadboard interface:

Here is a demonstration of the breadboard interface in action:

Now lets try programming. I am using microPython for micro:bit because it looks like it provides better support for SPI and I2C.

The microPython development environment is nice and simple - type in some code and click on the Flash button and the code automatically compiles, downloads and runs.

Here is my first program:

image

And here it is running:

For my second program I wanted to show the magnetometer sensor in action so I loaded a compass program:

image

And here it is running:

Back to more applications - programming with the breadboard:

Here is a program to toggle a pin on the micro:bit connector:

image

And here is the program running:

The micro:bit is a lot of fun to play with, the simple development environment and built-in hardware allow interesting programs to be tried out without a huge learning curve.

It may take some time before I get a Bluetooth 4 app running as none of my Bluetooth devices have BLE, but I intend to explore this capability.

There is a lot of power under the hood and I expect some of these modules will end up in amazing applications.

Thanks to element14 for the opportunity to explore the technology behind this bold educational experiment.

Anonymous
Parents
  • What happens if you place the anti-static bag under the disposable dinner board?

    Would it give the same results without the reflection?

  • It doesn't help much to put the dark material under the white material although it does make it a bit harder to see the "off" LEDs. The purpose of dark material is to provide high contrast to the LED light. The white material reflects ambient light which reduces contrast between it and the LED light. You can see in some of my videos that the ambient light can reflect off the white surface and "wash out" the LED light. This is exaggerated because of the bright movie lights I use.

    Red LED displays often use dark red translucent acrylic filters. They are so dark, they appear black. There is nothing red on the circuit card, so the meager portion of red light from ambient white light that gets through to the circuit card does not reflect back out to be visible, however the translucent red allows LED light through just fine. Unfortunately, I don't have a sample of such material.

  • used automotive tape that's sold to temporarily fix break lights.

Comment Children
No Data