Microchip SAML10/11 Xplained Pro Evaluation Kits - Review

View table of contents ...  

RoadTest: Microchip SAML10/11 Xplained Pro Evaluation Kits

Author: sparkytau

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: I imagine it would be similar to the KL82Z from NXP, and similar to the TI SimpleLink platform (minus the network connectivity)

What were the biggest problems encountered?: Finding proper documentation (my fault I'm sure), keeping track of which pin was which. I also had issues with getting the IDE to work, but I suspect that was a conflict with other development tools I had on that machine.

Detailed Review:

Before I begin, I’d like to thank the element14 and those involved in the Road Test for allowing me to do a run through of the SAML10/L11 Xplained Pro platform.  Secondly, I need to apologize. The author of this amazing review at the time of this writing had a very interesting month- an incident with a broken water pipe, dead cell phone, toasted laptop, fried logic analyzer (and oscilloscope) kind of left me in a bit of a pickle.    Most of the photos, code, logs and pretty screenshots I had were unfortunately lost in my re-creation of the Great Flood….

For what it is worth, I ran the L10 through its paces and was able to get it to perform really quite well with very little optimization on my part  The first ‘real’ project I ran on it was a classic of mine, a stress test of the UART and SPI lines, recording data from an external device to a SD card.  The test went beautifully and was dramatically faster than what I was used to (Granted, this is my first ARM microcontroller) and used dramatically less energy than I anticipated for the task.  It was by far the winner as far as performance, energy use and temperature of the uC, but alas, the photos, setup and results were lost, as well as the first (extremely well written) version of this review.  As a man of science I can not expect you to take my word for any of this.  That being said, I was able to recover some bits and pieces and tried to do the best I could with what time I had left.  Annnddd now back to the review...

 

I typically like to start these sorts of test drives/reviews with a quick introduction and unboxing, just so that we are all on the same page.  I’ve worked with just about every computer system out there (Amiga, Solaris, AS/400, Windows, MacOS… you get the idea). I have spent a good part of my professional life in IT and in embedded hardware design.  I started with the glorious PIC MCU’s, later I moved onto the Motorola/Freescale 86HC line, did a bit with the ATMega series, and as of late have been working a lot with the TI MSP430 platform. The SAML series is, therefore, my introduction into the world of ARM.

As far as unboxings go, this has been a pretty uneventful, as there was nothing in the box but the board, the antistatic sleeve it came in and a shipping manifest.  There was a lot of wasted space, but not the worst example I've seen.  I was slightly disappointed that it didn’t at least come with a USB cable (granted I have more than I know what to do with), or a business card that pointed to the documents/software needed.  image

 

image    imageimage

 

The differences between the two are fairly minor if you are not using the security features of the L11, the 30 second version is reflected below:

image

image

To save you some time as it took me longer than I would like to admit, here are the documents that were most helpful for me:

The quick start guide is here:

http://ww1.microchip.com/downloads/en/AppNotes/Getting-Started-with-SAM%20L10L11-Xplained-Pro-DS00002722A.pdf

          The SAM L10/L11 Xplained Pro User Guide was also invaluable:

http://ww1.microchip.com/downloads/en/DeviceDoc/70005359B.pdf

          Also a requirement whenever working with any chip (at least for me…) the data sheet:

http://ww1.microchip.com/downloads/en/DeviceDoc/SAM-L10L11%20Family-DataSheet%20-%20DS60001513B.pdf

 

Once I had AtmelStudio installed and running, then I really off to the races.

 

image

It was quite nice to see the IDE automatically recognize the device and load the related components.

As you can see there are plenty of example projects just waiting to be played with.  A slight disappointment that several of the examples require expansion boards that are required to go through all of the examples, but it is understandable.

As a side note, it appears there is a pretty significant conflict between the first two development machines I was using and the Atmel studio config, so I was forced to spin up a new development machine specifically for this test.  For reference, the system I was finally able to get AtmelStudio 7 to run on was a Windows 7 x64 box that had no built in serial ports. I suspect strongly that this is not AtmelStudio’s fault, but rather a conflict from other development tools that I frequently use.  I also ran into quite a few issues with AtmelStart downloading the files it needed to configure the projects, however I suspect this was related to the CenturyLink issues that were going on nationwide at the time.

image

image

 

I pretty quickly ran through several examples to get a feel for the board and the programming environment and although not intuitive at first, I picked it up easily enough, but I will say there are quite a few features that I am quite excited about but alas, due to the Great Flood I was not able to document or complete as many development runs through as I would have liked.  Of particular interest for me are the following features:

    • UART Bootloader- for fun in the field upgrades with only a serial connection
    • Chip level security- keep nasties from messing with my code!
    • Crypto accelerators (AES, SHA and GCM) - much easier and more secure to implement SHA/AES than writing algorithms from scratch
    • Secure key storage
    • TRNG
    • On dev board current measurement

 

Here is the part where I did all that work with the L10 but lost all evidence of it ;-(  I did find that the L10 performed quite well, I was amazed at the performance it had even when operating under very low power conditions (sleepwalking is awesome!)

 

This time, however I wanted to play with the TRNG on the L11- so that’s exactly what I did.  I set up the L11 to generate random numbers and send them across the serial line to my PC, and once I got enough of them, I ran them through an analyser just to see for myself.

  From the datasheet:

    • Passed NIST Special Publication 800-22 Tests Suite
    • Passed Diehard Random Tests Suite
    • May be used as Entropy Source for seeding an NIST approved DRNG (Deterministic RNG) as required by FIPS PUB 140-2 and 140-3
    • Provides a 32-bit random number every 84 clock cycles

 

I generated 12 megs of random data and started the heavy duty testing-  I tried compressing the file with 7zip- and it did nothing for it (which is good!) 

image

 

And then I got serious and ran it through the ent program from https://fourmilab.ch/random/

And was quite pleased with the results:

Entropy = 7.999986 bits per byte.

Optimum compression would reduce the size of this 12582912 byte file by 0 percent.

Chi square distribution for 12582912 samples is 241.53, and randomly would exceed this value 71.83 percent of the times.

Arithmetic mean value of data bytes is 127.5136 (127.5 = random).

Monte Carlo value for Pi is 3.139747620 (error 0.06 percent).

Serial correlation coefficient is -0.000329 (totally uncorrelated = 0.0).

 

I’d say that it passes the test.  I've attached the random data for your own eval should you decide to take a peek

 

**********UPDATED****************

Evidently I didn't put quite enough detail into these, so hopefully this is more satisfactory...

 

In summary:

Kudos:

  • Boards do exactly what they say they do, and I’m excited to start using this series of uC’s in my new projects.
    • Call me jaded if you must, but I've had many in the past that were not up to what their spec sheets read.  I may just be unlucky, but I've lost count of the number of dev kits that claim they can do something but fail to live up to their own spec sheets.
  • Board is manufactured incredibly well, nice and clean solder joints, sharp lines on the silkscreen. - I've had dev kits from other companies that came in looking like they were assembled by a 3 year old buzzing from large doses of Mountain Dew
  • Atmel START
    • This is really a hidden gem.   Very quick and easy to get framework going for the platform without nearly as much mess as piecing together example code snippets.  I know other vendors have similar tools, but its integration into AtmelStudio was quite surprising.  
  • The IDE is Visual Studio under the hood, so it is a bit more bloated than what I typically ran in the past, but it performs quite well and is actually enjoyable to use.
  • Sleepwalking rocks
    • This goes back to my incident with the broken pipe- I have no hard data unfortunately to share, but its capabilities are quite exciting and even without my data, I couldn't stay silent on it. 
  • The hardware RNG puts out very nice random data
    • Over the years I've dealt with many random number generation systems, and most of them are just "adequate" - as there is no test to prove it is random, (see  https://dilbert.com/strip-2001-10-25/  ) it is nice to see that the data coming off of it has very good test results with high entropy.    Typically I've used avalanche noise as a root source for random numbers when needed, but even that can be problematic depending upon conditions.  For a chip built with security in mind, this should be a requirement, but sadly many of the 'secure' designs don't include TRNG.      

Gripes:

  • Board itself shipped without a cable or even a quick start card pointing to docs (minor gripe)
  • Header pin out silkscreen is on the bottom of the board which made wiring things up interesting (Plenty of room on the front of the board for the silkscreen)
  • Expansion boards are relatively expensive to show off features of the chip- perhaps could include some of these on the board itself (it wouldn’t have been too difficult to put the I/O1 on the same board for instance as there is plenty of unused space on the PCB)

    • Aren't these dev kits supposed to show off the chip by default?   Maybe I've just missed the mark on this one...
  • No built in networking support
    • Truthfully this is one of the biggest downfalls.  In the IoT space, it is difficult to have a IoT device without the 'I'.   Yes, there are add-ons, and a number of ways to connect it, but there are single chip solutions available that do have onboard support for networking.
  • Broken pipes suck and are quite expensive.
    • I pray this is self explanatory enough...
Anonymous
Parents Comment Children