PSoC® 6 WiFi-BT Pioneer Kit (CY8CKIT-062-WIFI-BT) - Review

Table of contents

RoadTest: PSoC® 6 WiFi-BT Pioneer Kit (CY8CKIT-062-WIFI-BT)

Author: MARK2011

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?:

What were the biggest problems encountered?: Kitprog firmware update issues (described in RT below); Necessity of install at least two large programming suites (disc capacity issue) Lack of BT or TFT examples for particularly PSoC6 WiFi BT Kit

Detailed Review:

Thank you Cypress, thank you Element 14 for providing me not only very interesting equipment:Cypress PSoC6 WiFi-BT Pioneer kit

but also opportunity to deal with fascinating nevertheless quite challenging project.

 

 

 

The PSoC 6 board is a low-power programmable system dedicated to developers of modern IoT systems.

Learning its parameters and features we may become overwhelmed by such a small and powerful tool.

But don't worry - good documentation, instructions and manuals accompanied with many examples

together with active as well as helpful Cypress support / community forum will never let you get lost.

On the other hand - programming, using PSoC creator or Wiced Studio is relatively demanding.

In that (IDE) case advertised "Arduino compatibility" would not work.

 

I planned to write some details about features later but let me emphasize most interesting components of the kit:

  • 4GHz WLAN & Bluetooth functionality module ( WiFi + Bluetooth combo chip) which opens the "doors" to the world of IoT

image

  • 4” TFT display handy and useful.

 

And  invitation to create many incredible projects using additional sensing environment:

  • Capacitive sensing slider, buttons and proximity header
  • Motion sensor
  • Ambient light sensor

Maybe you think about audio related projects:

  • 32-bit audio codec
  • PDM microphone

last not least...

  • Headers compatible with Arduino 3.3V Shields and Digilent Pmods

 

The story starts from quick unboxing

The kit is delivered in safe and elegant box.

image

If you ask for quality of delivery and packing I'm glad to confirm the best ranks.

The USB “C” standard has been appreciated by Cypress which seems to be quite handy nowadays!

The USB cable is 1m long.

 

image

The mainboard and TFT module are delivered coupled.

If you hoped to start the adventure with PSoC6 from reading of paper manuals you may be disappointed but I'm sure all of us

are accustomed and confirm lack of paper documentation provided together with equipment.

not that there was nothing - Convenient and quality guide is attached

image

CY8CKIT-062-WiFi-BT PSoC® 6 WiFi-BT Pioneer Kit Quick Start Guide.pdf

A little funny thing are wires accompanied the kit.

image  jumper  and proximity wires

Although that hardware lags behind a little from remaining parts of the kit it's  not a bad idea to support some DIY conventional projects.

My question is did you Cypress wanted to keep the right balance between wired and wireless (WiFi+BT etc..) technologies?

 

Soon  after plugging  the kit greets us invited to explore the implemented onboard demo CE222494

image

But let me tell about it later.

 

At the beginning I want to summarize some basic names types and markings as we have it mixed a little.

 

Basic signings:

full name:

CY8CKIT-062-WiFi-BT

PSoC 6 WiFi-BT Pioneer Kit

 

other names used

Cypress PSoC6 WiFi-BT Pioneer kit

PSoC6 Pioneer Kit CY8CKIT

 

Main components:

CY8CKIT-062-WiFi-BT Board

CY8CKIT-028-TFT Display Shield

 

the heart of that beast is

CY8C6247BZI-D54  Cypress PSoC 6 MCU

 

I promised myself not to copy or multiply datasheets wide available on the net

the summary of parameters and features of the kit is well described and available on Cypress site.

But let me present only:

Kit Features

PSoC 6 WiFi-BT Pioneer Kit:

  • PSoC 62 MCU with up to 1MB Flash, 288KB SRAM, and 104 GPIOs
  • Murata LBEE5KL1DX Wi-Fi/BT combo module
  • On-board 512Mb QSPI NOR Flash Memory
  • EZ-PD™ CCG3 USB Type-C Controller with Power Delivery
  • CapSense touch slider, buttons and proximity sensor
  • On-board debugger/programmer (KitProg)
  • Arduino UNO v3 headers
  • Digilent Pmod interface
  • CY8CKIT-028-TFT shield board with:
    • 2.4-inch TFT display
    • Ambient light sensor
    • 6-axis motion sensor
    • PDM-PCM microphone

Remaining informations are easy available in:

Most important papers

Below - documentation I found most convenient and I used mostly:

CY8CKIT-062-WiFi-BT_Kit_Guide.pdf  (rev.E)

CY8CKIT-062-WiFi-BT_Quick_Start_Guide.pdf

PSoC 6 Brochure.pdf

 

AN210781 Getting Started with PSoC 6 MCU with Bluetooth Low Energy BLE Connectivity.pdf

AN219434 Importing PSoC Creator Code into an IDE for a PSoC 6 Project.pdf

AN213924 - PSoC 6 MCU Device Firmware Update Software Development Kit Guide.pdf

 

KitProg2_User_Guide.pdf  (Document Number: 002-10738)

 

All available at cypress site:

Cypress.com Kit Resource Page

https://www.cypress.com/documentation/development-kitsboards/psoc-6-wifi-bt-pioneer-kit-cy8ckit-062-wifi-bt

Cypress Programming Solutions

https://www.cypress.com/products/psoc-programming-solutions

 

or on the GitHub:  PSoC-6-MCU-Getting-Started

https://github.com/cypresssemiconductorco/PSoC-6-MCU-Getting-Started

 

32-bit Arm® Cortex®-M4 PSoC® 6

https://www.cypress.com/products/32-bit-arm-cortex-m4-psoc-6

 

 

And great help online:  Cypress Developer Community Page

with great support for PSoC 6 MCU

https://community.cypress.com/community/psoc-6

Software

PSoC Creator IDE

https://www.cypress.com/products/psoc-creator-integrated-design-environment-ide

image

PSoC Programmer

installs all components required for a programming and debug solution.

equipped with following additional tools

  • Clock Programmer
  • Bridge Control Panel is a simple debugging tool

 

WICED Studio SDK

https://www.cypress.com/products/wiced-software

image

WICED Studio Wi-Fi/Combo Docs and Downloads

https://community.cypress.com/community/wiced-wifi/wiced-wifi-documentation

Cypress PSoC 6 ModusToolbox

https://www.cypress.com/products/modustoolbox-software-environment

Honestly - not used yet but seems to be more and more required...

 

KitProg

KitProg is Cypress’ low-level communication firmware for programming and debugging - not available as a separate product.

Programming tools listed above use a KitProg. Cypress development kits have KitProg firmware installed, and so “just work” with supported IDEs.

After installation of the most recent programs, the KitProg2, is available

To get most recent (KitProg3 in my case) you need to initialize the upgrading.

 

All necessary documents, instructions basic examples as well as required software can be downloaded as an ISO image.

The content of DVD image:  CY8CKIT-062-WiFi-BT Kit ISO (Create CD)  (1,19GB)

image


image

I have decided to burn that disc but I don’t recommend it.

All of the disc content covers above described software and documents which is available and easy/ clear to find and download (fresh - most recent version)

Download packages variants:

CY8CKIT-062-WiFi-BT Kit Only: This executable file installs only the kit contents, which

include kit code examples, hardware files, and user documents. This package can be used if all the software prerequisites (listed in step 3) are installed on your PC.

CY8CKIT-062-WiFi-BT Kit Only Package (Kit Design Files, Documentation, Examples)  (33,1MB)

 

CY8CKIT-062-WiFi-BT Kit Complete Setup: This installation package contains the files

related to the kit including PSoC Creator, PSoC Programmer, and PDL. However, it does not

include the Windows Installer or Microsoft .NET framework packages. If these packages are

not on your computer, the installer will direct you to download and install them from the

Internet.

CY8CKIT-062-WiFi-BT Kit Complete Setup (Kit Design Files, PSoC Creator, PSoC Programmer, Documentation, Examples)    (568.65MB)

 

Talking about software I can't omit just another group of applications:

Cypress Semiconductor Inc. mobile applications

Yes: for any interested in development of BT projects, Cypress release free mobile apps:

image

https://play.google.com/store/apps/details?id=com.cypress.cysmart

OkładkaCySmart

https://play.google.com/store/apps/details?id=com.cypress.cypressblebeacon

OkładkaCypress® BLE-Beacon

https://play.google.com/store/apps/details?id=com.cypress.app.wicedsense

OkładkaWICED Sense

 

Examples and blogs worth to look at:

 

PSoC 6 MCU Code Examples

https://www.cypress.com/documentation/code-examples/psoc-6-mcu-code-examples

Materials are available on both Cypress "root" site or on its Github repositories

PSoC 6 MCU Device Related Designs

https://github.com/cypresssemiconductorco/PSoC-6-MCU-Device-Related-Design

 

Code example repos for ModusToolbox software (in my case - field of further experiments).

https://github.com/cypresssemiconductorco/Code-Examples-for-ModusToolbox-Software

 

Very valuable courses were prepared in "Cypress Academy"

I followed well presented webinars at:

Cypress Academy:Online Video Training and Tutorials from Cypress:

https://www.cypress.com/training/free-online-video-training-and-tutorials-cypress

Courses are accompanied with files needed to conduct examples from  "Cypress Academy PSoC 101"

https://github.com/cypresssemiconductorco/CypressAcademy_PSoC101_Files

 

And here let me for some complaining... one of (not a little) examples of my bad luck:

CE218138 – PSoC 6 MCU with BLE Connectivity: BLE Thermometer (RTOS)

Very interesting subject, fruitful from the point of view of learning PSoCs features

but unfortunately not for my WiFi-BT kit:

After some attempts to adapt it to run it on my (062 WiFi- BT) kit I found definitely confirmation that following statement is absolutely right:

"If you want to just use BLE, and want to use PSoC Creator then I suggest you get the CY8CKIT-062-BLE.

 

 

unfortunately above concerns most fine examples for PSoC kits.

I'm honestly disappointed that many BT examples I wanted to use/ learn/ modify, are dedicated to the BLE kit only!

 

 

Testing

I honestly admit, I decided to follow the instructions from getting started leaflet,

without special preparation and software installation.

The beginning wasn't smooth as I hoped …

After connecting to the USB driver installation started but soon I got:

image

it must have been driver mismatch!

image

???? 

lets find the solution: searching the "kitprog usbuart" sentence directed me soon at:

https://community.cypress.com/thread/20596

 

also looking for similar issues and the proposals of solution:

“Please re-install the PSoC Programmer from: <http://www.cypress.com/products/psoc-programming-solutions>.”

 

after install PSoC Programmer and plug in the device:

image

!!!!!!!!!!!!!!!!!!! OK!!!!!!!!!!!!!!!!!!!!

 

image

image

 

In the new "virtual" E folder I found the file:

STATUS.TXT with following content:

Cypress KitProg2 v1.05 Mass Storage Programmer.

Click the mode switch button to exit or enter Mass Storage mode.

NOTE: Only PSoC 4/6 Families are supported in this version. Dragging and dropping of a HEX

file shall trigger the programming of the target device. In case of an incorrect HEX file or a

programming error, firmware of the target device shall be erased.

Target device:CY8C6247BZI-D54

STATUS: Ready to be programmed with HEX file.

 

 

Now lets review the installation ofl

PSoC Programmer & KitProg

According to above links to Cypress software:

image

image

 

 

The file

image

 

During Installation I’ve just followed default options:

 

image

image

image

image

 

 

image

 

image

Help > About PSoC Programmer :

Installed CyInstaller Products:

Bridge Control Panel  1.20.0.4174

Clock Programmer  1.9.0.4174

Device Database  4174

Example Code  4174

PSoC Programmer  3.28.3.4174

USB Bootloader Application  4174

 

OK - looks fine it works now!

one important comment:

plug the dev board into the host PC before launching the programmer, and then the virtual drive should appear in the Port Selection box automatically.

 

After start of the Programmer the warning pops-up

The request of the firmware  update!

image

Sometimes I encountered memory mismatch errors FAIL (above)

The solution is to press "load from device"

image

 

image

DEVICE was recognized and works properly:

image

One thing is strange!

image

Is the kit really out of date.? Should I ask Cypress to get a replacement?

 

some messages from the programmers console:

 

KitProg2 (CMSIS-DAP/1B0B0EDD02197400)

Automatically Detected Device: CY8C6247BZI-D54

 

Device set to CY8C6247BZI-D54

1048576  FLASH bytes

Device Family set to CY8C62xx

Memory Types Load from HEX Requested

Active HEX file set

 

Port Opened with Warnings      KitProg2 firmware in CMSIS-DAP mode is detected.

 

Device Family set to CY8C62xx

Automatically Detected Device: CY8C6247BZI-D54

Silicon: 0xE206, Family: 0x100, Rev.: 0x22 (*B)

SROM Firmware: 2.01, Flash Boot: 1.0.1.20 (*B)

Protection state: 0x02 (NORMAL), Life Cycle stage: 0x01 (NORMAL)

 

KitProg3

According to the previous warning lets move to KitProg3

But simple run of upgrade isn’t available offhand

image - that “button” is grayed - unavailable!!!!

 

According to instructions - when  “Upgrade Firmware button is greyed out”,

It means, KitProg2 “is not in the right mode

- push the mode switch button (SW3)

image

- Then the Upgrade Firmware button will become available and you can click on it to update the firmware.

imageimage

But in my case that didn’t work

I tried to find the solution at the Cypress Community forum. That thread was quite informative for me:

https://community.cypress.com/message/196350#196350

 

Then I tried again: according to “KitProg2_User_Guide.pdf”

5.1 Enter or Exit the Mass Storage Programmer Mode

Follow these steps to enter or exit the Mass Storage Programmer mode of KitProg2:

1. Connect the kit to the PC. Ensure that the amber status LED is ON and not blinking.Amber status LED ON indicates that the current configuration is KitProg2 Programmer and Debugger.

2. Press and release the mode switch within two seconds. The KitProg2 re-enumerates as a MassStorage Programmer/CMSIS-DAP programmer if the previous configuration is PPCOM programmer and debugger.

The amber status LED stops glowing indicating that the kit is in Mass Storage

Programming/CMSIS-DAP programming mode.

3. The KitProg2 remains in the selected mode until you change the mode manually using the modeswitch. To exit the Mass Storage Programming mode, press and release the mode switch within two seconds.

The amber status LED is continuously ON, indicating that the KitProg2 is in theKitProg2 Programmer and Debugger mode.

 

image

 

BTW I decided to change firmware using:

“PSoC 6 MCU KitProg Firmware Loader”

“Another method is to use fw-loader.exe tool to switch between KP2 and KP3. 

BTW, please make sure the SW3 onboard is switched to correct mode for programming.”

I downloaded the loader from github:

https://github.com/cypresssemiconductorco/Firmware-loader

Fw-loader-2.1.0.52-windows.zip

In the folder bin\firmware I had file “version”:

1.10.2946

then following instructions:

first you need to get your kit out of "CMSIS-DAP HID" mode.  To do this, you press SW3 on your board.

After pressing that button, status LED 2, right below the SW3, should go from OFF (which I hope it is now) to ON.

Now, you should be able to run fw-loader --update-kp3

 

image

 

C:\PSOC 6\bin>fw-loader --device-list

Cypress Firmware Updater, Version: 2.1.0.52

(C) Copyright 2018-2019 by Cypress Semiconductor

All Rights Reserved

Info: Start API initialization

Info: Connected - KitProg3 CMSIS-DAP HID-1B0B0EDD02197400

Info: Hardware initialization complete (686 ms)

Error: Error =  Cannot open Hid device with the path: \\?\hid#vid_04b4&pid_f154&

mi_00#8&1e90080e&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}

Connected supported devices:

        1: KitProg3 CMSIS-DAP HID-1B0B0EDD02197400

First I couldn’t manage to run fw -updateproperly

But playing with SW4 SW3 at last let to work:

 

C:\PSOC 6\bin>fw-loader --update-kp3

Cypress Firmware Updater, Version: 2.1.0.52

(C) Copyright 2018-2019 by Cypress Semiconductor

All Rights Reserved

 

Info: Start API initialization

Info: Connected - KitProg3 CMSIS-DAP HID-1B0B0EDD02197400

Info: Hardware initialization complete (811 ms)

Device 'KitProg3 CMSIS-DAP HID-1B0B0EDD02197400' opened successfully

Info: Kit FW is 'KitProg3' ver. 1.01 b158.  Upgrade file is 'KitProg3' ver. 1.10

b2946. Upgrade file contains a Custom App.

Info: Disconnected - KitProg3 CMSIS-DAP HID-1B0B0EDD02197400

Info: Connected - KitProg Bootloader-1B0B0EDD02197400

Info: Bootloader Version: Major 1, Minor 1, Build 40

Info: FW Upgrade to version: 1.10 b2946. Upgrade of Custom App

Info: Bootloading of Custom App...

Info: Verifying of Custom App...

Info: Bootloading of KitProg FW...

Info: Verifying of KitProg FW...

Info: Upgrade completed

Info: Disconnected - KitProg Bootloader-1B0B0EDD02197400

Info: Connected - KitProg3 CMSIS-DAP HID-1B0B0EDD02197400

FW update completed successfully

 

 

The first, most funny is the message from PSoC programmer:

Port Opened with Warnings KitProg3 version Expecting 1.01.158, but found 1.10.2946.

image

and... my bad luck - I had auto-upgrade selected thus my "hard work" with obtaining most current version was lost…

Run the PSoC Programmer with autoupdate option downgraded 'KitProg3'  to ver. 1.01 b158!!!!

Successfully Connected to

KitProg3 (CMSIS-DAP/BULK/1B0B0EDD02197400)

KitProg3. CMSIS-DAP Version 2.0.0. Firmware Version 1.01.158. Hardware Id 02.

 

I realized that v1.01.158 is a bit...lame... Lack of DapLink support, unclear  ... or faulty ... functionality of SW3 (mode selection)

I have Important remark

KitProg3 with version 1.01 b158 couldn’t provide the mass storage - downloading the firmware through the virtual drive! DAPLINK didn’t work!

SW4 switched off the program, it let me say “bricked” the board. Both running code and programming was unavailable. Status LEDs 1-3 blinked.

That state was strange, didn’t fit any description from instructions.

I realised, thanks to cypress community forum, that I’m not alone with similar problems:

“After change from KitProg2 to  KitProg3 fw - unable enter into CMSIS-DAP mode with mass storage. there is no mass storage device with kitprog3 fw.

When I press SW3 (mode select) to enter into CMSIS-DAP mode nothing happened except com port is changed from COM0 to COM1. And also the LED2 which is supposed to be turned off

When I use kitprog2 fw everything works perfectly.

Is there any other solution except downgrading to KitProg2 FW?

>>>The KP3 does not cover mass storage mode any more. This mode has been transferred under DAPlink.”

 

That situation forced me to the second attempt...

After disabling auto-upgrade

image

I installed v1.10.2946 again using fw-loader --update-kp3

 

I started to enjoy the new tool. Easy availability of three modes: CMSIS-DAP Bulk +  CMSIS-DAP HID + DapLink delights indeed!

 

 

I could see the change of COM:

image

image

Changing the mode (SW3) I could switch between COM33 - COM34

KitProg is visible in the  Device Manager too

image

image

 

 

Also new : in the folder:

C:\Cypress\Programmer

New  hex files:

image

 

Lets explain the SW3 function:

It switches

CMSIS-DAP HID/CMSIS-DAP BULK modes

 

After upgrade with firmware v1.10.2946 mode selection works fine

In the state  SW3 BULK (with status LED 2 constantly lighting) I got:

C:\PSOC 6\bin>fw-loader --device-list

Cypress Firmware Updater, Version: 2.1.0.52

(C) Copyright 2018-2019 by Cypress Semiconductor

All Rights Reserved

 

Info: Start API initialization

Info: Connected - KitProg3 CMSIS-DAP BULK-1B0B0EDD02197400

Info: Hardware initialization complete (842 ms)

Connected supported devices:

        1: KitProg3 CMSIS-DAP BULK-1B0B0EDD02197400     FW Version 1.10.2946

SW3 - state BULK 

KitProg3 (CMSIS-DAP/BULK/1B0B0EDD02197400)

image

 

Switching SW3 into HID  - status LED 2 “ramp”

Disconnected KitProg3 (CMSIS-DAP/BULK/1B0B0EDD02197400)

Connected KitProg3 (CMSIS-DAP/HID/1B0B0EDD02197400)

image

 

C:\PSOC 6\bin>fw-loader --device-list

Cypress Firmware Updater, Version: 2.1.0.52

(C) Copyright 2018-2019 by Cypress Semiconductor

All Rights Reserved

 

Info: Start API initialization

Info: Connected - KitProg3 CMSIS-DAP HID-1B0B0EDD02197400

Info: Hardware initialization complete (639 ms)

Connected supported devices:

        1: KitProg3 CMSIS-DAP HID-1B0B0EDD02197400      FW Version 1.10.2946

 

It is important to emphasize, that KitProg3 doesn’t support anymore the virtual mass storage feature!

image

 

But now after update the FW and KitProg3 working properly, using SW4 I can enter the mode of  virtual drive DAPLINK

image

Successfully Connected to CMSIS-DAP/248484 CMSIS-DAP Version 1.10

image

 

Works!!!

Although the beginning was frustrating a little:

image

…it was temporary

 

No errors in Device Manager

 

image

image

It is recognized as

image

image

image

 

Folder E content changed:

DETAILS.TXT

# DAPLink Firmware - see https://mbed.com/daplink

Unique ID: 19000000dd0e0b1b02ddxxxxxxxxxxxxxxxxx

HIC ID: 2e127069

Auto Reset: 0

Automation allowed: 1

Overflow detection: 1

Daplink Mode: Interface

Interface Version: 0251

Git SHA: 0ceae64926c06bf4481xxxxxxxxxxxxxxxxx

Local Mods: 0

USB Interfaces: MSD, CDC, HID, WebUSB

Interface CRC: 0xab8e0b36

Remount count: 0

URL: https://mbed.org/device/?code=19000000dd0e0b1b02dd0e0b00000000000000002e127069?version=0251?target_id=@T

 

But nothing is ideal!!!

I cant upload Some projects via virtual drive

 

Now I realized, that attempts of upload of selected firmware, using mass - storage (DapLink) fails:

FAIL.TXT

error: The hex file cannot be decoded. Checksum calculation failure occurred.

type: transient, user

As I wrote above: only selected, some .hex were accepted, remaining rejected...

These binaries came from tested, successful build and were accepted when programming directly from PSoC Creator or WICED

.hex files "generated" using PSoC Creator are fine - I could program PSoC taking these files

and using mentioned above PSoC Programmer.

the "company": PSoC Programmer+ PSoC Creator + my .hex files in my opinion seems to be correct.

I suppose we should focus on PSoC board+DapLink when looking for the solution.

 

I'm afraid I need some fine-tuning around DapLink driver etc. but presently no idea what to fix...

 

That question was answered on Cypress community:

“I tested the "Drag-and-Drop Programming" feature of DAPLink mode just now, and found that the hex files

generated by PSoC Creator are invalid to be used under DAPLink mode.

You have to use mbed to generate the required hex files. I guess there are some differences between the file formats.

Just follow the steps shown in the part "Getting Started with Mbed OS" of the following link - PSoC 6 BLE Pioneer Kit | Mbed

 

Additionally:

In the  DAPLINK mode in the Folder E I found MBED.HTM

It directs to:

https://account.mbed.com/login?state=g6Fo2SBDc1pFaFp6d3VpN3JXWUxsbk5HcXI5ZFgtdUg1Y1M3daN0aWTZIE82UWtLUlJJLUNfejBmZ2FlZTg0MlM4TGZSb0sycjlho2NpZNkgb28zaWJvNHlnSXc1ZVRQamFnM1FJcGpkZ2pBY25ZNmg&client=oo3ibo4ygIw5eTPjag3QIpjdgjAcnY6h&protocol=oauth2&prompt=true&nonce=N6xZXvHGcis42rUSYHlcikrerKsnRyebxR5CMwbBIqNy4jvabDKVvMOZ37MEkiDr&redirect_uri=https%3A%2F%2Fos.mbed.com%2Fcomplete%2Fmbedopenid%2F&response_type=code&scope=openid%20profile%20email

image

The license key from your board will be transferred to your account. This will give you access to compiler tools for the following board:

I tried to run it

image

But unsuccessfully:

image

 

OK I decided to leave that issue for now.

 

PSoCCreator - installation

No comments - no issues  - just simple installation:

image

image

image

At that moment I decided to leave updates untouched.

image

 

PSoC Creator ready to (hard) work

image

 

 

UPDATE Manager

image

To be up-to date I had to install following PDL’s one by one...

image

image

Remaining software didn’t  ask for facelift.

 

Another necessary tool is

WICED-Studio

Simple comment from community forum: 

If you are looking to use PSoC 6 + WiFi then yes you must use WICED. There is no support for WiFi in PSoC Creator.

If you are looking use the BT/BLE features of the 4343W (Murata 1DX module) on the CY8CKIT-062-WiFi-BT then again you must use WICED.

 

image

 

image

 

Well another eclipse-based suite, another gigabytes taken…

Microchip, Matlab, Ti Composer, Digilent - Cypress add next 2 IDEs.

It's a pity we can’t use one “engine” for different programming environment.

 

Just only select the proper platform and we are ready to conduct our project.

image

Wait, one more

ModusToolbox

There are no plans to add WiFi support to PSoC Creator. The plan is to integrate PSoC and WiFi functionality into Cypress' new tool ModusToolbox

http://www.cypress.com/products/modustoolbox-integrated-design-environment-ide

Modus is a cross platform eclipse based IDE. It will provide tools to easily configure the PSoC peripheral and add in WiCED WiFi support.

https://community.cypress.com/community/modustoolbox/blog/2019/03/31/mbed-part-2-importing-a-code-example-from-the-cypress-modustoolbox-code-example-github-repository

As I said at the beginning, although I haven’t used it yet but that tool seems to be more and more required...

First WiFi program demo:

Let’s move some steps back to experiments with primary (onboard)  DEMO firmware.

The board already came with the WiFi-BT demo program preloaded. Demo helps to understand usage of implemented WiFi capabilities with both AP + client features

as well as simple usage of TFT module and impressing CapSense buttons/ slider.

It worked fine, following short instruction I successfully ran it

Following screens depicts progress of that exercise.

Initial screen of the TFT

image

AP recognized

image

image

 

Unfortunately using the PC I faced some issues related to connection errors:

image

image

image

 

I took the smartphone to try establish the connection and it work

image

 

image

image

 

 

image

 

192.168.0.31

 

image

CE222494 PSoC 6 WICED™ WiFi Demo

 

image

According the instruction, the demo program control the LED brightness by PPM, tuned using CapSense slider. Additionally light sensor readouts are presented.

The recorder

Another code example dedicated to The PSoC 6 WiFi-BT Pioneer Kit can be simply developed using PSoC Creator. CE222221 is available from  Start > Kits on the PSoC Creator Start Page.

 

image

 

According to instruction, file update should be deselected!

I forgot that remark, which caused errors:

image

image

image

 

Acting according to instruction let me successfully  compile the project

 

image

Another important settings in our workspace:

image

image

That project uses RTOS thus right memory management settings must be selected

 

After successful build  hex file is delivered:

C:\PSOC 6\examples kopie\Firmware\PSoC 6 MCU\CE222221\CE222221_Voice_Recorder.cydsn\CortexM4\ARM_GCC_541\Debug\

image

The Kit is converted now into the cute voice recorder with RECORD; PLAY; PAUSE features available with CapSense buttons and volume controlled with slider.

 

Then I tried to use another interesting demo project

CE225248 – PSoC 6 MCU RGB Display Interface

That example uses  EmWin Graphics library and Quad SPI FRAM as Display Buffer

To be prepared better to conduct that experiment I read about CapSense-based designs: https://community.cypress.com/docs/DOC-9249

and about similar example: PSoC 6 TFT Display Interface with EmWin Graphics Library

https://www.cypress.com/documentation/code-examples/ce223726-psoc-6-tft-display-interface-emwin-graphics-library

 

Trying to keep instructions:

 

make sure the file is not selected (it is deselected by default),

 

image

 

I thought I have success:

--------------- Build Succeeded

But soon I meet the sad reality:

main_cm4.c:14:17: fatal error: GUI.h: No such file or directory

compilation terminated.

The command 'arm-none-eabi-gcc.exe' failed with exit code '1'.

 

According to instruction

“Peripheral Driver Library (PDL) 3.0.4 or higher”

Must be set:

image

Some necessary fittings in project files:

LCDConf.c

/* Physical display size */

#define XSIZE_PHYS          240 //320

#define YSIZE_PHYS          320 //240

/* Virtual display size */

#define VXSIZE_PHYS         240 // 320

#define VYSIZE_PHYS         340 // 240

 

#define DISPLAY_DRIVER  GUIDRV_FLEXCOLOR //GUIDRV_TEMPLATE

 

Run “Generate application”

 

image

 

code:434496    sram:38820

Build Succeeded

Programming device 'PSoC 62 CY8C6247BZI-D54 (CM4)' with file 'C:\PSOC 6\examples kopie\Firmware\PSoC 6 MCU\CE225248_DisplayBuffer01\CE225248_DisplayBuffer01.cydsn\CortexM4\ARM_GCC_541\Debug\CE225248_DisplayBuffer01.hex'.

Device ID Check

Erasing of Main Flash...

Programming of Flash Starting...

Protecting...

Verify Checksum...

Finished Programming

Device 'PSoC 62 CY8C6247BZI-D54 (CM4)' was successfully programmed

 

 

????? Program run but I got nothing but the white screen !!!!!

Ok - I have already got used to - just another example of lack of good support for WiFi-BT board  - the example was as usual for the BLE version of the kit…

 

Disappointed a little I moved to exploration of WICED IDE

The most simple exercises based on the use of “download run” targets.

WICED Studio IDE projects

I started with “Demo  download run in WICED Studio IDE”

According to short instruction for snip.scan example I followed:

Right-click 43xxx_Wi-Fi in the Make Target window and click New.

image

image

Double-click the Clean Make Target to remove any output from the previous build.

It is recommended to do Make clean when any new files are added or removed to the corresponding Target.

image

Note from the manual: “Before executing the next step, ensure that you connect the CY8CKIT-062-WiFi-BT kit to the PC, ensure that the kit is successfully enumerated and Port Selection is set to CMSIS-DAP mode.

Double-click the snip.scan-CY8CKIT_062 to build and download it to the CY8CKIT-062-WiFi-BT.”

image

 

The project is built and programmed into the CY8CKIT-062-WiFi-BT

 

Build Finished (took 1m:9s.14ms)

 

With  KitProg3 the mode HID should be selected!

Programming using WICED I encountered problems when PSoC programmer was running parallely!

 

Let's check the results in serial terminal:

Remember right baud rate!

image

image

image

 

Works fine how about next simple exercise?

snip.apsta

snip.apsta-CY8CKIT_062 download run

 

I decided to make changes to avoid conflict with router address

apsta.c :

static const wiced_ip_setting_t ap_ip_settings =

{

    INITIALISER_IPV4_ADDRESS( .ip_address, MAKE_IPV4_ADDRESS( 192,168,  9, 1 ) ), //192,168, 0, 1

    INITIALISER_IPV4_ADDRESS( .netmask,    MAKE_IPV4_ADDRESS( 255,255,255,  0 ) ),

    INITIALISER_IPV4_ADDRESS( .gateway,    MAKE_IPV4_ADDRESS( 192,168,  9, 1 ) ), //192,168, 0, 1

};

 

Build results:

TOTAL (bytes)           | 279384 | 55796 |

Build Finished (took 9m:33s.520ms)

 

 

Results in the Terminal:

 

Starting WICED vWiced_006.002.001.0002

Platform CY8CKIT_062 initialised

Started ThreadX v5.8

Initialising NetX_Duo v5.10_sp3

Creating Packet pools

WLAN MAC Address : DC:EF:CA:A8:B3:00

WLAN Firmware    : wl0: Apr 30 2018 04:14:19 version 7.45.98.50 (r688715 CY) FWID 01-283fcdb9

WLAN CLM         : API: 12.2 Data: 9.10.39 Compiler: 1.29.4 ClmImport: 1.36.3 Creation: 2018-04-11 22:31:21

0000 00:00:00.000 wiced logging system is initialized

Joining : SSID

Successfully joined : XXXXXXX

Obtaining IPv4 address via DHCP

DHCP CLIENT hostname WICED IP

IPv4 network ready IP: 192.168.0.40

Setting IPv6 link-local address

IPv6 network ready IP: FE80:0000:0000:0000

0001 00:00:09.940 Pinging 192.168.0.1 3 times every 1000ms with a 900ms timeout.

IPv4 network ready IP: 192.168.9.1

Setting IPv6 link-local address

0002 00:00:10.942 Ping #0 Reply : 2 ms

0003 00:00:11.941 Ping #1 Reply : 1 ms

0004 00:00:12.941 Ping #2 Reply : 1 ms

IPv6 network ready IP: FE80:0000:0000:0000

0005 00:00:12.961 softAP "WICED Soft AP" is up

0006 00:00:13.941 Ping #3 Reply : 1 ms

0007 00:00:13.941 deregister ping timer

image

And again I had to use smartphone - PC didn't want to connect to the new AP

"WICED Soft AP

image

 

 

0008 00:05:07.868 http response stream callback, received 486 bytes

0009 00:05:07.868 data:

GET / HTTP/1.1

Host: 192.168.9.1

Connection: keep-alive

Accept: text/html,application/xhtml+xml,application/xml;q=0.9,image/webp,*/*;q=0.8

Upgrade-Insecure-Requests: 1

User-Agent: Mozilla/5.0 (Linux; U; Android 6.0.1;XXXXXXXXXXXXXXXX

Accept-Encoding: gzip, deflate

Accept-Language: pl-PL,en-US;q=0.8

X-Requested-With: com.opera.mini.native

 

 

 

 

According to my plans, I’m sure I will employ PSoC to work in my Smart Home Project.

As the very beginning I checked handy example for control application:

Home Appliance Control Application

First make the target:

demo.appliance-CY8CKIT_062  download run

 

Starting WICED vWiced_006.002.001.0002

Platform CY8CKIT_062 initialised

Started ThreadX v5.8

Initialising NetX_Duo v5.10_sp3

Creating Packet pools

WLAN MAC Address : DC:EF:CA:A8:B3:00

WLAN Firmware    : wl0: Apr 30 2018 04:14:19 version 7.45.98.50 (r688715 CY) FWID 01-283fcdb9

WLAN CLM         : API: 12.2 Data: 9.10.39 Compiler: 1.29.4 ClmImport: 1.36.3 Creation: 2018-04-11 22:31:21

IPv4 network ready IP: 192.168.0.1

Setting IPv6 link-local address

IPv6 network ready IP: FE80:0000:0000:0000:DEEF:CAFF:FEA8:B300

After entering 192.168.0.1 and delivering LAN access data

AP was removed

image

And in the terminal:

 

Joining : mySSID

Successfully joined : SSID

Obtaining IPv4 address via DHCP

DHCP CLIENT hostname WICED IP

IPv4 network ready IP: 192.168.0.40

Setting IPv6 link-local address

IPv6 network ready IP: FE80:0000:0000:0000:

 

Using above IP

I started web application

image

Pushing button we send commands by UART

imageimage

********************************************************************************************************

For those who want to learn console usage with PSoC the next example would be interesting:

test.console

Target looks as follows:

test.console-CY8CKIT_062 download run

Downloading resources filesystem ... build/test.console-CY8CKIT_062/filesystem.bin at sector 1  size 96...

Downloading apps lookup table in wiced_apps.mk ... build/test.console-CY8CKIT_062/APPS.bin @ 0x0000 size

Downloading Application ...

Download complete

 

Resetting target

Target running

Build complete

Making .gdbinit

Build Finished (took 10m:7s.291ms)

 

Starting WICED vWiced_006.002.001.0002

Platform CY8CKIT_062 initialised

Started ThreadX v5.8

Initialising NetX_Duo v5.10_sp3

Creating Packet pools

WLAN MAC Address : DC:EF:CA:A8:B3:00

WLAN Firmware    : wl0: Apr 30 2018 04:14:19 version 7.45.98.50 (r688715 CY) FWID 01-283fcdb9

WLAN CLM         : API: 12.2 Data: 9.10.39 Compiler: 1.29.4 ClmImport: 1.36.3 Creation: 2018-04-11 22:31:21

Console app

 

Then I went to the UART terminal

And tested few commands:

> start_ap myssid wpa2 password  6

IPv4 network ready IP: 192.168.0.1

Setting IPv6 link-local address

IPv6 network ready IP: FE80:0000:0000:0000:

 

> iperf -s -u

------------------------------------------------------------

Server listening on UDP port 5001

Receiving 1470 byte datagrams

UDP buffer size: 12.1 KByte (default)

------------------------------------------------------------

Spawning a listener.

 

> iperf -c 192.168.0.136 -u -S 0xE0 -t 90 -b 10M

------------------------------------------------------------

Client connecting to 192.168.0.136, UDP port 5001

Sending 1470 byte datagrams

UDP buffer size: 12.1 KByte (default)

------------------------------------------------------------

[ ID] Interval       Transfer     Bandwidth

[  0] 0.0-90.0 sec   107 MBytes 10.0 Mbits/sec

[  0] Sent 76534 datagrams

[  0] WARNING: did not receive ack of last datagram after 1 tries.

 

I tried to use another example of the target

but audio_loopbac example was not ksupported:

audio_loopback application does not support CY8CKIT_062 platform.  Stop.

 

CE222494 PSoC 6 WICED™ WiFi Demo - again

But now - let’s create it in the WICED Studio IDE

 

Above examples wasn’t very demanding to implement

Demo CE222494 is more tricky. To build the project some import/export between default folders were necessary.

For the  WICED WiFi-SDK our working directory is “43xxx_Wi-Fi”

Folders from the PSoC creator default folders (two directories called apps and resources)

image

Should be copied into WICED-Studio-6.1\43xxx_Wi-Fi\

image

image

As previous we need to put new Target Name in the Make Target window demo.CE222494_PSoC6_WICED_WiFi-CY8CKIT_062 download_apps download run

image

image

image

 

simple?

Making demo.CE222494_PSoC6_WICED_WiFi-CY8CKIT_062.bin

                                  |                                     | Static |

              Module              |  Flash  | RAM   |

App                               |    4922 |    1176 |

crc                               |    1060 |       0 |

device_configuration              |    3609 |      20 |

DHCP_Server                       |    1460 |     132 |

DNS                               |    2048 |      44 |

DNS_Redirect_Daemon               |     718 |       0 |

HTTP_Server                       |    3946 |       8 |

Interrupt Vectors                 |     652 |       0 |

libc                              |   32892 |    3368 |

Linked_List                       |     466 |       0 |

mbedTLS                           |  111926 |      88 |

Networking                        |    6030 |   13912 |

NetX-Duo - Interfaces & Stacks    |       0 |      16 |

NVRam                             |     640 |       0 |

Other                             |   93179 |    7625 |

Packet Buffers                    |       0 |   22470 |

platform                          |    3908 |     736 |

RAM Initialisation                |    4372 |       0 |

resources                         |   59611 |       0 |

Ring_Buffer                       |     160 |       0 |

Simple_HTTP_Server                |    1034 |       0 |

SNTP                              |     712 |      96 |

SPI_Flash_Library_CY8CKIT_062     |    1088 |     352 |

Startup Stack & Link Script fill  |     147 |      29 |

Supplicant - BESL                 |    7581 |     864 |

ThreadX                           |    8744 |     400 |

TLV                               |     214 |       0 |

ugui                              |    8052 |       4 |

WICED                             |    6006 |    1076 |

Wiced_RO_FS                       |     568 |       0 |

WWD                               |   18645 |    3208 |

----------------------------------+---------+---------|

TOTAL (bytes)                     |  380018 |   55624 |

Download complete

Resetting target

Target running

Build complete

 

What can we see in the serial terminal (115200)

 

Starting WICED vWiced_006.002.001.0002

Platform CY8CKIT_062 initialised

Started ThreadX v5.8

Initialising NetX_Duo v5.10_sp3

Creating Packet pools

WLAN MAC Address : DC:EF:CA:A8:B3:00

WLAN Firmware    : wl0: Apr 30 2018 04:14:19 version 7.45.98.50 (r688715 CY) FWID 01-283fcdb9

WLAN CLM         : API: 12.2 Data: 9.10.39 Compiler: 1.29.4 ClmImport: 1.36.3 Creation:     2018-04-11 22:31:21

*******************************************************

Using another device connect to the following WiFi network

SSID    :  WICED Config

Password:  12345678

Open a web browser and go to  http://192.168.0.1

On the page click the Wi-Fi Setup button. Select your WiFi network

type in the password, press connect

*******************************************************

IPv4 network ready IP: 192.168.0.1

Setting IPv6 link-local address

IPv6 network ready IP: FE80:0000:0000:0000:

 

Program works as described at the beginning of that RT.

 

After that success I tried to adapt that  “flagship" demo to have possibility to communicate with the initial AP from my PC.

I wanted to simply modify of initial IP address of PSoC (used when it starts and temporary works as the AP).

By default we have 192.168.0.1. I intend to play with last figures.

I tried to dig a little in the codes to find that phrase...  but honestly i feel lost until now

I found a lot of instances which appear to be the target of modification…

 

C:\Users\____\WICED-Studio-6.2\43xxx_Wi-Fi\apps\demo\wifi_onboarding\wifi_onboarding.c

C:\Users\____\WICED-Studio-6.2\43xxx_Wi-Fi\libraries\utilities\connection_manager\connection_manager.c

C:\Users\____\WICED-Studio-6.2\43xxx_Wi-Fi\libraries\daemons\device_configuration\device_configuration.c

C:\Users\____\WICED-Studio-6.2\43xxx_Wi-Fi\libraries\daemons\DHCP_server\unit\dhcp_server_unit.cpp

C:\Users\____\WICED-Studio-6.2\43xxx_Wi-Fi\libraries\utilities\command_console\wifi\command_console_wifi.c

INITIALISER_IPV4_ADDRESS( .ip_address, MAKE_IPV4_ADDRESS( 192,168,  0, 1 ) ),

 

Which one is correct? Is there one definition of that address?

I couldn’t find it…

Just to avoid some obvious questions: The purpose of that silly modifications...

Is just the conflict with the router I use (I was too lazy to change its default address…)

 

The only proposal I get was to go to testing a simple AP function, using snip\apsta,

That works of course, after modification of the right file

 

image

But I couldn’t adopt it in the DEMO project.

Thus my wish to modivy AP in PSoC 6 WICED WiFi Demo is still an open question.

 

 

Find code example

Then I checked demo projects from  “Find code example”

image

Hello world

image

image

“This example uses the Cortex-M4 (CM4) CPU of PSoC 6 MCU to execute two tasks: UART communication and LED control.

At device reset the Cortex-M0+ (CM0+) CPU enables the CM4 CPU.

The CM4 CPU uses UART Component to print a “Hello World” message in a UART terminal emulator and when the Enter Key is pressed by the user, the LED on the PSoC 6 MCU WiFi-BT Pioneer Kit starts blinking.”

 

First I had to import(download) the demo clicking the internet icon next to the example name.

image

image

Some hasitations but I decided to leave it as default

image

 

 

image

image

image

image

Now I moved to the UART terminal

 

image

After pressing ENTER (on the PC)

image

Green LED started to blink

 

 

I hoped to play with KITs onboard thermometer

18138 BLE Thermometer (RTOS)

 

image

CE218138_BLE_Thermometer_RTOS01

 

image

image

CE218138_BLE_Thermometer_RTOS01.hex

code:221524    sram:66136

--------------- Build Succeeded

 

Yes successfully build

  • But during upload the red LED lights

 

Isn’t it the problem with the PDL?

image

https://www.cypress.com/documentation/software-and-drivers/peripheral-driver-library-pdl

 

image

Check the  PDL status:

Confirm that PSoC Creator can find the PDL code.

A. Select the Tools > Options command to open the Project Management panel.

B. Confirm that the PDL v3 (PSoC 6 devices) location is correct.

 

 

image

That looks fine where is the issue?

 

Then I discovered -

My stupid fault  - I didn’t set correct  DEVICE

image

Unfortunately that example can’t be used on PSoC 62 CY8C6247BZI-D54

 

image

Error in component: BLE. The BLE_PDL_v2_0 component (BLE) is not compatible with the selected device. Please check the component datasheet for details on updating to a compatible component.

 

I’m not the only one who hoped to try that example on our kit:

https://community.cypress.com/thread/33753

#1 If you are looking to use PSoC 6 + WiFi then yes you must use WICED. There is no support for WiFi in PSoC Creator.

#2 If you are looking use the BT/BLE features of the 4343W (Murata 1DX module) on the CY8CKIT-062-WiFi-BT then again you must use WICED.

#3 If you want to just use BLE, and want to use PSoC Creator then I suggest you get the CY8CKIT-062-BLE. The PSoC 6 device on this kit has an integrated BLE radio (not a separate chip like the CY8CKIT-062-WiFi-BT). With this kit you can use PSoC Creator .

#4. The current generation of PSoC 6 devices do not have hardware to support eMMC.

#5. We are still working on USB Host support, probably won't be available until end of this year.

you have the CY8CKIT-062-WiFi-BT. The project you mentioned will not work on that kit. The project you mentioned is for the CY8CKIT-062-BLE.

 

If you are using the CY8CKIT-062-WiFi-BT, the BLE functionality is done on the 4343W radio chip that is separate from the PSoC 6. To do BLE or Bluetooth projects with this device you need to use WICED 6.1.

 

 

My  Dual-Core project ups and downs

Dual-Core Basics.

- First I download code example CE216795 - PSoC 6 MCU Dual-Core Basics.

image

First attempt to build was unsuccessful:

Hex File parsing failure. Hex file does not exist or cannot be opened.

 

I was too fast - some fine tuning was necessary!

Select Debug > Program. The Select Debug Target dialog appears

>Select the CM4 target,

image

image

The target device selected in this window does not have a Silicon ID and Revision that matches the current project's selected device. Either pick a different debug target here, or go back and change the project's selected device.

If you believe the target's detected revision number is incorrect, verify that the selected Debug Clock is 1/3 of the chip's Bus Clock and try running Port Acquire to reset the device.

 

 

As we know from PSoC programmer:

image

Our device is CY8C6247BZI-D54

 

I need to select it:

image

image

 

 

And Build the project again:

Select Debug > Program. The Select Debug Target dialog appears

Select the CM4 target,

 

 

Programming device 'PSoC 62 CY8C6247BZI-D54 (CM4)' with file

 

The CE216795_DualCoreBlinky01.hex file was generated

 

Device ID Check

Erasing of Main Flash...

Programming of Flash Starting...

Protecting...

Verify Checksum...

Finished Programming

Device 'PSoC 62 CY8C6247BZI-D54 (CM4)' was successfully programmed

 

Well done!  DualCoreBlinky works!


RTC

As the final project I decided to check clock (RTC) features of PSoC

I conducted that experiment as previous ones.

In that case I need to be careful with update files pop-up:

Note: During the build process, do not replace the stdio_user.h file

 

image

 

image

 

 

--------------- Build Succeeded

Programming device 'PSoC 62 CY8C6247BZI-D54 (CM4)' with file 'C:\PSOC 6\examples kopie\CE216825\RTC_Basics.cydsn\CortexM4\ARM_GCC_541\Debug\RTC_Basics.hex'.

Device ID Check

Erasing of Main Flash...

Programming of Flash Starting...

Protecting...

Verify Checksum...

Finished Programming

Device 'PSoC 62 CY8C6247BZI-D54 (CM4)' was successfully programmed

image

 

Mobile BT project

 

Cypress mobile application

Okładkais rady to communicate with PSoC

image

Unfortunately I didn't manage to create BT project

I treat it as a big failure of that RT. Looking for solution and attempt to learn how to program PSoC using BT section of the LBEE5KL1DX-883.

 

Check of general system immunity

At that point I see the pros only.

No interferences, stable work of all Kit’s parts, reliable manufacturing and qualified components.

I didn't experience any problem with communication when the unit was in relative close distance from the wifi router when in infrastructure  or laptop/ mobile using AP mode.

Quality

Mechanical issue - quality of implementation, form factor, compatibility with other boards etc

All above deserves the best, highest marks!

I didn't find any cons regarding board quality. Reliable and  handy for me all requirements are fulfilled.

 

The only, really small, remark concerns Arduino compatibility.

The form factor of the board pins - are 100% arduino compatible

But the voltage 3.3V - the little cons in the case of my experiments.

 

Final REMARKS

After relative (too) long time of dealing with CY8CKIT-062-WiFi-BT PSoC 6 WiFi-BT Pioneer Kit accompanied with the CY8CKIT-028-TFT,

spending several hours configuring and experimenting PSoC Creator IDE, WICED Studio SDK, PSoC Programmer with KitProg2&3

I feel ready to put some words as the summary.

 

I found PSoC 6 WiFi-BT as the promising system to develop both simple as well as advanced IoT projects.

 

We need to confirm that our KIT is a complete hardware & software solution to help develop Cypress IoT applications in the really simplest way.

Although I haven’t tested these features very much, it can be employed for mobile applications for control, telemetry and other IoT systems.

Supporting both wireless client and AP (server) modes that can be accessed directly without AP or router.

 

It's hard for me to criticize that sophisticated and powerful device.

But generally talking about the whole kit solution and concept, I'm confused now:

...plenty of tools, serious changes in functionality in new versions...

Starting with PSoC kit I knew I needed to learn and get acquainted with "PSoC Creator"  as well as "Wiced Studio"

Nevertheless I see that "Cypress Programmer" is still alive and some instructions/ examples basis on it...

Now I hear about "ModusToolbox" as the leading tool and successor of all above...

And additionally It seems the Mbed OS is required… what else?

 

I will repeat the sentence from the middle of that RT: another eclipse-based suites, another gigabytes taken…

Microchip, Matlab, Ti Composer, Digilent - Cypress add next 2 IDEs.

It's a pity we can’t use one “engine” for different programming environment.

 

My ups and downs with examples:

I'm honestly disappointed that many BT examples I wanted to use/ learn/ modify, are dedicated to the BLE kit only!

My learning curve basis mostly on good examples, I couldn’t find recommendation of good examples for particularly PSoC6 WiFi BT Kit,

except these basic, explained in the manual.

 

The usage of the PSoC Creator IDE, WICED Studio SDK which are eclipse based suites isn't good for beginners.

Some programming skills are necessary.

 

Nevertheless Possibilities of PSoC 6 WiFi-BT are outstanding indeed! I haven't even used a few percent of its functionality.

I focused on some simple examples but the tool is extremely universal. Having the skills and experience you can take on any IoT related challenges.

 

Thanks for reading (I promise to divide my report for smaller parts soon!)

Marek

Anonymous
Parents
  • Nice detailed road test report.

    Cypress does a good job of documentation, but it is very voluminous and takes a while to read and understand all of the capability they have provided you.

     

    Are you going to do any testing with the programmable digital and analog components?

     

    DAB

  • Thank you!

    I agree the documentation is prepared perfectly, I have no objections to the quality of Cypress job in that matter. My complains regard only some weakansy on the field of (lack of) examples "dedicated" to our kit.

    On the other hand - I honestly confirm that above depict my propably wrong and lazy attitude to the testing idea. I prefer learning using the ready examples not gathering knowledge building the project from the beginning.

    Only when I feel confident, comfortable ("at home"), I can build my own application.

    Nevertheless my plan is to first continue with attempts to create the BT application.

    Regarding programmable digital and analog components tests - for sure yes: soon - I hope

    Marek

Comment
  • Thank you!

    I agree the documentation is prepared perfectly, I have no objections to the quality of Cypress job in that matter. My complains regard only some weakansy on the field of (lack of) examples "dedicated" to our kit.

    On the other hand - I honestly confirm that above depict my propably wrong and lazy attitude to the testing idea. I prefer learning using the ready examples not gathering knowledge building the project from the beginning.

    Only when I feel confident, comfortable ("at home"), I can build my own application.

    Nevertheless my plan is to first continue with attempts to create the BT application.

    Regarding programmable digital and analog components tests - for sure yes: soon - I hope

    Marek

Children
No Data