New Year's Grab Bag RoadTest - Review

View table of contents ...  

RoadTest: New Year's Grab Bag RoadTest

Author: weiwei2

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: Renesas RAJ30600

What were the biggest problems encountered?: Unclear which firmware to replace on board. Unsure how to check whether item such as KMS is still intact on my board. Unable to retrieve some example files listed on the application note (such as the PMSM reference design having different directory structure look and field)

Detailed Review:

Opening

I like the colourful quick reference card that comes with both the FRDM-KV31F and FRDM-MC-LVPMSM

both provide the quick url to the jump start the design on one side of the quick reference card, and the legends of all the pinout on overleaf. One thing i can recommend to add is the IO voltage level, whether it is 5V or 3.3V.

But actual dealing with the board later is pretty challenging.

 

Introduction

First, let's understand what is PMSM and what is BLDC. The reason i state this is this is somewhat confusing. For some external reference, look at the discussion on https://www.researchgate.net/post/What_is_the_difference_between_BLDC_and_PMSM_motors

In short, PMSM motor (also can be referred as Brushless AC motor) is similar to Brushless DC (BLDC) Motor, in that they have the same structure and the same components. Both motors have permanent magnets in the rotor that interact with the magnetic field produced by the stator coils. PMSMs have a different Back-Electromotive Force (BEMF), since the flux linkage between the stator and the rotor is not trapezoidal. In the PMSM, the BEMF is sinusoidal. This is an intentional effect produced by the way the coils in the stator are wound (in a sinusoidal fashion), while in the BLDC motor the stator coils are evenly wound.

PMSMBLDC

image

distributed stator windings (coils spanning more than one tooth)

image

The geometry of the windings in a BLDC motor give it a trapezoidal back EMF waveform.

Image credit: Monolithic Power Systems

 

concentrated stator windings (coils wound around each tooth)

 

the difference windings decide which commutation control algorithmn can be used for each type of motor

 

Some control terminologies are:

  • FOC (field oriented control)

Also known as vector control. This is a method in which the current vector (magnitude and direction) is determined relative to the rotor, rather than on the basis of sine waves, as is done in sinusoidal commutation. While sinusoidal commutation has low efficiency at high speeds, FOC provides high efficiency across a wide speed range, as well as very smooth motion.

  • sinusoidal control algorithmn
  • trapezoidal control algorithmn (also named 6 step commutation) - used for BLDC motor control

in theory, the BLDC motor’s back EMF is trapezoidal, in reality, the back EMF waveform is not purely trapezoidal. Inductance in the motor smooths the back EMF into a more sinusoidal shape. And since the back EMF is more sinusoidal than trapezoidal, it is possible to use sinusoidal commutation with BLDC motors. This requires the addition of an encoder or resolver to accurately track the rotor position, which adds cost to the system, but it results in significantly reduced torque ripple.

  • Sensor and sensorless motor control

 

PMSM is typically controlled with FOC and sinusoidal control algorithmn, while BLDC motor can be controlled by trapezoidal, sinusoidal and FOC.

image

source: http://www.ti.com/lit/an/sprabz4/sprabz4.pdf

 

 

The FRDM_MC-LVPMSM has the features below

  • Power Supply Input voltage DC: 24-48VDC
  • Output current up to 5 amps RMS
  • Power supply reverse polarity protection circuitry
  • 3-phase bridge inverter (6-MOSFETs)
  • 3-phase MOSFET gate driver with over current and under voltage protection
  • Analog sensing (DC bus voltage, DC bus current, 3-phase back-EMF voltage)
  • 5.5 VDC auxiliary power supply providing FRDM MCU board supplying
  • Motor speed/position sensors interface (Encoder, Hall)
  • Freedom motor control headers compatible with Arduino R3 pin layout

The board is suitable for sinusoidal control algorithms (FOC). It is using Fairchild half-bridge gate drivers & power MOSFETs. The FDMS8090 100 V dual N-channel power MOSFETs (@10A continuous drain) are driven by FAN7888MX 3ch half bridge gate driver.

FAN4852IMU8X low power amplifier

 

The 5.5VDC auxiliary power supply statement is intriguing, considering that the FRDM-KV31F is mentioned to use 3.3V in the table below. A further check on Freedom FRDM-MC-LVPMSM Development Platform User’s Guide provides no further information. It is not so straightforward to navitage the wealth of documentation. In fact i end up finding the documentation is really on the downside as there is a lot of missing information and confusion.

It is also listed as compatible with FRDM-KV31F and FRDM-KV10z. The former is Cortex-M4 based while the latter is lower end Cortex-M0+ based

 

FRDM-KV31FFRDM-KV10z
  • KV31F512VLL12 MCU (Arm® Cortex®-M4 120 MHz, 512 KB flash, 96 KB SRAM, 2x 16-bit ADCs, 4x FlexTimers/PWM up to 20-ch. with quadrature decoder dedicated to motor and power control and 2x 12-bit DACs, 100 LQFP)
  • Enabled with Kinetis® Motor Suite, software solution that enables the rapid configuration of motor drive systems, and accelerates development of the final motor drive application, whilst improving overall motor system performance
  • Six-axis sensor combining accelerometer and magnetometer (FXOS8700CQ)
  • Tri-color user-controllerable LEDs
  • Two (2) user push-button switches for NMI interrupts and LLWU wake up (SW2/SW3)
  • Thermistor sensor to measuring temperature
  • Power selectable 3.3 V/1.8 V
  • Motor control auxiliary connector
  • Form factor compatible with Arduino™ R3 pin layout
  • Flexible power supply options – USB or external source
  • New, OpenSDA debug interface
    • Mass storage device flash programming interface (default) – no tool installation required to evaluate demo apps
    • MBED Debug interface provides run-control debugging and compatibility with IDE tools
    • CMSIS-DAP interface: new Arm® standard for embedded debug interface
  • MKV10Z32VLF7 MCU (Arm® Cortex®M0+ 75 MHz, 32 KB Flash, 8 KB SRAM, 16-bit ADC and FlexTimers with quadrature decoder dedicated to motor and power control, 48 LQFP)
  • Six axis sensor combining accelerometer and magnetometer (FXOS8700CQ)
  • Tri-color user-controllerable LEDs
  • User controlled push-button switches
  • Thermistor sensor to measuring temperature
  • Form factor compatible with Arduino ™ R3 pin layout
  • Flexible power supply options – USB or external source
  • New, OpenSDA debug interface
    • Mass storage device flash programming interface (default) –no tool installation required to evaluate demo apps
    • MBED Debug interface provides run-control debugging and compatibility with IDE tools
    • CMSIS-DAP interface: new Arm standard for embedded debug interface

I am not familiar with the OpenSDA, but reading about it on https://www.nxp.com/support/developer-resources/run-time-software/kinetis-developer-resources/ides-for-kinetis-mcus/open… gives more confusion than good. It is stated below

*Note: During development of OpenSDAv2 the reserved bootloader space was found to be too small. Thus a new version of OpenSDAv2 was subsequently released and named, OpenSDAv2.1.

after crosschecking, i am looking at the JLink (look at getting started below where after following forum, it is stated that we need to replace with Segger JLink debug version of the openSDA), its version is 2.1 (as stated on https://www.segger.com/products/debug-probes/j-link/models/other-j-links/opensda-sda-v2/ ) for FDRM-KV31F

 

getting started

 

Quick start guide lead us to freescale.com/FRDM-KV31F (redirect to https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/freedom-development-boards/mcu-boards/… )

likewise, the quick start guide http://freescale.com/frdm-mc-lvpmsm will redirect to https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/freedom-development-boards/mcu-boards/… )

as this board is pretty old (> 3 years) and before NXP's acquisition, the documentation can be misleading (which version of software is needed)

 

from the quick start card of FRDM-KV31F, Some further browsing on the listed application BLDC will lead us to https://www.nxp.com/applications/solutions/internet-of-things/smart-things/motion-and-motor-control/brushless-dc-bldc-mo… for a list of BLDC motor applications

One of them, for example is https://community.nxp.com/docs/DOC-340767 hands-on training for Kinetis motor suite. Although listed as BLDC

In short, at a glance, the documentation, although it does not directly point out the care to be taken by starting out with a 3 year old board, contains sufficient wealth of information. This is useful for a user to get started with the platform.

 

Hardware Setup

The FRDM-MC-LVPMSM is connected to the MCU in this manner.

image

from the hands-on training for KMS, the hardware connection is as below. however, my enumerated board is not the same as the screenshot (only shows two files - details.txt & mbed.html)

Note: doesn't matter with the firmware version as i have decided to just use refer to the wiring setup and not use KMS. KMS is kinda depreciated (refer to https://community.nxp.com/thread/495220 )

NOTE

The order of cables determines the physical direction of rotation of the motor (clockwise vs. counterclockwise) in sensorless velocity control. Inverting the order of your cables causes the same speed command to spin the motor in the opposite direction. Hence, the order of cables only matters if your motor or application must spin in a specific direction. This is not the case for sensored control, as described later in this section.

imageimage

 

Software Setup

credit to a fellow roadtester , he has pointed out of the new year grab roadtest start page forum https://www.element14.com/community/allRoadTestReviews/2015#recentReviews (Apr 3, 2019) on the installation of the necessary SDKs

(one has either the choice of KMS or MCUexpresso). So, i basically avoided the installation fiasco.

Here is what he mentioned

The KMS firmware embedded in the FRDM-KV31F board is around three years old I think and won't work with MCUXpresso. You will need to work with Kinetis Design Studio, and it needs to be v3.0.1, NOT the final version (3.2). You will also need the KDS SDK v1.3.0. and Kinetis Motor Suite desktop software v1.1.0.

 

First, you need to have the correct boatloader to work with the KMS software. When you plug your FRDM-KV31F board into a PC's USB port, it will either enumerate as MBED <drive letter> or FRDM-KV31F <drive letter>. Mine came with the MBED bootloader and that won't work with KMS. If you want to use KMS, you'll need to change it, following the instructions on this page.

 

Once you have the correct bootloader, you can go ahead and install the software listed above. Oh, and you'll need a power supply for the motor controller board. The motor is rated at 24v-40v 2.5A. It will work with less, but the KMS software may complain.

 

If you don't want to use Kinetis Motor Suite, you don't have to worry about any of the above. You can use MCUXpresso (the latest SDK has an example motor control project).

 

[Addendum] After installing KDS v3.0.1, remember to go to Help->Check for Updates and tick/install everything. This is important as it updates the debugger software and ensures that KMS is not erased from the board. n.b. Other combinations of KMS/KDS/MCUXpresso may also work but I haven't tried them yet.

like Steve's, mine also come with the MBED bootloader (with the tri colour LED keep changing colour). Clicking on the MBED webpage on the state my board is FRDM-K22F (which is puzzling). However the "Oh no!" post below from this page does say we need to install the mbedWinSerial.exe

i did a crosscheck on device manager and the MBED is not enumerated as serial port device

image

After installing MBED windows serial communication https://os.mbed.com/handbook/Windows-serial-configuration , the MBED is successfully enumerated (COM4 in my case)

imageimage

A check on the link provided by Steve from this page sounds alarming

OH NO!

It has come to my attention that a batch of FRDM-KV31F MCU boards, were shipped to people, programmed with MBED OpenSDA firmware.

 

The Kinetis Motor Suite GUI scripts load the reference project image into the KV31F MCU flash using the MSD programming built into the P&E Micro firmware. It specifically looks for the FRDM-KV31F MSD drive.  NXP moved away from the MBED firmware to eliminate the mass erase possibilities that could occur.

 

The FRDM-KV31F does not appear on these MBED boards. In fact, unless you have run the mbedWinSerial.exe installer found here, or get the latest driver herethe mbed serial port will not enumerate. Plug in your FRDM-KV31F board and run the installer.  But let's not stop there. We want to make sure you don't mass erase your MCU and blow away the  KMS execute only library stored in the MCU's flash.

Let me give you a work around for now. Any MBED enabled FRDM board will still work with KMS, but you should use the Segger JLINK debug interface. It will not mass erase your KMS firmware like the MBED debug interface can.

while it is mentioned that FRDM-KV31F will not have this MBED OpenSDA firmware, mine is obviously having it. Wei follow the guide above to replace the openSDA with Segger JLink debug interface from this page

https://www.segger.com/products/debug-probes/j-link/models/other-j-links/opensda-sda-v2/

image

 

 

We setup the SEGGER J-Link as below

image

after installation, i find i have 2 J-Link version (i believe one of them might be installed by MCUXpresso

image

after doing this segger J-Link step, we then have to change the firmware. It is this step that causes the most confusion as i am unsure which firmware to use

 

As shown in the screenshot below, we download the software and the OpenSDA image from https://www.segger.com/downloads/jlink/#JLinkOpenSDABoardSpecificFirmwares

image

the file above is 64KB

 

After much confusion, i have followed the step by I have successfully use 51KB firmware JLink_OpenSDA_V2_1.bin which can be downloaded from the post by Philip Drake on https://community.nxp.com/thread/495220

image

image

 

Kinetis® Motor Suite

from the quick start card of FRDM-MC-LVPMSM, the listed tool is Kinetis Motor Suite (KMS), although from various forum sources, this seems a risky step as it is older and tends to mass erase. I have decided to try MCUXpresso first, although it lacks the tuning capability. In fact from https://community.nxp.com/thread/495220 , it is mentioned KMS is not longer supported by NXP. Hence i decide to use it after able to test out MCUXpresso

To get KMS, we go to https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/kinetis-cortex-m-mcus/v-serie… , then move on to https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/kinetis-cortex-m-mcus/v-serie… , it will prompt for login. I install version 1.2.0. Note that my MCUXpresso (featured in next section) is 10.3.1

 

The getting started guide video on https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/kinetis-cortex-m-mcus/v-serie…  is pretty useful (although the packaging box is clearly newer than mine)

 

Anyhow, by following the lab1 of the https://community.nxp.com/docs/DOC-340767 ,

image

 

MCUXpresso

This is the latest recommeded supported IDE. We start with https://mcuxpresso.nxp.com/en/welcome , we can search for our board and it will list down the steps needed

This is to download the necessary SDK

image

pressing Build MCUXpresso will lead to the page below

image

We then add the PMSM example

imageimage

Download the MCUXpresso

image

to use the SDK, we need to download the IDE https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-inte…

i download 10.3.1

image

we drag the downloaded SDK to the view, click ok and we will have the sdk shown in the Installed SDKs

imageimage

we can then import the SDK example

image

image

we need to select Redirect printf(scanf to UART)

image

After successful loading, the main.c looks like as below. It should be able to be built successfully

imageimage

we then press debug. with MBED windows serial configuration installed, we will see this

image

click ok and with successful debug we will reach here

image

sadly, proceeding beyond this doesn't move the motor. So i have to change the firmware to J-Link and redo it. with J-Link. I load the hello world example instead of the PMSM. it will find a new probes for debug

image

i then encounter this screen that appears only shortly and i am not able to put a reply, until it has error.

imageimage

To resolve this error, i restarted the pc. Then it is fine, i have enough time to press accept and it no longer has error. The debug settings is the "debug using Segger J-Link probes

if we don't set the "Redirect printf(scanf to UART)", the hello world be output to the console

image

The serial port will shows this if we click resume.

image

After verifying that the board indeed reponse, we change back to the PMSM demo. One of the biggest problem is the red led light up and the motor is not turning. It takes me quite some time to realize that i need to press the button SW2 in order to start running properly.

image

successful steps i have is following some of the steps mentioned in https://www.nxp.com/docs/en/user-guide/FRDM-KV31FQSG.pdf

on the page i paste below. The only way to make the green LED light up instead of RED is to follow these steps.

image

The motor is turning eventually.

 

 

Freemaster and Kinetis Design Studio

i got this again from a forum posted by Steve, on https://community.nxp.com/thread/495220

The next step is to get the PMSM reference design software from here and the FreeMaster tool here  These installations still rely on the Kinetis Design Studio IDE.  These are being ported to the latest IDE MCUXpresso later this year.

Kinetis Design Studio version used is 3.0.1 (after update) , while Kinetis SDK is 1.3.0. Upon install we update it

image

upon running the build in example of PMSM with MCUExpresso, we follow instruction in https://www.nxp.com/docs/en/user-guide/KMSUG.pdf to try tune the motor

 

 

 

 

Summary

Although originally i do want to find out whether it can be run with Arduino, the complexity running it on its own platform implies that it won't run with a typical Arduino board, as the library is very different.

 

Pros

the FRDM-MC-LVPMSM requires no jumper based settings. This is a good design as often the jumper settings requires care and may lead to board damage.

 

Cons

the documentation is very confusing, despite its wealth of information. For example, https://www.nxp.com/docs/en/application-note/AN12374.pdf  mention about PMSM reference design but does not tell where to get it. Attempting to download by searching ourselves yield a directory structure which is different and we are not sure if it is correctly installed.

KMS is only available from factory. User is not able to reprogram the KMS itself. Note: KMS is not supported by NXP anymore

It lack detailed documentation on how to use freemaster with KDS

 

Brief comparison with other BLDC & PMSM evaluation kit

 

Renesas BLDC motor control

i have use Renesas https://www.renesas.com/tw/zh/products/ics-for-motor-actuator-driver/ics-for-motor-control.html  for trapezoidal BLDC. It also have some precautions on matching of IDE version and an external FPGA based debugger tool (ICS) that can collect and log signal in real-time, but not as complicated as Kinetic Motor Suit.

 

 

Epilogue

for the past few years since 2013, i have dealt with a number of motor control projects. The biggest is the research project i lead with the German MNC in BLDC for power tool. We have tried out 3 different MCU brands throughout and currently in its extension we are trying out Infineon.

Hence i want to do broad motor control eval kit comparison. To be fair, they are not exactly the same as all my previous such attempts are BLDC, a cousin of the PMSM in this roadtest

the common items to roadtest is the wealth of documentation, the ease of running the board with its intended IDE, the clarity of the examples, the performance (this is subjective and to be frank, is not something i have standardize so far), its debug capability (one cannot single step during the commutation cycle, for example, but different vendor has different means of doing debug or logging), the east of writing firmware for the board (aka some of my other boards have device driver wizard)

i also want to test if the FRDM-MC-LVPMSM which has arduino footprint, can be used with Arduino. Seriously, the arduino world lacks a serious BLDC (and to some extend PMSM) shield

i plan to also attach the board to a simple project as demo as the best use case for an eval board is to use it in a demo application. i have some simple project in mind like motorized scissor or simple trajectory control for camera rotation

 

on a extended perspective: i want to provide some review of doing motor control via Model Based Development(MBD)-> that means simulation based design which is the important use case for engineer to develop complex motor based system

such as automotive and industrial automation. i have access to software like Altair Embed that can complete the firmware design via IDE. i intend to show some level of simulation for the roadtest

however, a full MBD review might not have enough time partly because although cortex M3 and M4 is supported by Embed, this Kinetis board is not a supported board (means with all the driver mapped)

 

 

References

https://www.element14.com/community/allRoadTestReviews/2015#recentReviews

[1] MCUXpresso online reference manual https://mcuxpresso.nxp.com/api_doc/dev/942/

[2] https://www.motioncontroltips.com/faq-trapezoidal-back-emf/

[3] https://www.motioncontroltips.com/faq-sinusoidal-emf-sinusoidal-current/ contains a link to TI's tutorial video on PMSM vector control

[4] https://www.ecnmag.com/article/2009/10/comparing-motor-control-techniques

[5] FRDM-KV31F https://www.nxp.com/docs/en/user-guide/FRDM-KV31FQSG.pdf

[6] PMSM Field-Oriented Control on FRDMKV31F with Hall and Encoder Sensors https://www.nxp.com/docs/en/application-note/AN12374.pdf

[7] Kinetis Motor Suite v1.2.0 Lab Guide https://www.nxp.com/docs/en/supporting-information/KMSLG.pdf

 

 

Work Planned but not carried out

 

motorized scissor version 2 -> to fit this motor to my motorized scissor

comparison with other BLDC and PMSM board --> underestimated the effort needed to follow the example for kinetic motor suit

Anonymous
Parents
  • Thanks for the mentions!

     

    I think using MCUXpresso is a good decision with this kit. Otherwise it is quite confusing working out what works and what doesn't. It's worth looking at Freemaster if you have time. It will definitely work with MCUXpresso when they finish porting it.

     

    Good luck with your future motor projects.

  • actually i am still kinda trying to figure out whether my onboard KMS is missing as what you posted, though i have never able to run it with KMS. Ya, Freemaster is the only way going forward as it seems. Will definitely still try it.

Comment Children
No Data