Raspberry Pi 3 Model A+ - Review

Table of contents

RoadTest: Raspberry Pi 3 Model A+

Author: florinescu

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: Raspberry Pi 3 B+, Pi 4, Pi Zero W, Arduino Yun

What were the biggest problems encountered?: needing to buy additional parts (getting slightly expensive) to fully support the board's capabilities, weak documentation

Detailed Review:

Introduction

 

Hello! My name is Florin, I am a major in Systems Engineering currently working in an automotive company and here is my review of the Raspberry Pi 3 A+ Development Board.

 

With this review I attempt to analyse the board and its capabilities, to try to answer the questions "How can it help me develop an IoT solution? What differentiates it from other products?". I have two small demo projects to demonstrate what I can obtain from the board. I will not go in-depth on synthetic benchmarks because the internet is already full of these, and instead talk about my experience with the board and what I "feel" regarding its usability.

 

Use in teaching

 

The board is first and foremost marketed as a learning device. It provides some embedded development experience, but not quite on the same level as, say, an Arduino. It doesn't have that many low level peripherals and you don't have to delve that deep into configuring registers to get things working. The documentation for the microcontroller is very hard to find and what the manufacturer's website provides is lackluster, so not very good for learning once you want to get deeper into how the peripherals work.

 

It provides however an entry point into embedded development for people used to Linux, or into Linux for people used to handling registers directly in C or assembly (this is where I would fit). Its strength lies in the addition of the ability to write code in higher level languages such as Java or Python, or using old-school, well documented linux programs instead of writing everything by yourself. Also, stitching together Linux services, C, Python libraries, bash scripts to reach your goal. All this brings new possibilities into IoT like:

  • machine learning/data analysis
  • image processing
  • networking
  • multimedia applications

 

Oh, and there's a version of Windows 10 IoT core available for people unfamiliar with Linux. More on this near the end of the review.

 

Unboxing

 

I received a small box containing just the board. First of all it's surprising just how tiny the board is for how powerful it is. It's pretty close to the size of an Arduino. Here it is next to my hand:

image

 

It is very much pointed out on their website that in addition to the board, you NEED a micro usb cable+power supply, an HDMI cable AND a micro SD card to get started. On the one hand it's nice to have everything modular so that you don't need to pay for all components since you will most likely have an HDMI or Micro USB cable lying around. On the other hand, it is a big shame that the original package doesn't provide you with the bare minimum required setup and that you need to do some research in order to buy everything necessary. There is only one "official" supplier for Raspberry for my country, and looking at its page we get the following:

  • the board itself - 25 euros
  • the official power adapter is around 10 euros and surprise - out of stock
  • SD card with OS on it and an HDMI cable another 15 euros
  • the official camera is around another 35 euros - out of stock
  • LCD touchscreen display 75 euro - also out of stock

 

So I need to resort to some external suppliers to get what I want and shell out extra cash to fully exploit the board's capabilities.

 

There are some quirks regarding the additional components that you need to learn about before purchasing:

  • The USB power supply needs to be able to provide 2.5 A power. The board WILL work with smaller power supplies and this threshold is specified only to allow for current draw by other devices connected to the USB port (a worst-worst case). People will most likely have a recent phone with quick charge capability, and those can usually provide 5 V at 3 A. You can usually get away with a 2 A charger, which is what I have used sometimes without a problem. Just be careful that if the board crashes due to the power supply not being able to keep up, there is a high chance to get the SD card corrupted.
  • The micro USB cable needs to be able to support the current draw. So cheapo or very long cables may fail. It doesn't need to be a data cable (data pins can be unconnected inside the cable), unless you use a phone charger where it MIGHT also need the data lines to switch to higher current.
  • The micro SD card needs to be at least 8 GB and it will be what will hold the OS and all your data. There are detailed instructions on the Raspberry website on how to set it up to install the OS. For a card bigger than 32GB there are some additional steps required because the default format for these large SD cards is exFAT and this cannot be read by the Pi bootloader which requires FAT. It is also possible to buy SD cards pre-formatted and with the OS installer already on them.
  • There are lots of camera models on the web. The official model has two versions: oldest, now discontinued version, using a OV 5647 sensor - 5MP photos, 1080p 30fps video, and the newer one using the Sony IMX219 with 8MP photos, 1080p 30fps video. Personally, I do not see a lot of relevance for choosing the newer version with extra MP photos, as I am more interested in video recording which on paper is the same. Also if you want to do any kind of image processing you will most likely downsize the video/image to get better performance, so sensor output is less relevant. There are a lot of unofficial cameras online and I like the ones by Waveshare. They provide a big selection using the first gen sensor but with many different options: fisheye lens, adjustable focus lens, infrared or a combination of those. Searching for the second gen cameras gave me a poorer selection to choose from (no lens options).

 

My setup

 

My setup eventually consisted of the following:

  • USB wall plug from my Motorola phone. Provides 5V 3A.
  • 64 GB micro SD card. Figured I'd get a larger one to be able to hold very long video logs (days' worth). Also I will try to have a dual boot with Windows and Raspbian.
  • 1920x1080 monitor
  • Separate speaker connected to audio output, even though the HDMI is audio capable (my monitor isn't)
  • Waveshare RPi camera F with infrared and adjustable focus lens and an additional 1 meter ribbon cable
  • BLE mouse
  • wireless keyboard connected via USB dongle
  • aluminium "Armor" case. The entire case acts as heatsink and has silent fans. For me it's the best case on the market.

 

First few weeks of the review period (without the case and camera):

image

 

Rest of the review, where I got the case and the camera:

imageimage

 

Support documents

 

As I touched on this before, the Raspberry website provides extensive explanations in regards to the additional components you need for the board and installation procedure. They provide mechanical drawings and electronic schematics which are detailed enough.

 

My biggest disappointment is that the information provided by the Raspberry Foundation regarding in-depth CPU details is very lackluster and they reference A LOT of 3rd parties or enthusiast sites on their site for more detailed information. The information is not gathered in one place (the producer's website or a PDF) and this greatly complicates development. There is also in my opinion limited responsibility assumed by the Raspberry Foundation since most documentation is not provided by them directly, merely linked to. For instance, all of there are the only way to get relevant info about something, linked from the official website:

  • site 1 for GPIO library
  • site 2 for basic GPIO details
  • site 3 for in-depth GPIO details
  • some more GPIO details are available on Raspberry's website
  • site 4 for a different SPI library
  • etc.

 

There is no correct datasheet version available for the 3 A+'s CPU. Official information is only available for peripherals of CPUs of older generations of Pis (the BCM 2835). The official statement from Raspberry's site is something along the lines of "CPU x is similar to y, but the ARM core is different. CPU y is similar to CPU z, but the ARM core was replaced with another ARM core". So not that exact and detailed. There are some datasheet variants on the web put out by some universities for the 3 A+ CPU (the BCM 2837B0), such as this one. But they are not without their drawbacks, and to quote the guy who created the BCM2837 document:

I created that document. It is indeed simply a modified version of the original BCM2835 document with the intention of preventing confusion and bugs as students work through assignments. As explained on the course website:

If you open the manual we’ve linked you to, you’ll see references to the BCM2835 chip everywhere. This is because we’ve simply taken the documentation for the BCM2835 chip, fixed relevant errata [and addresses], and [changed] the title to say BCM2837.

Even if it may be correct, for me this is not so trustworthy as it is not an official source. And considering that peripheral addresses changed for different Pi boards (more on this in the peripherals chapter), to me it becomes even more doubtful that the old datasheet applies to the 3 A+'s CPU.

 

This was just the document describing the peripherals. Typically this would be all you need, but in case you need information about the ARM core (address spaces, arithmetic unit etc.), you need to also look at the ARM documentation for the Cortex-A53 core, which is available on ARM's website. The Raspberry website does provide links to the ARM core documentation for older Pi CPUs, but not for the one in 3 A+.

 

Next I tried to go into detail to find as much as possible about GPIO functionality. I found this page where it explains configuring GPIO drive strength. It only specifies that it applies to "all models up to and including the 3B+ model". Are all CPU variants since Pi 1 all the way to the 3 A+ and B+ 100% identical in this regard? What about the Pi 4? There are register addresses and descriptions available, but only the drive strength configuration bits are explained here. It doesn't even touch on what do limited slew rate or input hysteresis mean.

Going back to the drive strength setting, it states that "Even if you set the drive strength to 2mA and then load it so 16mA comes out, this will not damage the device". How is the drive strength configuration then relevant? Why should I configure it? No clear answer...

image

 

On the official website they also provide a link to an external user's guide of the board's pinout, which provides more in-depth information. It goes into pretty decent detail, such as: "Pin x which can be configured as I2C SDA, includes a fixed, 1.8 kohms pull-up to 3.3v, which means this pin is not suitable for use as a GPIO where no pullup resistor is desired". This however is the kind of information that can make a big difference when designing for my board, so it is disappointing that it is not clearly stated on the producer's website and is only available from 3rd party sources (even though they are referenced by the producer). I cannot give this kind of documentation to an "old-school" HW engineer and expect him to understand what to connect to which pin for an application.

 

There still are some useful things they did, like the pinout command. You type it in the terminal and it tells you the board pinout so you don't need to print out a pinout sheet to permanently have on your desk.

image

 

Overall, it feels like the Raspberry follows the "maker" way of doing things, where everything is not 100% clearly documented. You just try and fail or browse stackoverflow for hours, hoping not to damage the board while trying to understand what goes where. You rely heavily on forums and amateur opinions which we all know how well they work. An official, well structured, complete documentation is lacking for everything Raspberry and pushes away a more "professional" approach.

Then again, it is meant as a teaching device, so maybe it doesn't necessarily need to provide that kind of detail.

 

Installation

 

Out of the box, the Pi doesn't have an OS and you need a separate PC to download Raspbian, a modified Debian (Linux) distro for the Pi. The Raspberry Foundation provide detailed setup instructions on the Pi's setup guide. The way it works is you put a tool for this called NOOBS on the SD card from a separate PC, plug it in the Pi and the OS installation will start at first boot, downloading the OS from the cloud.

 

During installation you get a list of available OSes and you can tick several to install them, so I thought I would attempt a dual boot setup with Windows and Raspbian. Raspbian installed successfully, however for Windows I got an error saying that NOOBS cannot actually install Windows. Why have it as an option then?

image

 

Anyways, I would focus on other parts of my review and later come back to Windows. As it turned out, the installer did in fact create some NTFS partitions for windows, and all Raspbian partitions were in total around 28GB. I left it at that and tried at a later point to reinstall Raspbian to get the entire SD card available.

 

Another thing to note is that Bluetooth devices obviously will not work during the installation so you need a USB mouse and keyboard. Also a USB hub if they both are wired or use separate dongles.

 

Board usage

 

First impressions of Raspbian

 

As with any Linux system, going through the OS menus, starting and closing apps feels much smoother than Windows on a more powerful PC.

This is the first time I am using a Raspberry. So the first thing I wanted to try was to watch a youtube video in 1080p image, since it would theoretically support this. Chromium comes preinstalled so I was glad to be in a familiar environment. I ran into a video codec issue and all videos looked really funky. Through a quick google search I found the package I need to install and the video looked better afterwards, although at an unwatchable FPS. This is how all videos looked without the codec:

image

 

Chromium is as much a memory hog as its sibling Chrome and this is where the smaller RAM of 512MB is becoming and impediment. Browsing the web from the Pi to look for code examples while also having a development environment open proved nearly impossible as it would take up almost the entire RAM and be really sluggish for a few minutes, before finally giving up and closing itself. You can tweak the amount of RAM shared with the GPU but it doesn't really help much.

I later found out that the unusability of Chrome was because I logged into my user account, and it automatically downloaded adblock, which was eating up 50-100 MB of RAM. Removing it improved the browsing experience to something almost usable. Viewing video on YouTube was still nearly impossible. After reinstalling to the new Raspbian 10, things improved slightly and I was able to do some google research while tinkering with code without a problem.

 

Otherwise, the OS comes with a bunch of IDEs preinstalled so you can jump right away into writing code for most common languages. Here is the default IDE for C/C++, Geany, running a Hello World example:

image

 

Installing or updating new programs is possible via the classic apt-get command, but there is also a basic GUI which can do this in a more user-friendly way. I wanted to install eclipse since it is easily extendable and can handle a lot of programming languages:

image

 

With eclipse it is possible to have one IDE for C, C++, Python and Java. This is great for helping people learn how to accomplish the same thing in different languages. I cannot stress enough how the Pi's biggest strength is the fact that you are not bound to a single language as with most IoT solutions. It's very easy to even mix multiple programs written in different languages to accomplish a task. For instance, here are some really short Hello World snips for these 4 programming languages:

imageimageimageimage

GPIO, peripherals

 

After getting familiar with the board I wanted to tinker around a bit and see what is possible from the Pi's peripherals. Sadly there is no analog input, so you need an external ADC chip for that, but otherwise most peripherals you would expect from an embedded controller are there.

From the Pi website you get a link to a library on how to work with the GPIO/peripherals in Python, and how to access registers in C. The easiest way would probably be to work in Python, where this is how to blink an LED for once a second:

from gpiozero import LED
from time import sleep

led = LED(21)

while True:
 led.on()
 sleep(1)
 led.off()
 sleep(1)

 

They also provide possibilities for PWM-ing an LED, very straightforward:

from gpiozero import PWMLED
from time import sleep
import RPi.GPIO

led = PWMLED(21)

while True:
 led.value = 0.20
 sleep(1)
 led.value = 0.80
 sleep(1)

 

The python library for working with GPIOs, GPIO Zero, along with basic tutorials can be found here. What I really like about it is that in addition to providing basic input/output functionality, it also provides a lot of helper classes in an OOP fashion with added functionality. Which is what most of us would anyways write when starting with a new microcontroller. For instance:

  • LED class allows you to configure the LED as active low or high and simply turn it on() or off() in code (instead of remembering to always set the GPIO directly high or low)
  • Motor class allows you to configure which pin is used as backward/forward for the driver or whether to use PWM or not. And then you just do something like motor.forward() to move.

Here is a picture of the class hierarchy for output devices:

image

 

Otherwise to write the code in C, while I am sure there are libraries out there, the "embedded" way would be to access the registers directly. The official website links to yet another website describing how to do this, found here. There are no headers defining registers and mapping them to their correct addresses as would be expected of an embedded development environment. You have to do this yourself using macros for the "base peripheral address" and offsets according to the peripherals datasheet mentioned previously. Since there have been changes over time for the Raspberry CPUs, the base peripheral register address changed and the Raspberry Foundation are kind enough to provide a library with some helper functions which will work on all Pi boards and should be future-proof. Neat!

 

Going further, I tried to get UART communication running. First, I connected the UART pins of the Pi through a MAX3232 UART to RS-232 converter, to my PC's serial port. The Raspberry Foundation this time suggested a different library called WiringPi-Python. A bit annoying how you need to bloat your code up with several libraries to achieve basic embedded functionality. Here is a snippet of how to send a message once a second:

import wiringpi
import time

wiringpi.wiringPiSetup()
serial = wiringpi.serialOpen('/dev/ttyS0',9600)
while (True):
 wiringpi.serialPuts(serial,'greetings from the Pi')
 wiringpi.serialPutchar(serial, 0x00);
 time.sleep(1)

 

This is where I need to highlight some limitations of the Pi, all of them caused by poor documentation, unconventional HW implementation, or the implementation behind "unofficial, officially-supported" libraries:

  • for PWM, following points were clarified to me by this question on stackoverflow
    • the default frequency is 19.2 MHZ - WAYYYYY to high for any motor driver out there. Changing frequency is not as easy as it would be expected.
    • changing the duty cycle actually affects the frequency too, due to some weird implementation of PWM in the hardware
    • it is possible to configure it to work as "usual" PWM peripherals
    • but with awkwardly named functions like pwmSetClock() and pwmSetRange() which actually control what seems to be two separate prescalers. This is using the WiringPi library, not the GPIO Zero one.
  • for UART:
    • older Pi versions used the linux device /dev/ttyAMA0 for the UART port. However on newer versions this UART is used for communicating with the WiFi/Bluetooth chip and there is no clear indication of this in official documentation
    • ttyAMA0 is therefore unavailable in the pin header and sending anything to it crashes the bluetooth chip (my BLE mouse becomes unavailable until I restart the system). To find this out I went from the Pi website to this one which then linked to this one for more info. So cumbersome!
    • the correct device to use for these boards is /dev/ttyS0, which can be seen in the snippet above
    • after finally being able to send data, following screenshot shows 2 loops from the previous snippet and what is received on my PC. This garbage would be indicative of an incorrect baud rate, however my logic analyzer confirms that the baud rate transmitted by the Pi is actually 9600.
    • image
    • hooking the UART up to my Microchip board instead, I receive the data correctly while debugging (code shown is from the ATmega MCU:
    • image
    • Googling around I find some stackoverflow guys saying that the UART on ttyS0 may be dependent on CPU frequency, meaning baud rate could change if the CPU is throttled, and the peripheral datasheet does confirm this. To have a stable UART you need to limit the CPU frequency to its lowest possible value of 250MHz. MAJOR design oversight on Broadcom's part!
    • I was unable to determine why the RS3232 transceiver didn't work, as it was working fine with other boards.  Maybe the baud rate is not precise enough and, coupled with possible delays introduced by my transceiver, leaves the PC unable to recreate the data sent.

 

Power draw

 

As stated by the official website, the Pi requires a solid 5V supply capable of delivering 2.5A. I used a USB cable that I cut the ground wire from, to connect an Ammeter to measure the current draw. I also sometimes used a Voltmeter to measure the supply voltage on the 5V line.

 

In idle with a display, my keyboard and mouse connected, the power draw was around 200-300 mA and the supply voltage was holding steady at around 4.9-5 V.

image

 

With the Pi Camera connected the power draw was 300-400 mA higher, due to the fact that my camera has infrared LEDs and they are almost always on due to the bad lighting in the room. The camera module by itself eats about 100-150 mA while not running. Running the camera, the power draw is about 800 mA:

image

 

And the power draw grows to almost 1 A while running the image detection project. The supply voltage also dips to ~4.5 - 4.8 V momentarily during heavy tasks so I should probably find a better power supply.

image

 

Still, for me getting a 5 W power draw for a security camera that cost ~60 euros sound pretty good.

 

Performance issues

 

You can see in various screenshots that I have in this review that in the corner I have configured it to show CPU temperature, CPU usage % and RAM usage %, in this order from left to right. The CPU was running at 45-50 degrees C when idle, with RAM usage at 20-30%. When browsing the web in Chrome or doing more intensive tasks the RAM was usually the bottleneck, getting almost full very easily, sometimes to a point where the Pi was completely unresponsive. The CPU would also get hot to 50-60 degrees, at which point it would start to throttle (the temperature chart in the corner turns red when the frequency was throttled due to heating AFAIK). This is a screenshot from my Object detector example:

image

 

The case helped a lot with thermals and is very sturdy (dropped it once or twice without a problem to the Pi). The entire case acts as a heatsink and connects to the CPU and RAM chips with thermal tape. Two letdowns regarding the case:

  • USB socket was a bit squeezed by the case so I had to push a bit harder to get the keyboard dongle in the first times
  • Camera and display connectors aren't accessible with the case on. I needed to connect the camera cable first and then screw in the case and leave it there for the rest of the review.

image

 

Anyways, the CPU temperature was kept at a constant 35 degrees by the case and barely exceeded 40 degrees on the same example program as before.

 

Regarding memory usage, there is not much you can do and you simply have to live with this limitation. Building programs from source as is common for Linux is nearly impossible as you run out of RAM easily. Browsing the web is not very smooth. Pages take a while to load and memory fills up very quickly with 2-3 tabs open in Chrome.

 

Due to Linux, the Pi uses a swap partition for when RAM gets really low, but since the swap stuff is written to the SD card (much slower than RAM), the system becomes unusable once swap is used. I used the commands described by this guy here to disable the swap mechanism. This way, when a process uses too much RAM, the system kills it instead of getting frozen.

 

The audio output was very low compared to my PC but of decent quality. I couldn't initially connect my Bluetooth LE mouse (and I expect the speaker to be the same) due to some Raspbian mumbo-jumbo. I found some help on their forums here, after which my mouse connected without a problem automatically at every boot-up.

 

IoT use cases

 

I was unsure in the beginning where the board would fit in an IoT context. Since the board is incomparably more power hungry than other boards it cannot be battery-powered. The peripherals are fairly hard to set up. And obviously it would make a lot of sense to take advantage of its processing power. Therefore the best choices would be either image processing applications or as a concentrator/data processor in a network of IoT devices.

 

Concentrator/brain of an IoT network

 

The first use case I conceived for the board is that of a concentrator, where it gathers data from several devices, processes it and outputs results or sends commands to devices in the network. For this I have an existing Google Cloud project from my previous roadtest. I also use a board from Microchip from the same roadtest, which reads its temperature and brightness sensors and outputs them to Firebase (a Google cloud hosted database) via a WiFi connection. Receiving that data on the Pi would be a pretty good demonstration of the concentrator functionality.

 

To connect to Firebase I used the REST API available for it, basically sending HTTP requests to exchange data with the database. This is the Firebase guide to how the HTTP links would need to look like and what REST commands can be used to send/receive data. This is a really nice website describing how to call REST APIs in Python. Following is my Python code that resulted. It's not the best implementation possible, but everything is fairly obvious and it gets the job done. Also, I removed the path to my Firebase project and to my board UID from the code snip just to be safe.

 

import requests
import cv2
import time
import json
import matplotlib.pyplot
import numpy
from datetime import datetime
from matplotlib import pyplot

avrDevice = #UID of my device
firebaseDbPath = #link to Firebase database, something like 'https://project-name.firebaseio.com'
avrLastUpdatedPath = firebaseDbPath + '/avr-iot/lastUpdated'
avrDataPath = firebaseDbPath + '/avr-iot/data/' + avrDevice

latestTimestamp = 0
xs = []
ysLight = []
ysTemp = []
fig, axs = pyplot.subplots(1,2)
pyplot.ion()
pyplot.show()

while True:
   
    resp = requests.get(avrLastUpdatedPath + '.json')
    if resp.status_code != 200:
        print('Error while getting avr last timestamp: ' + str(resp.status_code))
    else:
        if (latestTimestamp != resp.json()[avrDevice]):
            latestTimestamp = resp.json()[avrDevice]
            
            print('New data at ' + str(latestTimestamp))
        
            resp = requests.get(avrDataPath + '.json?orderBy="time"&limitToLast=1')
            if resp.status_code != 200:
                print('Error while getting avr data: ' + str(resp.status_code))
            
            data = next(iter(resp.json().values()))
            light = int(data['Light'])
            temperature = float(data['Temp'])
            timestamp = datetime.fromtimestamp(int(data['time']/1000))

            print(light)
            print(temperature)
            xs.append(timestamp)
            ysLight.append(light)
            ysTemp.append(temperature)
            
            if (len(xs) == 31):
                xs.pop(0)
                ysLight.pop(0)
                ysTemp.pop(0)

            axs[0].clear()
            axs[1].clear()
            axs[0].set_title('Light')
            axs[0].set_xlabel('Time')
            axs[0].set_ylabel('Light (lux)')
            axs[1].set_title('Temperature')
            axs[1].set_xlabel('Time')
            axs[1].set_ylabel('Temperature (°C)')
            axs[0].plot(xs, ysLight)
            axs[1].plot(xs, ysTemp)
            fig.autofmt_xdate()
            pyplot.pause(0.1)

 

Here's how the charts look. At first I had the other board next to an open window, so it was pretty bright and slightly colder. As I took the board inside at ~19:54:13, it was much darker and starting to get warm.

On an unrelated note, the board was actually measuring the board temp, not the ambient one, since the sensor is a very small SMD chip. It wasn't that hot inside! image

 

image

 

The data loaded consistently, the charts updated in real time, and the CPU and memory weren't that stressed. Great success!

 

Image recognition

 

Another thing I wanted to try was an image recognition software. I would like to integrate this within my existing IoT home 'network', by using the same Firebase database. The Raspberry would analyse data from the camera and this data could trigger actions on another device like keeping a light on if it detects a human in the room.

 

I want to use a camera for this application for these 2 reasons:

  • possibility to also use the Raspberry as a security camera (record video to a hard drive if it detects people). This would be helpful if for example I had a porch where I would want the light to stay on as long as I'm there, but at the same time record video at night in case there's a burglar (why I got a camera with infrared capability)
  • for the same example with the porch, I would want the light to stay on AS LONG AS I'm there, not just momentarily when I go there, as it would with a PIR sensor. Also PIR sensors have some field of view issues and various sensitivities, things that a camera would fix.

 

For the image recognition, I found this project on GitHub by user EdjeElectronics. It is a python script based on the TensorFlow machine learning library from Google and provides a detailed tutorial for the installation process and source code for connecting everything together. It also uses an already existing model for the object detection, meaning what a person or several items (clock, refrigerator etc.) "look" like. You don't have to train the model from scratch so the algorithm would "know" what a human looks like.

 

The way this program works is it takes a live feed from the Pi Camera and runs the inference model on individual frames from the camera. This inference reports an array of objects it has detected, the certainty with which it "assumes" that what it detected is that certain object, and coordinates of where in the picture the objects were detected. Then the program draws nice boxes around the objects detected using OpenCV. There is also an FPS display in the corner. It will detect multiple objects, as can be seen here (test image from the TensorFlow website):

image

 

Installing everything went ok on my first attempt, keeping in mind that TensorFlow 1.13 is available pre-built to install for the Pi, while the latest version is 1.14 and 2.0 is in the beta. The 1.13 version worked ok but I had problems when I decided to reinstall the OS to get the full SD card available. Due to the Raspbian update from the beginning of July (with the launch of Pi 4), OpenCV failed to install and I also had to try several times to install TensorFlow. Finally after getting everything running, this is how it looks on my setup:

image

I'm 87% a person, yay! image Excuse the coloring, this is due to the camera running on infrared because of the low ambient light in the evening. Also to note, the 1 meter camera cable didn't affect video quality at all.

 

Straight away we can notice the very low FPS below one per second. By default the python script runs the camera at 720p continuously capturing JPEG images. Lowering the resolution gradually, down to even 240p, does provide slightly higher framerates but just up to 0.8 FPS. Also increasing the resolution to 1080p lowers the FPS to around 0.5. I decided to leave it at 720p.

 

Now to add the data to Firebase is very easy. I just add the connection to my database, and for every image captured I send new data to the database indicating if a human is detected or not. I used code taken from the concentrator project (REST API) and this got me to a result of around 0.18-0.2 FPS (one every 5-6 seconds). Terrible performance which would clearly benefit from running things asynchronously, but anyway, here's a sample:

image

Worth noting that it doesn't need to see an entire human body or whatever object it's detecting to identify it. This means you get to be a little more flexible with the camera placement.

Also you can see that the RAM usage (red chart in the taskbar next to the clock) is almost at full. While the CPU could probably handle more, clearly the RAM is the bottleneck in this case. Also you can see in the temperature chart that when it goes red, CPU is throttling. Not sure why it throttles at 50 degrees though, as I would expect it to happen at 80.

 

Anyways, same script no longer detecting me and reporting state via Firebase. See, it picked up my fridge image

image

 

And here is the concentrator script, altered from my earlier example to pull the new data from Firebase. I ran this on a separate PC since the raspberry obviously wouldn't handle both tasks at the same time. You can see where it first detected me at 22:46 (the timestamps display the day of month and not the seconds for some reason). Followed by a few minutes of silence since the script on the Pi was killed (low memory I assume), and then at 22:50 I restarted the script and you can see me getting in front of the camera again.

image

 

It is also worth mentioning at this point that I installed a version of TensorFlow intended for CPU processing. There is another version which does processing on the GPU but it is sadly not available for the Raspberry. There is a third version, TensorFlow Lite, which works in a different way and is tailored towards mobile devices and IoT. I figured I'd give this one a shot too and see if it brings any performance optimizations. Benchmarks on the net for the Pi promise 2-3x better performance compared to the regular library!

 

TensorFlow Lite for Python is bundled with the regular TensorFlow Python package, but it is disappointingly broken for the Pi. It crashes as it expects some NEON support function, but apparently the library for that wasn't linked when building the official TensorFlow package for the Pi. NEON is related the vector arithmetic core in the ARM CPU, so pretty mandatory for speeding up advanced math calculations. Awkward moment!

 

I tried to build TensorFlow Lite on the Pi but to no success due to RAM limits. I tried to build it on a separate PC running Ubuntu for literally >2 weeks but failed miserably. Things that went wrong:

  • the configuration was broken and things needed changing in the makefiles
  • the particular targets for building for the Pi needed some workarounds
  • more and more packages were missing
  • the docker build from Google's website compiles for an older version of Python and for some reason won't install on my Pi
  • the build was configured to only work with old versions of bazel, Google's build tool
  • the build had unit tests generated and executed to make sure that everything was working, but they weren't building even though the library I needed did build at some point

The build process is very long and tedious, not that well documented, and I have encountered several bugs while building of which most or all were tracked on Google's GitHub, but some without official fixes.

 

This goes to show how complicated things are in the Linux world. "Open source, download sources and see for yourself that we don't do shit, build for yourself and run" doesn't really work in the real world, where people aren't really deep into what they're doing. Eventually I gave up due to time constraints for this review, but I may try it again at some point in the future.

 

Directions for improving this project:

  • doing the REST API asynchronously
  • capturing video and processing images asynchronously to allow 30 FPS
  • it could just output the results (human/no human) instead of showing a video stream and the data can be processed externally (in the cloud or by another device)

 

Windows 10 IoT Core

 

So far it seems to me that this is a very stripped down version of Windows, which allows you to run Windows apps (basically write them in C#, take advantage of .Net, Azure Technologies etc.). But they need to be build for ARM and therefore regular apps meant for x86 will not work here.

Seems there is no switching around windows and launching apps, so development will not be done directly on the Pi. Rather, you use your regular PC to develop an app, push the app to the Pi and then the Pi displays only that app. My feeling is that Windows would be much more limited than Linux on the Pi. Dual boot seems to not provide any benefit at this point.

 

So far I have failed to get to boot Windows 10 IoT Core several times. Installation requires you to download an application on your PC and use it to write the SD card. Done. However whenever I put the card into the Pi, it just wouldn't boot and remain stuck at the "rainbow" screen. I am not sure how Windows works and would like to see someone using it, but for me it has been too much time wasted on installing (clicking next, next, next) just to not have it work in the end without an error I can google. This is anyways none of Raspberry Foundation's fault and going back to my previous statement, Linux is much better supported for the Pi so I will stick to that.

 

Comparison with other Pi boards

 

Out of the entire roster of Raspberry Pi boards, I find the Pi 3 A+ to be the choice for me due to it being a good compromise device between performance, size and cost. All other devices perform better in some of these 3 points, but are lackluster in the others. The A+ is a "Jack of all trades, master of none", if you will. Following, a more detailed comparison:

 

Pi 3 B+

 

The A+ and the B+ have pretty much the same hardware. This is a choice between size/cost vs performance:

  • the 512 MB of the A+ makes it feel very limited if you want to do any kind of multi tasking (looking up on stackoverflow while writing code).
  • the single USB 2.0 port makes it also a bit weaker for developing. If you have to connect a keyboard and a mouse, maybe even a USB flash drive, they will all be slowed down due to using the same HW interface on the CPU. For instance I saw my wireless keyboard bugging up and registering "ghost" inputs when connecting it via a hub alongside a USB drive.
  • the B+ has the ethernet port. May be better for applications which require no radio output, otherwise the speed you get from it is comparable to WiFi.
  • the A+ comes in a much smaller physical package, so it is easier to fit in whatever custom enclosure if your application needs this.
  • the A+ is cheaper - 11 euros difference in my country. Costs can add up very fast if you need to use several boards in a project or you intend to use it commercially.

 

Pi 1, Pi 2, Pi 3 B, Pi Zero

 

There is not much to compare. The Pi 3 A+ is almost in every regard better than any previous generation

  • Pi 3 B and Pi 3 A+ are the only ones providing wireless connectivity and a multi-core CPU
  • you may be able to get the older ones for cheaper than the current generation but it would be a niche case where the performance hit doesn't affect your application
  • the previous generation Pis would only make sense in a new project if you already have one lying around

 

Pi Zero W

 

Going back to the A+ vs B+ argument, the Zero W takes the A+ and goes way further by reducing size and cost.

  • if performance is a requirement, the Zero W's 1 GHz single core absolutely blows compared to the A+'s quad core 1.4GHz
  • if price or size is a deciding factor between the B+ and the A+, might as well go for the Zero W instead. 15 euro cheaper for my country than the A+ and wayyyy smaller. You can get THREE Zero Ws for about the same price as ONE B+ board.
  • the Zero doesn't have a ribbon cable display connector.
  • due to the lower perfomance CPU and limited physical connectivity, the Zero W is preferable for power usage. It is still not low power enough to be long term battery powered.
  • also for some applications the thermal footprint due to low power consumption may become relevant.

 

Pi 4

 

While writing this review the Raspberry Pi 4 got released and I got a bit jealous of its incredible performance. It is going more in the direction of a low power computer than an embedded device. So for IoT, I feel like there are limited use cases which can benefit more from the Pi 4. Further comparison points between the Pi 4 and the Pi 3 A+:

  • faster CPU and multiple RAM options for the Pi 4. This would enable better SW compilation times, better live image processing performance, the ability to browse stackoverflow AND listen to youtube music while writing code image
  • WiFi 802.11ac and gigabit ethernet - you can stream A LOT more data if needed.
  • Bluetooth 5 vs BT 4.2 on the A+ - improvements to speed and range apply only to BLE devices. Otherwise this adds the possibility to connect 2 audio devices, which again, few applications can benefit from this.
  • USB 3.0 would help a lot if using an external hard drive to save data (i.e. camera stream at better resolution, for longer durations). It will also make it possible to use a swap partition for RAM, but not that necessary if you get the 4GB variant.
  • double micro HDMI ports instead of just one, and they are BOTH at 4k 60FPS. Good for developing, but unless you plan to make a Pi based TV box, not that useful in a final product. Also having to buy a micro HDMI to HDMI adapter or cable adds to costs.
  • OpenGL ES 3.0 hardware support. Might see interesting and far more complex graphical interfaces maybe even games developed due to this.
  • the Pi 4 has more demanding power draw requirements and uses a USB-C connector, so extra costs to be expected here.

 

Final Impressions

 

Official documentation and supporting documents are a major letdown for this board and improving this doesn't seem to be on the radar for the Raspberry foundation. With this in mind, it is hard to develop anything too serious using this board, and most people anyways use it as a "learn to write python stuff on it, make a demo project, but then leave it in a drawer forever".

 

With that being said, it is still a very capable board exceptionally cheaply priced. I am happy to report that I have found a proper spot for the Pi 3 A+ in an IoT context. These are what I believe are major use cases and where it would make sense to consider this Pi board:

  • learning device -> probably not the best idea solely due to the low RAM and a single USB port. A Pi 3 B+ or Pi 4 would be so much better in this regard and the code will most likely be 100% compatible.
  • image processing -> can yield satisfying results, one of the cheapest solutions out there
  • voice recognition -> same as image processing. Need a USB microphone though.
  • aggregator in a network - where it collects/processes data from several other devices and possibly provides interface to a user -> this is where it really shines as an alternative to All-in-One or full fledged PCs due to its small size and cheap price, but good enough performance.
  • "pure" embedded device - by this I mean doing stuff such as sensor input, motor control etc. that doesn't leverage wireless connectivity, display connectivity or processing power -> these tasks can be done on far cheaper, less complex, 8 bit devices like an Arduino. There are more peripherals available and they are so much better documented on other architectures.
  • battery powered device -> even though it is possible to have the Pi running without a display and there are various means to minimize power consumption, it still wouldn't make sense to use the Pi in a battery powered application because you would still have to charge it once a day or more often.
  • software development platform for a professional custom HW product -> since the CPU is not freely available on the market, it is not possible to use the Raspberry Pi as a development board to build a prototype product, and then migrate to a custom PCB/mechanical casing to launch a "professional" product. This would be possible for e.g. the Arduino, where ATmega microcontrollers are available on the market. You want to use the Raspberry for whatever reason, you have to stick with the Pi board.

 

I hope that people reading this review will find it useful in deciding if this board makes sense for them.

I would like to thank element14 for this learning opportunity and for giving me a chance to provide something back to the community. I also get to keep a cool device after all this! image

Anonymous
Parents
  • Hi Florin,

     

    Your findings regarding i/o libraries rings similar to my findings too - several locations recommend gpiozero, but it's half-baked. It's more complex than WiringPi, and WiringPi is more capable. Also gpiozero is missing I2C (unless it has been introduced recently). Plus, many newcomers to engineering will come via Arduino, and wiringPi looks more similar to them, so less of a learning curve.

    I had started using gpiozero, but I've gone back to using wiringPi again.

Comment
  • Hi Florin,

     

    Your findings regarding i/o libraries rings similar to my findings too - several locations recommend gpiozero, but it's half-baked. It's more complex than WiringPi, and WiringPi is more capable. Also gpiozero is missing I2C (unless it has been introduced recently). Plus, many newcomers to engineering will come via Arduino, and wiringPi looks more similar to them, so less of a learning curve.

    I had started using gpiozero, but I've gone back to using wiringPi again.

Children
No Data