Weller Soldering Station WT Series - Review

View table of contents ...  

RoadTest: Weller Soldering Station WT Series

Author: dimiterk

Creation date:

Evaluation Type: Workshop Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?:

What were the biggest problems encountered?: The only issue that was encountered was the lack of a set of tips for the WP90 soldering iron. The new tips feature a different design.

Detailed Review:

This road test will focus on the Weller WT1 soldering iron station I received from Element 14.

This is the 90W version with the North American power plug rated at 120W.

The photos below shows the Weller WT1 that was given for this road test.

 

The WT package is comprised of the:

 

  • Soldering iron WSP-80
  • Soldering station WT1N
  • Soldering iron holder WSR 201

image

Unpacking

 

The soldering iron station is named the WT1N rated for 90W. The version I received uses the short LT series tips. I was surprised to actually find only a single bevel edge tip came with it.

The WSR and the WPT80 come in their own separate boxes.

imageimage

The soldering iron safety rest was unboxed next.

After setting up the soldering irons station ,the unit was turned on and the first thing you'll notice is the LED display,  with a well lit white background and black letters.

Unboxing the unit, shows that the soldering station is tucked well with the power cord in the bottom as well as the accompanying Weller manual.

imageimageimage

image

 

Soldering Iron station

It's a bit tough to show this on the photo but the display has options for a thermocouple, an NFC connection as well as for a fan speed. The temperature rate of change is shown by a vertical bar on the LED.

Probably this unit does not support such options and the display is shared with higher end models.

imageimage

There is a rubber holder on top of the unit that allows stacking additional units on top.

imageimageimage

imageimageimage

imageimageimage

 

This is quite useful since it saves quite a bit of space. The unit has 4 buttons on the front panel as well a high contrast LCD display.

 

The first button returns to the main menu. The next two buttons (up, down ) are used for adjustment while the last button is used for selecting.

imageimage

 

The default temperature is in Fahrenheit so for those that feel challenged in converting to Celsius you need to follow the steps below.

So to convert to Celcius, press the last button, move to the offset menu and press the up button to set the degrees in Celsius scale.

imageimage

 

The RJ11 connector at the bottom is used in conjunction with the Zero Smog extraction system.This part is procured separately . I did not get to test this since I did not receive this equipment from Weller.

As with all soldering equipment it is suggested that the user use a fume extractor when working on these projects.

 

The other connector is a 3.5mm jack that is used for grounding for ESD purposes.

 

Soldering Iron WSP-80

The soldering iron has a temperature sensor embedded below the soldering iron tip.

Even though the soldering iron has a small mass, it heats up relatively fast. In less then 10 seconds it jumps by almost 100 deg.

imageimageimage

The handle is quite comfortable to touch. When I turned on the unit for the first time I heard a humming/hissing sound coming from the bottom of the soldering iron. This stopped after a minute or so.

 

imageimage

 

 

There are differing opinions on choosing between a brass wool and a sponge. It should be noted that the bras wool will affect the tips' life.

The stand and the station are separate pieces which allows for flexibility in how you can set it up. The soldering iron chord has a length of a bit less than 1m.

 

The LT series tips can be procured from the usual CM for around $12 CAD each. As was mentioned only one bevel edge tipcomes with he unit.

imageimage

 

 

Quick tip: Using a high temperature shortens the life of the soldering tips so aim for a medium range temperature.

 

Iron Holder

The safety rest is quite sturdy and heavy. It comes with a metallic stand used to hold the tips that can be attached via screws.  . I ended up replacing the sponge with the brass sponge for cleaning the iron’s tip.

imageimage

The safety rest for the soldering iron is called the WSR. (Weller Safety Rest). It comes equipped with a brass wool and a yellow rectangular sponge as well as a holder for the iron tips.

Personally I like the brass wool. The main disadvantage of the sponge is that wetting the tip imparts a thermal shock on the tip which requires a second or two for it to reheat again to the original temperature.

 

 

Project

After unboxing and setting it up , I decided to solder some 0.1inch male headers to a couple of MEMS microphones. This scenario represents the most common situation encountered by intermediate users.

imageimageimage

I tested the unit on:

 

a) 4 MEMS microphone breakout boards

b) 32 SMD components on a custom ESP32 board I build recently

 

The bevel edge tip worked fine for all 0603 and even 0402 components as well as the IC's with the castellated pads.

I had to use a hot-air gun for one QFN24 package. Even a fine tip would not have worked in that case.

 

Comparing with the low end model I have been using so far one can notice that the better temperature stability and fast setting time of the WS1  makes the soldering joints easier and better.This basically means no cold solder joints in practice.

 

Final comments

All in all I like the fast heating time, the ergonomic design of the soldering iron and the sturdiness of the safety rest.

At this price point I would expect that Weller had also included a fine tip for use in soldering fine pitch components however all the components included are top-notch quality.

This is a product which is definitely recommended for the seasoned professional or for the hobbyist working in his home garage.

 

Pros:

  • Great temperature control
  • Fast settling time.
  • High contrast LED
  • Good ergonomic design
  • Excellent construction for stacking up units
  • Programmable parameters such as sleep time, offset ..

 

Cons:

  • More expensive than other models
  • Only 1 tip with the soldering iron
  • No accelerometer on the soldering iron so unit cannot tell when it's at rest. This is alleviated by the fact that the unit can be programmed to enter sleep mode so no biggie.
  • Supplemental Operating Instructions printout not included on the box
Anonymous
Parents
  • I see from the RoadTester listing, ,we are both on the same journey of RoadTest the Weller solder station. Can I get some confirmation/clarification on the components in your system. You make the following commentary in your opening statement that causes me some confusion.

     

    "The soldering iron station is named the WTP90 which presumably stands for 90W. The version I received uses the short LT series tips. I was surprised to actually find only a single bevel edge tip came with it. The WSR and the WPT80 come in their own boxes."

     

    image

     

    I received a WSP80 solder pencil with a WSR200 Safety Rest. The WSR200 Safety Rest packaging indicates the Rest is for the WTP90 solder pencil.

     

    The whole unit I believe is referenced as a WT1012 and not a WTP90 as you indicate. This link https://www.weller-tools.com/professional/USA/us/Professional/Soldering+technology/Soldering+stations/Soldering+stations…

    on the Weller website seems to confirm my suspicion.

     

    My WSP80 pencil came with a chisel tip T005 44 405 99 LT B as referenced in the manual.  The test subjects who evaluated the unit would have preferred the concial long tip T005 44 406 99 LT S.  I placed an order for these tips.

     

    Break..Break...

    Since you have the correct Safety Rest for the solder pencil, can you confirm an operation for me.

     

    image

    The image is from a tag found with my unit. It does not reflect the Safety Rest configuration I have but does show the barrel and tip assembly.

     

    If I remove the barrel from the solder pencil, (still containing the tip), and place it vertically in the circle holder on the Safety Rest, the tip rests on the sponge. The distance is not sufficient to keep the tip from touching the sponge. Also the holes in the circle holder that supports the barrel are too large in diameter to hold the tips only, the tips fall through.

     

    Can you confirm in your Safety Rest does:

    1. the barrel & tip assembly touch the sponge while sitting in the circle holder

    2. the circle holder actually hold a tip without a barrel.

     

    I made note of the component errors in my review Weller Soldering Station WT Series - Review  but did not include all the above commentary. If the Safety Rest and pencil are a mismatch then issues are due to arise. I'm curious to discover if the difficulties I describe, actually exists when the Safety Stand is matched to the correct solder pencil.

  • Sean,

    Weller stands usually fit the iron like hand in glove. I think your suspicion - that the stand you have isn't matching the iron - is correct.

     

    I have an iron, a heat gun and a desolder iron here from Weller (they came in one kit), and they all 3 have different stands that are designed specifically for the tool.

     

    image

Comment
  • Sean,

    Weller stands usually fit the iron like hand in glove. I think your suspicion - that the stand you have isn't matching the iron - is correct.

     

    I have an iron, a heat gun and a desolder iron here from Weller (they came in one kit), and they all 3 have different stands that are designed specifically for the tool.

     

    image

Children
  • I suspected as such.

     

    Knowing the mismatch, I didn't think harping on the issue provided any value in the RoadTest Review. It would have been nice to match the pants with the shirt so to say.

     

    I am a one tip kinda guy, so a Rest with flexibility to hold multiple bits is redundant. I guess it would be a good place to store a spares.