Raspberry Pi 3 in a Box - Review

View table of contents ...  

RoadTest: Raspberry Pi 3 in a Box

Author: robogary

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?:

What were the biggest problems encountered?: 1) Noobs uSD card failed on first powerup. 2) Adventures in Raspberry Pi 2nd Edition printing 2015 was included. The 3rd edition was available 3 years ago. 3) The resource help site for examples & videos: https://www.wiley.com/go/adventuresinrp2e and https://www.wiley.com/go/adventuresinrp3e did not work .Showed a 403 ERROR The request could not be satisfied. Request blocked. We can't connect to the server for this app or website at this time. 4) Adventures into Python had a couple roadblocks, no Python IDLE in the Raspian GUI Menus. found this Forum advice: https://www.raspberrypi.org/forums/viewtopic.php?t=245120 The advice worked ! The adventures rolled on, 5) Chapter 9 had missing/inaccurate information in the manual, and no way for a young user to get resolved. Ch 9 Part 2 missed a step to install the VLC module (pip3 install python-vlc) . It could have done more to show how to get files transferred from a memory stick or other computer. Ch 9 Part 2 The LXTerminal command line was incorrect for running jukebox1.py, please seereport details. Ch 9 Part 3 should show a detailed schematic of the pull down resistor pushbutton circuit.

Detailed Review:

Arrival of the Raspberry Pi In a Box , initial findings

  • The kit is well protected in stylish sturdy packaging.
  • The kit is complete with a nice looking contemporary styled case of raspberry and white. The case has component markings to label needed input connectors.
  • The matching white power supply is plainly marked 5.1V  2.5A , so I know its going to work well with the Pi.
  • Altho I prefer wireless mice and keyboard, the wired mouse and keyboard are helpful to younger folks to keep track of these accessories.
  • The mouse is a nice size and comfortable. It is good for little hands, with big right and left clickers, an index roll, and pushbutton.
  • The Quick Start Guide was used to wire and get the Pi going. The Quick Start guide has an oddly worded description for connecting to WiFi, but no matter, the Raspberry Pi walks the user through it on boot up.
  • On power up, it took about 25 seconds to show Noobs splash screen. Click to install Rasppian Debian, took 23 minutes for OS to install. Took 9 minutes to walk thru setup and do automatic updates.
  • The book included in the box is: ADVENTURES IN RASPBERRY PI  2nd Edition

                                  Chapter 1 Now What ?

                                  Chapter 2 Taking Command

                                  Chapter 3 Scratch

                                  Chapter 4 Turtles

                                  Chapter 5 Python

                                  Chapter 6 Minecraft

                                  Chapter 7 Sonic Pi

                                  Chapter 8 GPIO

                                  Chapter 9 – JukeBox

 

My Overall first impression SUMMARY, the Adventures in Raspberry Pi book has a ton of relevant information, the chapters ordered in a logical progression.

The chapter topics geared to younger audiences with fun cartoon helpers , relevant examples, and direct straightforward explanations of keywords.

After reading and doing the book’s raspberry Pi adventures, I can summarize the experience as “Great Googily Moogily that was really fun ! “  It is thoroughly enjoyable and I learned a lot. 

This book is good for new users, explaining basic terminology and gradual easy steps. The content may  be tough for an eight year old to follow, but a eleven year old or so could dig right in ( in my humble opinion).

The Raspberry Pi case can be taken apart several different ways to allow access to the insides for whatever project you're working on. 

imageimageimageimage

imageimageimage

imageimageimage

 

imageimageimage

 

 

 

Road Test Details:

The book is a bit out of date with regard to screen shots of the menus and programs, but that seems to be the norm anymore as things change so fast.

It didn’t include the Preferences menu with the Raspberry Pi Configuration GUI , and my baseload used mu and Thonny Python rather than Python 3 IDLE.

 

Chapter 1 includes the RPI basics command line, menus, proper shutdown of the Raspberry Pi, and about using Win32 disk imager to make backups. A great suggestion.

 

Chapter 2 – essential for command lines. Excellent chapter

 

Chapter 3Scratch. I basically knew Scratch, but I learned more of programming blocks and had FUN doing the adventures.

I tend to skim over things that I’ve seen before, but not this time. I was riveted.  See my screen capture and video.

 

Video link:  https://youtu.be/GSWQF5pCmuw

image

 

Chapter 4Turtle graphics. A cute simple sneaky way to teach the concept of variables and loops, and again is a ton of fun. No skipping examples, they are too engaging.

Moving onto Python had a roadblock, no IDLE in the Menus.

I kept trying to reinstall Python until I found this Forum advice on getting Python IDLE to show up in GUI menus: https://www.raspberrypi.org/forums/viewtopic.php?t=245120

The advice worked !  The adventures rolled on, my adventures looked like the book.

 

Video link: https://youtu.be/V8MaUNY6hkM

imageimageimage

 

 

 

Chapter 5 Python - A very good introduction to python. The adventure games are a very fun way to learn code and spark the creative imagination.

 

Python 3 IDLE is in the NOOBs baseload, but doesnt  show up in the RPi menus. Go to LXTerminal and run  sudo apt install idle   Then it will appear in the programming menu list.

 

The handle_room function is introduced. I got carried away with the descriptions , badgering and trolling the user (me).  As the textual adventure built up in complexity, I need to sketch a storyboard / map / flowchart to keep the code development organized. I wish this chapter introduced flowcharting ( or one lines) as a way to plan out the game and routes, thats how I planned it out.

 

Chapter 6 Minecraft - This is the largest selling video game ever. The allure still escapes me, but my kids loved it.  The Creeper is everywhere. Its very important to bookmark the page 132  Table 6.1 Minecraft Pi Controls.

image

 

Chapter 7 Sonic Pi - Sonic Pi section is another unique way to use coding concepts to do something fun musically.

Sonic Pi adventure exercises are hard to put down.....then I found some more online examples hehehe

A music teacher can use a Pi as an instrument of learning (pun intended).

Nintendo Mario Program played using Sonic Pi, my video:     https://youtu.be/HCTm2RkL3bQ

 

imageimage

 

Chapter 8 GPIO – a surprise ! page 179 shows a parts list and places to order them.

Its OK, I’m a road tester, and have my own stuff on hand. Page 190 shows mapping an input from the keyboard, now we’re talking !

 

This topic is always confusing because the GPIO pins can be defined 2 ways.

GPIO will also be a challenge, to be successful, the case needs taken apart. Hopefully its not a big deal for the youngsters.

Difficulty level also depends who you have helping. 

 

imageimage

 

Anytime I work on a project using real IO , I always make a IO map. It helps in programming, in wiring, and in troubleshooting. 

imageimage

imageimageimage

imageimage

 

An example video of the GPIO Adventure, a 10 LED bar strobing when the Pushbutton input is pushed.

The scan LED loop continues as long as the pushbutton is held down, see video here : https://youtu.be/lGuy86hV4jo

 

Chapter 9 - THE BIG ADVENTURE ! Building a RPi Juke Box.

 

  • Changed Hostname to: raspberrypi_in_a_box. bad move  :-)  see fix in part 2

 

     9. Part 1: The LCD Screen

  •           I dont have a 2 line LCD on hand for this build, try using a "Nokia 3310 style" Geeetech 5110 LCD matrix 

                    https://www.geeetech.com/Documents/Nokia5110%20datasheet.pdf

      

                    Adafruit has nice tutorials and example code on this matrix LCD

                 https://learn.adafruit.com/nokia-5110-3310-lcd-python-library

                 https://learn.adafruit.com/nokia-5110-3310-monochrome-lcd

            

               to see Nokia 3310 wiring diagram to the RPi, loaded Fritzing tool to the Raspberry Pi   sudo apt-get install fritzing

                                    image

          install driver libraries:

 

  •      Sudo pip3 install Adafruit-Blinka

         image

  • Enable SPI in the Raspberry Pi Configuration GUI.

 

                                   image

The Hello World is provided from a sample program named  pcd8544_pillow_demo.py

 

  9. Part 2: Downloading and playing MP3s

          I choose to use personal mp3s rather than download music from freemusicarchive.org

             The Book suggested to create a music directory, however the NOOBS installation creates one already.

 

               When Transfering mp3 files from my PC to the RPi using WinSCP – My HOSTNAME had underscores & didn’t work correctly. Shortened to raspberrypiBox

               NEED SSH turned on to connect with WinSCP to transfer mp3 files.

 

               The mp3 file names can’t have spaces or punctuation characters when using LXterminal commands to run VLC.

image

 

once I broke down and connected via wifi,  scrot command could be used to get screen captures and transfer back to my W10 PC rather than taking pictures with a camera.

 

9.2.a Next Problem : Following the example Page 208 in the book to run Write a JukeBox Python Program

      Figure 9-7 on page 211  ( calling VLC inside Python )  the first line of code is import glob, random, vlc

     On RUN, python throws a ModuleNotFoundError: No module named VLC  however VLC is installed and works from its GUI.

solution: From LXTerminal type:   pip3 install python-vlc    refer to:   https://discourse.psychopy.org/t/no-module-named-vlc/6546

 

9.2.b Next Problem : Following the example Page 208 in the book to run Write a JukeBox Python Program

      Figure 9-7 on page 211  ( calling VLC inside Python )   the second line of code

if len(sys.argv) <= 1:

    print ("Please specify a folder with mp3 files")

    sys.exit(1)

 

If the user enters $ python3 jukebox1.py   as indicated in step 11 on page 211   sys.argv will always be 1  , the jukebox1.py program will always exit

solution: The proper LXTerminal command is $ python3 /home/pi/Documents/jukebox1.py  /home/pi/Documents/music

 

9.2.c Next Problem : Following the example Page 208 in the book to run Write a JukeBox Python Program,

the code will appear to not work, but does work .....if enough description is provided in the print statement

When the button is entered in the keyboard it has to be entered with quotations to work.

 

refer to lines of code

button = input ("Hit a Button" )

if button == "1"

print ("pressed play button")

solution: Change the code    button = input ("Hit a Button" )   to  button = input ("Select a number from 1 to 4 , type in quotation marks around it before pressing ENTER" )

 

 

Even tho the command line error message said connection refused, the audio files still played.

image

 

Chapter 9 Part 3 - Controlling Jukebox with pushbuttons.

 

Because I used a different LCD display that the book listed, my GPIO assignments and wiring are different, from the Adventures in Raspberry Pi book. 

Again, this project shows why doing a IO map for maker projects is so handy.

As the project gets built, it is so easy to see what IO spots are available,and keep the list updated as features get added.

 

Part 3 GPIO buttons patched in the jukebox1.py  easily, no problems with part 3 at all !

I do suggest to the authors to include a schematic of of a push button using a pull down resistor.

image

 

Chapter 9 Part 4 - The Fabulous Finish Displaying Jukebox info on the LCD screen.

 

Since I'm using a matrix LCD screen ( a screen that can do graphics ) alot of my code is different than the book.

I enjoyed alot of adventure rewriting the python code to use digitalio library rather the GPIO library, and creating variations of LCD screens.

For example to display splash screen RPi JukeBox , and then display PLAY, PAUSE, BACK, FWD when those buttons are pressed.

    imageimage

I thought this was a fun and meaningful project for learning python. The coding learned can be applied to other projects I have in process.

 

%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%

%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%

 

After completion of the projects in the provided book, the test plan was to also do an additional project not done in the book.

 

I ended up installing digital communications ham radio software and operating using the Raspberry Pi in a Box as the radio station PC.

None of the software or project material I worked on in the Adventures book were removed.

Installation instructions are provided per this website, and software was so easy, I couldnt believe it.

image

This is a photo of the Raspberry Pi in a Box, in operation, with an FT8 digital contact is in process.

The red lines in the screen show a received message with my radio call sign in it.

image

Just use your raspberry Pi menu, select Preferences , install software

search for fldigi - install it, then search for WSJT and install it too.

image

 

 

image

 

 

image

The software even creates a menu selection

image

The most important configuration item for each digital software package is to setup the audio interface.

In my case I use a signalink USB (external soundcard) that connects from a PC USB to the radio ( either the microphone input of the radio or a dedicated sound card input jack depending on the radio).

image

 

image

 

Here is a screen capture of a radio contact on a Raspberry Pi 3B using FT8 mode in WSJT software.

image

 

 

 

 

Here is a screen capture my 1st contact on a Raspberry Pi 3B using PSK31 mode in FLDIGI software. The other radio operator is in Portugal.

image

 

Thanks this was a fun road test

Anonymous
  • If you are a person that dabbles in Ham Radio then your Pi with a antenna kit and dongle will open up the world of SDR (software defined radio). This subject matter is ideal for people that have a knowledge of RF and like to explore.

     

    I am not a Ham Radio operator myself. I have an RF background from my days in supporting aviation electronic systems. I did work a little bit with Ham Radio in the early eighties. If SDR piques your interest rtl-sdr.com is the site to start with. It is the definitive place for all things SDR. I have purchased their antenna and dongle to develop a few computer magazine articles on SDR and GNURadio.  I registered at the site for a weekly email summary of activities in the world of SDR.

     

    Some of the projects require some CPU horsepower. I have successful gotten some of the software to run on the Pi. GNURadio is a software project that was developed to replace much of the physical test equipment in an RF electronics lab with a software. Checkout the project gnuradio.org. It is another avenue to dwindle away time playing with a Pi and RF.

  • Just added a "postlude" to my road test report, loading digital mode ham radio software to the RPi 3B, connecting to my equipment and making radio contacts with it.

    The Rpi 3B is perfect for a go kit - for portable radio operations.

  • I had heard about the keyboard but never actually seen the unit.

     

    Where did you get the unit?

  • Nice walkthrough of RPi, but be beware of that image lemur, trying to break your USB connection during the RoadTest.

  • This keyboard is very light and thin. It connects to the Pi with a USB connector. There are no other connections for accessories to the keyboard.

  • So on this version of the keyboard I think it is the v1 it doesn't have the external usb port on it to be able to plug in the mouse to it or any other media like usb drives

     

    image

     

    I know your thinking of this official keyboard with the ports if it has a usb wire directly soldered to it instead of a usb mini it won't have it.  So if you buy a kit make sure the keyboard has no wires connected or has a extra micro usb cable in the kit image

  • I recall a comment that in addition to the keyboard being a keyboard it was a USB? I haven't seen you comment on it, so I assume it is not.

  • The keyboard is a wired USB, the same size as the keypad on my laptop, minus the numeric keys.

    It has a good feel, and is a nice white color matching all the other accessories. Did I answer your question ?

  • Nice review. Envious it was a bad boy I was hoping to snag.

     

    Do you have any additional feedback on the keyboard. I understand it is a USB extender also?