PMODTMP2 Temperature Sensor and Thermostat Control - Review

View table of contents ...  

RoadTest: PMODTMP2 Temperature Sensor and Thermostat Control

Author: Unknown

Creation date:

Evaluation Type: Evaluation Boards

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: analog devices tmp36 / sensirion SHT series / Dallas IC DS18B20

What were the biggest problems encountered?: The device performed as expected throughout, there were no significant problems of note. The only downside being a lack of example code but those familiar with I2C devices should be more than capable of writing their own interface software.

Detailed Review:

Preface

 

One of my planned projects is to mod a Bigtrak which was a popular toy back in the 80's and has been reproduced recently, the modification is going to incorporate a Rapsberry Pi. Whenever a computing device is encapsulated it's a wise precaution to include some temperature sensing and some cooling to prevent the system from getting too hot! For this reason I applied for this roadtest and would like to extend my thanks to those involved in selecting my application.

 

I already have a number of temperature sensors but it was the features of the Digilent PmodTMP2 that caught my eye, identifying some features that would undoubtedly add a performance boost over the others that I had considered using.

 

Some of the other sensors would need analog to digital conversion and others would need an entire bus to themselves, using their own protocol rendered them unsuitable to be used along with other devices.

 

One of the things that all of the other sensors had in common was they would all need polling on a regular basis by the main controller which would then have to be responsible for the cooling system.

 

Reasons To Consider This Sensor

 

The PmodTMP2 in this review has the advantage of high temperature and critical temperature interrupts which are programmable to any temperature within the devices range of operation (-40 to +150 Celsius). This means that the main project processor doesn't have to be continuously checking as the sensor can raise an alert if the temperature gets too high.

 

It's not even necessary to alert the main processor in some cases the over temperature interrupt can independently trigger a cooling circuit without any intervention of the main controller. Of course with an additional critical temperature interrupt this allows the processor to be alerted if the cooling system isn't managing to adequately cool the system and the temperature continues rising towards a dangerous limit.

 

The sensor also has the ability to set a low temperature interrupt, one particular example of using this feature would be to monitor a greenhouse during the winter and early spring, if the temperature falls into a range where tropical plants are going to suffer or even freeze then the low temperature interrupt can be used to instruct a heater to turn on.

 

Test Setup

 

To test this sensor I used an Espruino which is one of my go to microcontrollers for rapid testing, eventually I will be using this device with the Raspberry PI but at present there aren't any straightforward libraries which is something that I will address in the near future, I plan on making a simple interface that should be relatively easy to use.

 

Example Code

 

There is a provided code example for chipKit MPIDE and also an external link provided to an instructable for using this device on the Raspberry Pi using Python in conjunction with the smbus library which I couldn't get to work and there isn't any actual example code in the link, maybe I'm not patient enough but I do feel I would be better creating my own control interface.

 

This is the code I used to gather an initial temperature reading using an espruino

 

var i2c=I2C1;
i2c.setup({scl:B6,sda:B7});
var devadd = 0x4B;
var temp_register = 0x00;

function getTemp(){
    i2c.writeTo(devadd,temp_register);
    raw_data = i2c.readFrom(devadd,2);
    data_16_bit = (((raw_data[0] & 0xff) << 8) | (raw_data[1] & 0xff));
    temp_deg_c = data_16_bit / 128;
    return temp_deg_c;
}
}

 

The top parts setup the I2C port whereas the function reads the data from the sensor and stores them as 2 8-bit values in an array which then shifts the 2 returned 8-bit values into a 16-bit variable and finally divides that with a value of 128 to give us the value in degrees C. From here, calling the function getTemp() will then return the temperature data as a value in degrees Celsius

 

 

Like mentioned in the video I'm leaving tomorrow to work away from home for the majority of next week so I won't be able to go any further until then. Once I do get back I'll spend some time getting the sensor to work with the Raspberry Pi and then testing the interrupt function and providing examples, this will all probably happen in a seperate blog but I'll paste a link into the comments below so don't forget to check back and see the progress.

Anonymous
Parents
  • Nice idea to utilise it into something else.

     

    Cna you give me the details of the Esprino board you were using please.

     

     

    Thanks

    Mark

  • Former Member
    Former Member in reply to mcb1

    Sure, you can check it out in the first ever roadtest I did at element14 back in July 2014 https://www.element14.com/community/roadTestReviews/1828/l/espruino-review

     

    Website https://www.espruino.com/Tutorials

     

    distributors https://www.espruino.com/Order

     

    Essentially Espruino is/was the name of the javascript platform that can be installed onto microcontrollers, the Espruino board was made by Gordon who came up with the idea, its basically an STM32 with the javascript runtime installed. The board also has a micro sd slot and prebuilt javascript functions to alliw you to easily save data to it for logging etc.. which wasnt a very common feature even just a couple of years ago.

     

    If you check the website there are compatable javascript modules for the majority of common devices written by Gordon and other users of the devices as well. Theres also a great reference resource for general javascript functions and also the special javascript functions required to use the hardware.

     

    You can only see me accessing it with a Linux terminal but the main way to program it is through a google chrome browser app that has a code editor and a graphical editor that are fully compatable with each other, it beat the codebug and microbit hands down just 2 years ago but was just never up for consideration, marketed wrongly and slightly before the time of that particular market. Shame because its a great little tool.

     

    --------'edit

     

    I think the only downside is the price which is around £20 GBP for not a great deal more you can get a Raspberry Pi, for some it can be difficult to see past the hardware and realise that the easy to use software that makes learning and rapid development simple are part of whats being paid for

  • Cheers

    I did a quick check back on your contents and for some reason I didn't see that one..... ( new glasses reqd )

    I did see the list of hardware it worked with, and that's what caught my eye.

     

     

    You're right about the £20 GBP but even most genuine Arduinos are hovering close to a RPi, however the advantage of these boards is the faster boot and more robust I/O.

     

     

    Mark

Comment
  • Cheers

    I did a quick check back on your contents and for some reason I didn't see that one..... ( new glasses reqd )

    I did see the list of hardware it worked with, and that's what caught my eye.

     

     

    You're right about the £20 GBP but even most genuine Arduinos are hovering close to a RPi, however the advantage of these boards is the faster boot and more robust I/O.

     

     

    Mark

Children
No Data