Arduino Nano 33 IoT Embedded Dev Kit - Review

Table of contents

RoadTest: Arduino Nano 33 IoT Embedded Dev Kit

Author: garymii

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: Nothing at this price point, the other available processor boards do not include WiFi.

What were the biggest problems encountered?: Using the code libraries were easy to find but took awhile to incorporate into an existing script.

Detailed Review:

I like the size of the board and the pin layout, makes it easy to attach to a prototyping perf board. I started out by creating a Temperature controller by using the SPI channel to an RTD driver IC (MAX31865). It was wired to a three wire PT100 RTD attached to a block heater on a syringe containing an adhesive. I easily found a library online for the PID source code and modified the PID values to achieve a precise temperature for the adhesive. By having online libraries for the source code, it was very easy to write a script, upload the PID code, incorporate the code as a state machine, and call it as needed. The next function for the project was to control the speed, direction and distance for two DC brushed motors. An L298 Dual H-Bridge module (also very low cost) was used and controlled by 4 Outputs from the Arduino (PWM is another method for speed control). The code for driving the H-Bridge was also found online and uploaded to the script from a library. Once the basic functionality of the motor driver was confirmed I ran a DOE to determine the ON/OFF times for the 3 pairs of different state machines needed for the slow, medium and fast speeds of the motors and the distances needed. The WiFi was just as easy to setup (from a library found online) and allowed me to monitor the motor speeds and adhesive temperatures remotely.

Over all I found this very low cost Arduino extremely easy to use (I am NOT a programmer) and will be using it for assembly line functionality testing. The WiFi capabilities make this an easy solution and cuts down on the wiring for test fixtures. I was absolutely surprised to learn how easy it was to program by searching online for whatever function you need. I found numerous Websites with Arduino code libraries as well as modules for motor drivers, Temp controllers, LED drivers, Touchscreens, etc. at low costs easily purchased at  Newark, Amazon, Ebay, etc.

Anonymous
Parents Comment Children
No Data