RoadTest: Raspberry Pi Pico
Author: dougw
Creation date:
Evaluation Type: Development Boards & Tools
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: Cypress - InfinionTechnologies PSoC 4200M CY8CKIT-043 has a higher price and lower performance - because the Raspberry Pi Pico sets a new standard for performance at its low price point. Other companies such as Adafruit, Sparkfun, SeeedStudio and Arduino use the same MCU in some of their products, but they add extra features to their modules and have correspondingly a higher price. The Espressif ESP32 is also a good competitor in this low cost microcontroller market.
What were the biggest problems encountered?: The only problem for me so far has been obtaining a Raspberry Pi Pico, but this road test supplies one, so it isn't an issue for this road test.
Detailed Review:
Background - Why Am I Doing This Road Test?
I applied for this road test because I think the Raspberry Pi Pico is the most exciting Raspberry Pi so far, and I had not been able to get my hands on one. I have about a dozen Raspberry Pi computer modules spanning a half dozen different models, but they are all computer modules with HDMI and USB. My activities are much more focused on small microcontrollers and the Raspberry Pi Pico brings a new level of performance at a nice low price point to the application space where I spend most of my time. I fully expect to use more Pico's than any other model of Raspberry Pi.
Just because they are smaller than previous Raspberry Pi models, does not mean they aren't powerful. Here is a quick apples-to-oranges comparison with the original IBM PC:
| Specification | IBM PC | Raspberry Pi Pico |
|---|---|---|
| CPU | Intel 8088 (8/16 bit single core) | RP2040 (32 bit dual core ARM Cortex M0+) |
| CPU speed | 4.77 MHz | 133 MHz |
| RAM | 16 - 64 KB | 264 KB |
| Mass Storage | 5.25 floppy disk drives 160/320 KB | 2 MB FLASH |
| Price | $1565 (16K RAM) | ~$4 |
Some of the things I like most about the Raspberry Pi Pico are its speed, the amount of memory, the form factor, the interface suite and the price.
Even though I tend to use small microcontrollers in my projects, I have been looking for a little more capability for those projects that need it. For example, I would like to start using more Python in my projects but Python really needs more memory than what is in the microcontrollers I have been using. Python may run a bit slower than other languages, so the increased speed of this MCU will be useful to keep performance up. I am hoping the move to python will decrease development time and increase project productivity.
In summary the Raspberry Pi Pico has the potential to both reduce the cost of my projects and reduce the time it takes to complete them. These are the two most important factors in any project (beyond the technical objectives). (Fortunately, I don't need any help with technical objectives.) This will allow me to tackle more projects, because of the low cost, as well as slightly bigger projects, because of the reduced development time, and these are the main reasons I am so excited about this product.
Pico Features Overview
This list of features is well thought out to provide a very flexible platform to address modern microcontroller applications.
Block Diagram of the RP2040 MCU used in the Pi Pico
The Road Test Plan
When I do a road test I like to go beyond simply regurgitating the manufacturer's datasheet and show real applications of how the product is used. In this case the Raspberry Pi Foundation seems to have excellent documentation to get started with a brand new product, so showing product features and specifications has been easy and I can provide links to anything I don't cover explicitly.
My overall objective with this road test is to develop work flows with the Raspberry Pi Pico that will streamline development projects that incorporate this module.
To do this I will develop some real applications and explore how the features of this product can be leveraged efficiently to reduce the amount of work, make development easier and generally improve development performance.
The Raspberry Pi Pico can be plugged into a breadboard but it was also clearly designed to be mounted on a PCB, so I want to show that aspect of it.
In order to make a product into an efficient development tool, requires that we build up reusable IP that we can apply to any future project. This takes the form of libraries and functional blocks both for the CAD interfaces and corresponding software.
One of the neat little twists with the Pico module is its connection interface. It uses both castellated connection points, for surface-mount soldering at its edges, and through-hole vias for standard headers. I want to use both of these connection methods to minimize problems in the development process. In the first stages of powering up a new design, I want to use the through-holes as a temporary socket to test functionality before soldering the Pico to a PCB. It is possible the castellated connections will be better for this than the though-holes, it depends on the diameter of the through-holes. I will design the PCB for both eventualities and show how it works in this blog. Some pins in the "socket" can be removed if that part of the circuit could cause problems, or if those pins only need to be tested later.
The PCB footprint for the Pico will have both though-holes and SMD pads so the Pico can be mounted on headers, sockets, or surface mounted.
Application Features
The PCB I am developing will have the following features:
In this road test I will focus on trying to get the display working, but I want to use all pins in the design so that the PCB can be used for a wider range of future projects.
Schematic Design
In order to design a schematic that implements the features above, we need to decide which pins on the Pico will perform which functions.
Here is a nice graphic showing the Pico pinout:
I find pinout diagrams like this very handy when choosing pins, but I always make a spreadsheet that has pins for each interface to ensure the connections are consistent with device documentation.
The reusable spreadsheet makes it quick to build variants with different features and interfaces by adding columns for new interfaces and selecting which columns will be included.
Once I have entered the various new components into the CAD library, the connection spreadsheet can rapidly be converted into a schematic - like this:
The VS connector is intended to connect to an audio module that also has a mSD card interface - in a future project, but it can also be used to connect any SPI peripheral module.
The BT connector is intended to connect a Bluetooth module in a future project, but it can also be used to connect any serial port peripheral module.
The display connectors include both an LCD display and another mSD card interface.
This gives the Pico access to 2 mSD cards at the same time, opening up the possibility of it being used to clone mSD cards.
PCB Design
I use Eagle so I can design the layout on one screen while designing the schematic on another screen with forward and backward annotation occurring in real time.
For this design I want to put the display, touch screen and buttons on one side of the card and Pico and everything else on the other side like this:
The power switch will be at one end so it can be accessed regardless of which side of the card is facing the user.
This card is simple enough that there are only a few vias.
Note the notch in the top to provide better access to the mSD card under the display.
After creating the Gerber artwork, I transferred a zip of the files to a PCB manufacturer. (PCBWAY)
Within 40 minutes, they had reviewed the artwork and pronounced it manufacturable.
I then paid them $5 to make 10 PCBs.
They emailed me back the next day indicating the build was complete and the cards had been shipped.
I had paid for a courier, so the cards were delivered 55 hours after uploading the files. (it might have been even faster, except it was over a weekend)
I still cannot believe how quick and low cost this whole process is, but it means making variations on the PCB will be quick, cheap and easy.
From left to right this image shows the touch screen, the QVGA LCD the display side of the PCB, the Pico side of the PCB and the Pi Pico
On top is the section of reel tape the the Pi Pico came in. This type of packaging is well suited for automated assembly, if an application were to transition into production..
Note the SMD pads (and through holes) on the Pico side of the PCB that allow the Pico to be surface mounted or header mounted.
I had the LCD and touch screen in stock, which is important, because shipping issues these days could easily have made it problematic to obtain these parts in time to complete this review. Complete touch screen LCDs are available of course, but they are still pretty expensive compared to this solution.
Touch Screen
The touch screen is a replacement resistive touch screen for a Nintendo DS. It is big enough to cover the 2.6" LCD but I also put an extra connector for it on the other side in case I want to make a keyboard below the LCD, without using the display. I may do this for this first build since the flex ribbon connector is not long enough to reach the connector if I put the display in a socket.
For the first build I prefer to use a socket.
I wanted to show how a resistive touch screen can be interfaced to a Pico. The technical reason is that the screen can display a significant amount of text and it needs a cost effective way to enter text. The touch screen is just going to be used as a cheap keyboard.
A resistive touch screen has 2 transparent resistive layers. The top layer has conductive contact along the left and right edges. The bottom layer has conductive contacts along the top and bottom edges. This sketch shows how these contacts are driven differently depending on whether the X position is being read or the Y position is being read. One layer is being driven while one layer just reads the voltage at the touch point. The driven layer has voltage gradient across its resistance, similar to a potentiometer. Here the voltage gradient is shown as a color gradient from red (VCC) to black (GND). The entire layer that is not driven simply goes to whatever voltage is at the touch point.
The pins on the Pi Pico can supply enough current that they can drive these resistive sheets directly without external drivers.
One minor addition is needed, because if the input pins are left floating they could read a random position, so a weak pull-down resistor is applied to each pin, making its default input voltage zero. These pull down resistors are so weak, they have minimal effect on the voltage gradient when a touch occurs. The Pico inputs can be configured with internal pull-ups or pull-downs, but they are strong enough to have some influence on the reading, so I am using external pull-down resistors.
This touch screen is not intended for high speed touch typing or gesture control, it is just a way to add a lot of buttons inexpensively and without using a lot of pins.
Python
MicroPython and CircuitPython are both supported on Pi Pico as are other languages. See the links below for lots of in-depth resources. I tried using Mu, PyCharm and Thonny. All editors worked okay. I had used Mu before and still like it, Thonny is clean entry level editor that I found a bit simpler. The PyCharm link below is a very detailed and accurate step-by-step tutorial on getting PyCharm working properly.
I messed around with MicroPython and CircuitPython for a week trying to get SPI working without much initial luck. When you are using trial-and-error because the documentation isn't clear and example snippets are incomplete and there are a bunch of unknowns, you end up with a n-dimensional matrix of test cases to run through. Compound that with careless inconsistency in the letter case and mistakes in indentation and everything grinds very slowly forward. Digole SPI is not exactly standard, and I couldn't find an example of driving a Digole using Python SPI, plus the variable types were misleading.
After many, many attempts with partial successes, I corrupted something and the Pico would not show up as a USB drive in CircuitPython. Fortunately Adafruit provides a flash_nuke.uf2 utility that recovers from this condition.
Now it is the weekend and I can make a more concerted effort to understand what is going on ... and finally have the SPI display running from CircuitPython:
The code is not pretty, but at least some of the bones are now understood.
# Raspberry Pi Pico CircuitPython Test
# by Doug Wong
import board
import busio
import time
import digitalio
import microcontroller
from digitalio import DigitalInOut, Direction
print ("Init start")
time.sleep(.5)
led = DigitalInOut(board.LED)
led.direction = digitalio.Direction.OUTPUT
MOSI = board.GP11
MISO = board.GP12
SCK = board.GP10
lcdcs = digitalio.DigitalInOut(board.GP14)
lcdcs.direction = digitalio.Direction.OUTPUT
lcdcs.value = True
# set spi pins & configure
spi = busio.SPI(SCK, MOSI=MOSI, MISO=MISO)
time.sleep(8)
while not spi.try_lock():
pass
spi.configure(baudrate=1000000, phase=0, polarity=0)
lcdcs.value = False
spi.write("CL")
spi.write("SF5")
spi.write("TT")
spi.write("---------------------")
spi.write(" Raspberry PI PICO ")
spi.write("---------------------")
spi.write(". CircuitPython .")
spi.write("----------------------")
lcdcs.value = True
spi.unlock()
while True:
led.value = True
time.sleep(0.5)
led.value = False
time.sleep(0.5)
I am attempting to use MicroPython to read the resistive touch screen and display text on the LCD. So far it looks like I have a problem with being able to switch a pin from a digital output to an analog input on the fly. I was trying to save a couple of pins by doing this, but no luck so far - CircuitPython complains that the pin is already in use. I thought I had seen an arduino example where this was done, but will have to explore it later as I want to get something published. I could jumper in a couple of other pins to perform the digital output function, but they are all allocated. It only cost $5 to make a new card, so I will likely do that in the future. I might try to find a faster LCD while I am at it.
Arduino IDE
Fortunately the Arduino IDE already supports the Raspberry Pi Pico, so it uses the standard Boards Manager and is just like adding any other board into the IDE.
The one little twist is that the category for the Raspberry Pi Pico is "Arduino Mbed OS RP2040 Boards", so look for this in the Boards Manager.
The USB port can be used for other purposes than uploading programs, so a method is needed to tell the Pico to enter its programmable mode. The method is to push the BOOTSEL button on the Pico at the same time as power is applied. Contrary to some other blogs, I had to do this pretty much every time I wanted to load a new C++ program.
This is a simple program to show that the Arduino IDE works fine with Pi Pico. The video of it working is in the demo section.
/*
* Pi Pico Demo by Doug Wong 2021
*This demo uses a Raspberry Pi Pico to display text and graphics on a 2.6" Diigole Graphic LCD adapter via SPI
*/
#define _Digole_Serial_SPI_ //To tell compiler compile the special communication only,
//other interfaces available are:_Digole_Serial_UART_, _Digole_Serial_I2C_ and _Digole_Serial_SPI_
#include <DigoleSerial.h>
DigoleSerialDisp mydisp(11,10,14); //SPI:Pin 11: data, 10:clock, 14: SS, you can assign 255 to SS, and hard ground SS pin on module
#define SC_W 240 //screen width in pixels
#define SC_H 320 //screen Hight in pixels
#include "e14RT1.h" // element14 Road Test splash screen image 240 x 320 262K colors
#include "Pico3.h" // Pico module image 240 x 320 262K colors
void setup() {
delay(8000); //wait for the Digole display to go through it own boot and demo
pinMode(LED_BUILTIN, OUTPUT); //set up to flash the onboard LED
mydisp.begin();
digitalWrite(LED_BUILTIN, HIGH); // turn LED on
mydisp.setBackLight(70); //set brightness of backlight as 70%
mydisp.clearScreen();
mydisp.setPrintPos(10, 8, _TEXT_); //locate text cursor near mid screen
mydisp.println("element14"); // print some test text
mydisp.setPrintPos(10, 10, _TEXT_);
mydisp.println("Road Test");
mydisp.setPrintPos(6, 12, _TEXT_);
mydisp.println("Raspberry Pi Pico");
mydisp.setPrintPos(0, 0, _TEXT_);
delay(5000); //wait 5 seconds
digitalWrite(LED_BUILTIN, LOW); // turn LED off
}
void loop() { // this loop alternates between the roadtest image and the Pico image
mydisp.setMode('C'); //set graphic Drawing Mode to COPY
mydisp.drawBitmap262K(0,0,240,320,RTsplash); //display roadtest image
delay(5000); //wait 5 seconds
mydisp.drawBitmap262K(0,0,240,320,picopic); //display Pico image
delay(5000); //wait 5 seconds
}The "Arduino" C++ demo program is actually very short, because all it does is display some text, flash an LED and display a couple of images.
Digole Development Utility
Digole provides a convenient online browser utility to create display content and simulate results.
Here is a quick video of how it works - at least the parts I used:
It will generate display content in a format that Digole displays can use directly, but I had a bit of trouble with it. For some reason the RGB output was shifted by 2 colors, so the RGB bytes were in GBR order. It may just be my misunderstanding about how to use the output file, but to fix this I had to insert a couple of extra color values at the beginning of each image. (2/3 of a pixel)
Hardware Build
The PCB made the hardware build pretty straightforward. I just soldered on a few connectors and switches and plugged everything together.
Demonstration
The main demonstration video shows the Pi Pico displaying text and graphics on an LCD.
Here is the video demo....
Note the slow rate of transferring an image to the LCD. This is due to a couple of reasons:
This slow speed is disappointing, even though I never intended to use it for video - I used SPI mainly because it should be much faster than other serial standards. (The display supports I2C as well as UART)
I am not sure why these pictures didn't turn out as crisp and colorful as the display appears to the eye, but it definitely looks a lot better to the naked eye.
Conclusions
This road test included building the Raspberry Pi Pico into a little system, complete with a QVGA LCD. It may seem a little excessive for a $4 module road test, but the work, the libraries, the PCB and the code will all be re-usable as building blocks or a base platform for other projects and the learning curve will be invaluable in developing new applications.
I like the minimalist Pi Pico module that makes it easy to access all the features of the new MCU without pre-supposing what it will be used for. The small form factor and dual connection interface allows the module to be used in a wide range of applications. The faster speed and larger memory space (than older Cortex M0 modules) provide a lot of flexibility and capability to improve performance and tackle larger applications.
I do have one funny little quibble with the Pi Pico.... Since pico is normally a prefix, I think it just natural to call the module a PicoPi and I would have preferred that to be the name. I think I understand why they didn't use the normal convention, but it somehow makes the name a bit awkward.
Overall, the Raspberry Pi Pico has a well thought out list of features to provide a very flexible platform, able to address a wide spectrum of modern microcontroller applications.
Hopefully this road test provides some insight into the great potential of this new MCU. I think Raspberry Pi Pico is well positioned in price and performance to enjoy wide popularity, which will translate into the availability of extensive support for complementary software and hardware resources. Even at launch the product already has support for multiple design environments and the whole eco system is ramping up quickly. I am happy that that my CAD library part for the Pico has been validated and that the custom PCB worked well, and since I ordered a batch of 10 cards, it will serve as a platform for other projects. I have ordered more of Pico modules and expect to use them regularly. That is a pretty concrete endorsement of the potential I see for the Raspberry Pi Pico.
Relevant Links
Raspberry Pi Pico Road Test page
https://datasheets.raspberrypi.org/pico/raspberry-pi-pico-python-sdk.pdf
https://hackspace.raspberrypi.org/books/micropython-pico Getting started with MicroPython on Raspberry Pi Pico - free book
https://thonny.org/ Python
https://www.youtube.com/watch?v=5l3W-brnO7E&ab_channel=NotEnoughTECHNotEnoughTECH MicroPython on Thonny
https://circuitpython.org/board/raspberry_pi_pico/
https://circuitpython.org/libraries
https://www.youtube.com/watch?v=QywUT3f-_7w&ab_channel=TheMachineShop PyCharm MicroPython installation
https://micropython.org/download/rp2-pico/
https://learn.adafruit.com/getting-started-with-raspberry-pi-pico-circuitpython
https://www.youtube.com/watch?v=5YOEauk9bLo&ab_channel=LearnEmbeddedSystems How to use the Arduino IDE with Raspberry Pi Pico
https://www.youtube.com/watch?v=9vvobRfFOwk&ab_channel=LearnEmbeddedSystemsLearnEmbeddedSystems Using 2 cores on the Pico
https://www.digole.com/tools/digole-emu.php Online tool to create content for Digole displays and simulate results
Raspberry Pi Pico - Review by Tony Goodhew
-
BigG
-
Cancel
-
Up
+5
Down
-
-
Reply
-
More
-
Cancel
Comment-
BigG
-
Cancel
-
Up
+5
Down
-
-
Reply
-
More
-
Cancel
Children