RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Polls Roadtesting the easyE4 Nano PLC: AC or DC, What's Your Preference?
  • Blogs
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 14 Aug 2020 9:36 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:00 PM
  • Views 5306 views
  • Likes 2 likes
  • Comments 47 comments
Related
Recommended

Roadtesting the easyE4 Nano PLC: AC or DC, What's Your Preference?

I will be roadtesting the Eaton easyE4 Nano Programmable Logic Controller in the very near future. If you haven't heard about it, let me tell you a few facts:

 

The easyE4 nano programmable logic controllers combine timers, relays, counters, special functions, inputs and outputs into a compact device that is easily programmed. It provides an

exceptional level of flexibility together with a substantial savings of commissioning time and effort. The easyE4 is available in six styles with 12 I/O that can be expanded to 188 I/O points, which provides the ideal solution for material handling, HVAC, pump control, irrigation, lighting, energy management, industrial control, and home automation. The easyE4 nano programmable logic controller excels in traditional applications where multiple relays, timers and pushbuttons are used.

 

For the purpose of ordering the roadtest units, a question arose about the input voltage while discussing the roadtest with Eaton. The two types I am considering is 24VDC or 110-220VAC. While both versions are available, and I could get both, I just wanted to get a sense what would be a roadtester's preference. This is more a logistics question than a tech question. Both versions have the same functionality.

 

Here's the 24VDC version

 

**Image is updated***

 

easyE4 Nano Programmable Logic Controllers 24vdc

**** Datasheet is updated**** Datasheet EASY-E4-UC-12RC1

 

 

Here's the 110-220VAC version

 

easyE4 Nano Programmable Logic Controllers 110-220VAc

Datasheet

 

Poll question: Which version do you prefer AC or DC?

  • scasny
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • rscasny
    rscasny over 5 years ago +6
    I will ask about the EasySoft7 software. But it seems there is a desire for both AC and DC. I will ask for both. I'll ask for these two models: Easy-E4-UC-12RC1 and Easy-E4-AC-12RC1 Randall --element1…
  • michaelkellett
    michaelkellett over 5 years ago +5
    Definitely DC, kind of places you use these devices often have limited access and very frequently need live commissioning and/or debugging. A 24V DC based solution may cost a little more (needs more 24V…
  • cghaba
    cghaba over 5 years ago in reply to hugohu +5
    When you talk about programming PLCs you talk about programmming in Ladder Diagrams, Instruction List, Structrued Text, Function Blocks languages. For this PLC it is used the Ladder Diagram language.
Parents
  • michaelkellett
    michaelkellett over 5 years ago

    Definitely DC, kind of places you use these devices often have limited access and very frequently need live commissioning and/or debugging.

     

    A 24V DC based solution may cost a little more (needs more 24V DC <-> mains interface components) but is much, much  safer.

     

    For example, my neighbor has a horrible but cheap Chinese lifter for cars. I've already had to help him with replacing a few switches and we confidently expect the controller to die at some time.

    A small PLC would be the ideal control element but there is no way I want mains trundling about to sensor switches and small actuators.

    24 VDC ( and a [proper certified safety relay on the E-stop) every time.

     

    If I were choosing I'd want the 24V AC/DC model with the 8A relay outputs, your pics show the AC mains model with 8A relays but the 24VDC with 0.5A transistor outputs.

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 5 years ago

    Definitely DC, kind of places you use these devices often have limited access and very frequently need live commissioning and/or debugging.

     

    A 24V DC based solution may cost a little more (needs more 24V DC <-> mains interface components) but is much, much  safer.

     

    For example, my neighbor has a horrible but cheap Chinese lifter for cars. I've already had to help him with replacing a few switches and we confidently expect the controller to die at some time.

    A small PLC would be the ideal control element but there is no way I want mains trundling about to sensor switches and small actuators.

    24 VDC ( and a [proper certified safety relay on the E-stop) every time.

     

    If I were choosing I'd want the 24V AC/DC model with the 8A relay outputs, your pics show the AC mains model with 8A relays but the 24VDC with 0.5A transistor outputs.

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data