RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Polls Are you Interested in Roadtesting the 96Boards ON Semiconductor Dual Camera Mezzanine?
  • Blogs
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 6 Oct 2020 9:21 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:00 PM
  • Views 2052 views
  • Likes 2 likes
  • Comments 15 comments
Related
Recommended

Are you Interested in Roadtesting the 96Boards ON Semiconductor Dual Camera Mezzanine?

I had a meeting this week and the new 96Boards ON Semiconductor Dual Camera Mezzanine by AVNET was being considered for a roadtest.

 

This 96Boards mezzanine card features two Polight IAScompatible imaging modules based on imaging sensors from ON Semiconductor. These sensors interface to an AP1302 imaging coprocessor. By using the 96Boards standard, this card could be easily prototyped with the Ultra96-V2 platform. This kit simplifies the complex process of developing with imaging sensors.

 

96Boards ON Semiconductor Dual Camera Mezzanine

 

MIPI-CSI2 is widely used in the consumer industry for high-speed communications from host processor to image sensors, but many image sensor modules have varying connector formats which can lead to difficulties with experimenting with different camera modules. The Imager Access System (IAS) image sensor module format from ON Semiconductor helps solve this problem and enables the following:

 

- Ease of Design-In: OEMs do not have to source lens or explore module vendors

- Decreases time to market by enabling low-touch design

- Prior imaging system expertise is not required since IAS is a plug-and-play solution

 

It works with the Ultra96-V2, so that would probably be included in this roadtest.

Ultra96 V2

 

I want to gauge the interest on the element14 community for this roadtest. Please vote below. Providing a comment on what you would do with this gear would also be helpful. Thanks. (More info by going here: 96Boards ON Semiconductor Dual Camera Mezzanine )

 

Randall Scasny

RoadTest Program Manager

  • aes-acc-u96-oncam-mez
  • community survey
  • 96boards on semiconductor dual camera mezzanine
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • crisdeodates
    crisdeodates over 5 years ago +11
    rscasny This seems a very nice pair indeed. Very well interested in trying this dual camera stereo setup on an Ultra96-V2 for depth sensing and subsequent obstacle avoidance along with a ROS powered control…
  • dougw
    dougw over 5 years ago in reply to crisdeodates +4
    I like the Meccano...
  • Fred27
    Fred27 over 5 years ago +3
    I've already bought one and plan to blog about it when I get a chance. I'm busy with work and the second part of my Eclypse Z7 road test at the moment. My first impressions: It's not obvious the cameras…
Parents
  • Fred27
    Fred27 over 5 years ago

    I've already bought one and plan to blog about it when I get a chance. I'm busy with work and the second part of my Eclypse Z7 road test at the moment.

     

    My first impressions:

    • It's not obvious the cameras are monochrome. I actually bought it without realising this. It makes sense for image processing so that's fine, but it's not mentioned anywhere that I can see.
    • There's a connector that fits the Pcam5C so this may allow other (colour?) cameras to be used with the Ultra96. Nothing documented though.
    • Software support is not there yet. I've got a beta copy, so it's definitely on the way. Also, Adam Taylor has a project on Hackster.io to get you started.
    • It's not easy to get on and off. A combination of a stiff low speed header with a delicate high speed header and cameras make it awkward.

     

    Also, beware ordering one direct from Avnet if you're in the UK. I expected to pay tax, but DHL don't hold back on other fees! It might be worth waiting for resellers such as Farnell to stock it.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Fred27
    Fred27 over 5 years ago

    I've already bought one and plan to blog about it when I get a chance. I'm busy with work and the second part of my Eclypse Z7 road test at the moment.

     

    My first impressions:

    • It's not obvious the cameras are monochrome. I actually bought it without realising this. It makes sense for image processing so that's fine, but it's not mentioned anywhere that I can see.
    • There's a connector that fits the Pcam5C so this may allow other (colour?) cameras to be used with the Ultra96. Nothing documented though.
    • Software support is not there yet. I've got a beta copy, so it's definitely on the way. Also, Adam Taylor has a project on Hackster.io to get you started.
    • It's not easy to get on and off. A combination of a stiff low speed header with a delicate high speed header and cameras make it awkward.

     

    Also, beware ordering one direct from Avnet if you're in the UK. I expected to pay tax, but DHL don't hold back on other fees! It might be worth waiting for resellers such as Farnell to stock it.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • neuromodulator
    neuromodulator over 5 years ago in reply to Fred27

    The card looks interesting bit i also found there was very little info. I suppose schematics specifies all that, but I also was wondering about sensors and what resolutions and framwrates could be achieved

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 5 years ago in reply to neuromodulator

    I expect to provide more information the closer I  get to launching to the roadtest. But thanks for commenting. I'll see if I can find the info you talked about.

     

    Randall