RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Polls Poll: What Has Impeded You In Applying for the USB104 A7: Artix-7 FPGA Dev Bd RoadTest
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 26 Oct 2020 7:22 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:00 PM
  • Views 1146 views
  • Likes 2 likes
  • Comments 7 comments
Related
Recommended

Poll: What Has Impeded You In Applying for the USB104 A7: Artix-7 FPGA Dev Bd RoadTest

We are currently enrolling applicants for the USB104 A7: Artix-7 FPGA Dev Bd RoadTest.

 

You can submit an pplication by going here: https://www.element14.com/community/create-roadTestApp!input.jspa?containerID=1069&containerType=700&roadTestID=2234&isR…

 

About the USB104 A7: Artix-7 FPGA Dev Bd RoadTest

The first Digilent board to adhere to an industry-standard form factor, the USB104 A7 brings power and versatility to your PC/104 stackable PC. The board measures 95.89 mm x 90.17 mm and provides the standard mounting holes with standoffs included.

 

The USB104 A7 features the industrial temperature rated Xilinx Artix-7 XC7A100T. ArtixRegistered-7 devices provide the highest performance-per-watt fabric making the USB104 A7 ideal for size, weight, and power (SWaP) constrained projects.

 

image

 

I/O is provided with on-board LEDs and push-buttons, and, of course, three 12-pin Pmod ports. A SYZYGY-compatible Zmod port is available as well, allowing for high-speed signal acquisition and generation. An onboard USB hub and controller conveniently interfaces the USB104 A7 with JTAG, UART, and a parallel data interface (DPTI) through a single connection. The DPTI data transfer interface provides host-to-FPGA data transfer and is easily managed with Digilent’s Adept 2 application. This ease of use and high-speed data transfer is especially useful for deployed systems.

 

Features

Artix-7 100T (XC7A100T-1CSG324I) FPGA

  • Logic Cells: 101,440
  • DSP Slices: 240
  • Memory: 4,860
  • GTP 6.6Gb/s Transceivers: 8
  • I/O Pins: 300

USB

  • USB-JTAG Programming circuitry
  • USB-UART bridge
  • Adept DPTI/DSPI data transfer interface for high speed host to FPGA data transfer
  • Onboard USB hub eliminates the need for multiple USB cable connections

Expansion Connectors

  • One standard SYZYGY port (Zmod)
  • Three standard Pmod ports

Form Factor

  • PCB adheres to PC/104 form factor and includes the standard mounting holes
  • Board is 3.775” x 3.550” (95.89 mm x 90.17 mm).

Additional Information

  • Datasheet
  • Reference Manual
  • Schematic

 

Question: What Has Impeded You In Apply for the USB104 A7: Artix-7 FPGA Dev Bd RoadTest?

  • usb104 a7: artix-7 fpga dev bd roadtest
  • community roadtest survey
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +3
    The spirit is willing, but my ADD makes it a no go. DAB
  • hlipka
    hlipka over 5 years ago +2
    When looking at this road test, it makes me wonder whether there should be a statement "this is what we expect from this road test". The range of reviews can be very broad here - from just testing that…
  • michaelkellett
    michaelkellett over 5 years ago +2
    The problem with this board, from my point of view, is that the access to the FPGA pins is compromised by the use of three PMOD and one ZMOD (I mistyped that as ZMAD which may be prophetic) ports. For…
Parents
  • hugohu
    hugohu over 5 years ago

    I have never worked with FPGAs. Nor, DDR3, etc.

     

    Out of my pay grade.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • hugohu
    hugohu over 5 years ago

    I have never worked with FPGAs. Nor, DDR3, etc.

     

    Out of my pay grade.