RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Polls RoadTest Poll: Do You Have Access to 210 VAC 3-Phase or 300VDC to Roadtest New Eval Board?
  • Blogs
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 4 May 2021 4:58 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:00 PM
  • Views 1026 views
  • Likes 2 likes
  • Comments 8 comments
Related
Recommended

RoadTest Poll: Do You Have Access to 210 VAC 3-Phase or 300VDC to Roadtest New Eval Board?

I have been contacted by a supplier who would like to sponsor a roadtest on a new quasi-resonant AC/DC Converter with a Built-in SiC MOSFET Isolation Fly-back Converter.

 

Its input voltage is much higher than what we normally see for products I roadtest.

 

This image communicates my point of concern in holding this roadtest:

 

Rohm RoadTest Image

Poll Question: Do You Have Access to 210 VAC 3-Phase or 300VDC?

 

Sincerely,

 

 

Randall Scasny

RoadTest Program Manager

  • rohm
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 5 years ago +2
    I'd have access to 3-phase at work but I don't think I'd be allowed to connect a road test product up to it. At home (in the UK) it's 240V single phase.
  • kmikemoo
    kmikemoo over 5 years ago +2
    Oh, yeah! This is right up my alley! More power. Whoot! 208v, 240v & 480v. 50w output. I could rig something up.
  • rsc
    rsc over 5 years ago +2
    Kinda looks like this board with some components changed to surface mount. ROHM BD7682FJ-LB-EVK
Parents
  • navadeepganeshu
    navadeepganeshu over 5 years ago

    I have home wiring with 230V AC/3-PH and also used for water pump, but not the 300V DC(may need an additional rectifier system for it). I don't think someone would have 300V DC access unless in a power electronics lab or a super serious hardware garage at home. Anyways, I am out of high voltage RoadTest.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • navadeepganeshu
    navadeepganeshu over 5 years ago

    I have home wiring with 230V AC/3-PH and also used for water pump, but not the 300V DC(may need an additional rectifier system for it). I don't think someone would have 300V DC access unless in a power electronics lab or a super serious hardware garage at home. Anyways, I am out of high voltage RoadTest.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data