<?xml version="1.0" encoding="UTF-8" ?>
<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/"><channel><title>Volkswagen to implement cylinder deactivation in 4-cylinder 1.4 TSI engines in 2012</title><link>https://community.element14.com/technologies/automotive/w/documents/8973/volkswagen-to-implement-cylinder-deactivation-in-4-cylinder-1-4-tsi-engines-in-2012</link><description /><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>Volkswagen to implement cylinder deactivation in 4-cylinder 1.4 TSI engines in 2012</title><link>https://community.element14.com/technologies/automotive/w/documents/8973/volkswagen-to-implement-cylinder-deactivation-in-4-cylinder-1-4-tsi-engines-in-2012</link><pubDate>Fri, 08 Oct 2021 03:40:23 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:2da86594-1e80-409b-8f7d-ca8cface59e2</guid><dc:creator>autoembedded</dc:creator><comments>https://community.element14.com/technologies/automotive/w/documents/8973/volkswagen-to-implement-cylinder-deactivation-in-4-cylinder-1-4-tsi-engines-in-2012#comments</comments><description>Current Revision posted to Documents by autoembedded on 10/8/2021 3:40:23 AM&lt;br /&gt;
&lt;p style="margin:0;"&gt;Volkswagen will &lt;a class="jive-link-external-small" href="https://www.volkswagen-media-services.com/medias_publish/ms/content/en/pressemitteilungen/2011/09/02/volkswagen_presents.html;jsessionid=59feedb8-4410-6344-84c7-22c09f407d6c?actionID=ms" rel="nofollow ugc noopener" target="_blank"&gt;debut&lt;/a&gt; cylinder deactivation (cylinder shut-off) technology in the new&amp;nbsp; 1.4-liter TSI turbocharged, direct-injection engine beginning in 2012.&amp;nbsp; Volkswagen is the first carmaker to implement this technology in a&amp;nbsp; turbocharged four-cylinder engine in large-scale production.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;The primary goal of the system is to reduce significantly fuel&amp;nbsp; consumption by temporarily shutting off two of the four cylinders&amp;nbsp; (cylinders 2 and 3) during low to mid loads; Volkswagen says that&amp;nbsp; cylinder shut-off reduces fuel consumption of the 1.4 TSI by 0.4 liter&amp;nbsp; per 100 km in the NEDC driving cycle. When the Stop/Start functionality&amp;nbsp; is integrated, which deactivates the engine in neutral gear, the savings&amp;nbsp; effect adds up to about 0.6 liter per 100 km.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;table align="right" border="1" cellpadding="5" cellspacing="0" class="table" rules="none" style="font-size:8pt;line-height:140%;font-family:Geneva,Arial,Helvetica,sans-serif;margin-left:10px;width:225px;"&gt;&lt;thead class="thead"&gt; &lt;tr&gt;&lt;th align="center" style="border:1px solid black;"&gt;1.4 TSI&lt;/th&gt;&lt;/tr&gt;&lt;/thead&gt; &lt;tbody&gt;&lt;tr&gt;&lt;td align="left" style="border:1px solid black;"&gt;The new 1.4 TSI outputs 103 kW (140 PS, 138 hp), with 250 N·m (184 lb-ft) of torque between 1,500 and 4,000 rpm.&lt;/td&gt;&lt;/tr&gt;&lt;/tbody&gt;&lt;/table&gt;&lt;p style="margin:0;"&gt;The greatest benefits of the technology are realized while driving at&amp;nbsp; constant moderate speeds. At 50 km/h (31 mph), in third or fourth gear, savings amount to nearly&amp;nbsp; one liter per 100 km. Even when running on two cylinders, the 1.4&amp;nbsp; TSI—with its excellent engine balance—is still very quiet and low in&amp;nbsp; vibration, Volkswagen says.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;Cylinder shut-off is active whenever the engine speed of the 1.4 TSI&amp;nbsp; is between 1,400 and 4,000 rpm and its torque is between 25 and 75 N·m&amp;nbsp; (18–55 lb-ft). This applies to nearly 70% of the driving distance in the&amp;nbsp; EU fuel economy driving cycle. As soon as the driver presses the&amp;nbsp; accelerator pedal sufficiently hard, cylinders 2 and 3 are reactivated&amp;nbsp; unnoticed.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;Under the deactivation process, the combustion chambers are filled&amp;nbsp; with air—this entrapped fresh air leads to minimal cylinder pressure and&amp;nbsp; therefore to lower energy consumption. Afterwards, the system closes&amp;nbsp; the intake and exhaust valves of cylinders 2 and 3; engine ignition only&amp;nbsp; occurs once per crankshaft revolution. The pistons of the deactivated&amp;nbsp; cylinder are now dragged by the crankshaft. On the other hand,&amp;nbsp; efficiency increases in the two active cylinders, because their&amp;nbsp; operating points are shifted to higher loads.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;The valves are closed using a complex set of actuators: on both the&amp;nbsp; intake camshaft and the exhaust camshaft, there are two adjustable&amp;nbsp; sleeves (cam pieces) that are placed on special tooth systems. They are&amp;nbsp; responsible for the eight valves of the second and third cylinders. At&amp;nbsp; the ends of each cam piece, there are two different profiles adjacent to&amp;nbsp; one another: a conventional full profile and a so-called zero-lift cam.&amp;nbsp; The full profiles actuate the roller cam followers, which in turn&amp;nbsp; actuate the valves in four-cylinder operation; that is, they behave like&amp;nbsp; very conventional cams.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;However, the zero-lift cams rotate over the&amp;nbsp; followers—i.e. they do not actuate them—and the valve springs hold the&amp;nbsp; valves shut. Engine management simultaneously shuts off fuel injection.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;Spiral-shaped slots are milled in the outer surfaces of the rotating&amp;nbsp; cam pieces; these slots permit shifting the sleeves a few millimeters&amp;nbsp; along the shafts very quickly; when electromagnetic actuators in the&amp;nbsp; valve cover get a signal from the engine controller, two integrated&amp;nbsp; metal pins engage the slots from outside and move them to their end&amp;nbsp; positions. Finally, the cam pieces are locked in place by spring-loaded&amp;nbsp; balls. As soon as the driver presses the accelerator pedal sufficiently,&amp;nbsp; cylinders 2 and 3 are reactivated.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;All mechanical switch-over processes are executed within one-half&amp;nbsp; camshaft revolution; they last between 13 and 36 milliseconds, depending&amp;nbsp; on engine speed. These processes are smoothed by accompanying&amp;nbsp; interventions in ignition and throttle valve control.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;Volkswagen utilizes information from the gas pedal sensor to detect&amp;nbsp; the driver’s mode of driving. If the driving exhibits a non-uniform&amp;nbsp; pattern—e.g. while driving in roundabout traffic or in a sporty style on&amp;nbsp; a country road—shut-off functionality is suppressed.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;The components for cylinder shut-off weigh a total of just over 3&amp;nbsp; kilograms. Their actuators, the camshafts and their bearing carriers are&amp;nbsp; integrated in the valve cover. Two roller bearings reduce the friction&amp;nbsp; of the shafts.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span&gt;&lt;a href="https://community.element14.com/resized-image/__size/620x429/__key/communityserver-wikis-components-files/00-00-00-00-11/contentimage_5F00_13869.png"&gt;&lt;img alt="image" src="https://community-storage.element14.com/communityserver-components-secureimagefileviewer/communityserver/wikis/components/files/00/00/00/00/11/contentimage_13869.png-620x429.png?sv=2016-05-31&amp;amp;sr=b&amp;amp;sig=%2F0Xukm26WeVI3GXDqlNJ%2FqDq2OV0jqdct0lJB1ZgCYw%3D&amp;amp;se=2026-10-17T23%3A59%3A59Z&amp;amp;sp=r&amp;amp;_=2aLDn5hBPPj1dFsaPksctw==" style="max-height: 429px;max-width: 620px;" /&gt;&lt;/a&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;strong&gt;SOURCE:&lt;/strong&gt; &lt;a class="jive-link-external-small" href="http://www.greencarcongress.com/2011/09/zas-20110902.html?utm_source=feedburner&amp;amp;utm_medium=feed&amp;amp;utm_campaign=Feed%3A+greencarcongress%2FTrBK+%28Green+Car+Congress%29" rel="nofollow ugc noopener" target="_blank"&gt;www.greencarcongress.com&lt;/a&gt;&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;

&lt;div style="font-size: 90%;"&gt;Tags: transportation, fuel_efficiency, engines, vehicle_systems, automotive, volkswagen, auto&lt;/div&gt;
</description></item></channel></rss>