Code Exchange
  • Technologies
  • More
Code Exchange
Forum PI3 wlan0 access point without internet and predefined 192.168.XXX.XXX IP and eth0 with DHCP
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 48 subscribers
  • Views 2578 views
  • Users 0 members are here
  • tcpip
  • rpi
  • access_point
Related

PI3 wlan0 access point without internet and predefined 192.168.XXX.XXX IP and eth0 with DHCP

ataf
ataf over 7 years ago

Good Day,

 

 

I try to create wlan0 AP (access point) without internet which allows to open tcpip socket connection to my process running on the rpi3 (just for some packages exchange with client application connecting to the AP with predefined 192.168.XXX.XXX IP adress and port), at the same time I need eth0 internet connection with DHCP.

 

 

Apparently, I get pretty close result configuring /etc/hostapd/hostapd.conf

[code]

interface=wlan0

driver=nl80211

ssid=MY_AP_SSID

hw_mode=g

channel=6

macaddr_acl=0

auth_algs=1

ignore_broadcast_ssid=MY_AP_SSID

wpa=0

wpa_passphrase=passphrase

wpa_key_mgmt=WPA-PSK

wpa_pairwise=TKIP

rsn_pairwise=CCMP

[/code]

and after that running

[code]

/etc/init.d/hostapd stop

ifdown wlan0

ifup wlan0

/etc/init.d/hostapd restart

[/code]

and I can connect socket and communicate with the rpi3 from my PC but I get "dynamic" IP 169.254.XX.XX. The IP is the same every time but it doesn't look like the constant one.

 

 

The question is: [b]how to configure static 192.168.XXX.XXX IP for the AP?[/b]

 

 

As soon as I try to do it with /etc/dhcpcd.conf addition like

[code]

nodhcp

static interface wlan0

static ip_address=192.168.111.111

[/code]

I can see the correct wlan0 IP in the 'ifconfig' and 'ip -4 addr show' output and I can  'ping 192.168.111.111' successfully on the rpi3 but I get 'destination unreachable' if I ping the IP from my PC connected to the AP.

 

 

I use  RPI3 (model B) with 'raspbian jessie lite', 'uname -a' output is

[code]

Linux raspberrypi 4.9.59-v7+ #1047 SMP Sun Oct 29 12:19:23 GMT 2017 armv71 GNU/Linux

[/code]

 

 

Any comment, thoughts, ideas are welcome image
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.