Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Blog Amphenol / SV Microwave SF2921-61506-1S SMA coaxial connector: behavior under vibration
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 4 Mar 2023 5:41 PM Date Created
  • Views 2911 views
  • Likes 9 likes
  • Comments 10 comments
  • svmicrowave
  • amphenol
  • SF2921-61506
  • SF2921-61506-1S
Related
Recommended

Amphenol / SV Microwave SF2921-61506-1S SMA coaxial connector: behavior under vibration

Jan Cumps
Jan Cumps
4 Mar 2023
Amphenol /  SV Microwave SF2921-61506-1S SMA coaxial connector: behavior under vibration

In this post I test the Amphenol / SV Microwave SF2921-61506-1S SMA coaxial connector's DC resistance behavior when vibrating. How well does the spring contact stays connected to the PCB?

image

I want to check if, under vibration, the middle contact keeps in touch with the copper pad it's pushing against. I've mounted a connector on shabaz 's test PCB, and soldered test leads  to signal and ground. I then made a shortcut in the adapter using aluminium foil and kept that locked in place by mounting some devices on it. I used a sub 1-GHz antenna (photo in the mail header) and a little SMA gender-converter. Both tests are interesting because they have a different mass, and they behave differently at resonance frequencies. In both cases, I measured approximately 155 mΩ at rest. Fiddling with the setup doesn't change that.

I mounted the PCB on a the shaker from the Vibration Measurement with the MCC 172 roadtest.

image

I vibrated the setup between 20 and 150 Hz.  

image

The vibrations are visible on the resistance graph, +- 0.5 mΩ. That is nothing, and very likely interference picked up in the measurement setup. If I switch my meter to mV, it shows the vibrations too.

image

For short periods, I drove the shaker to its maximum, and the connection never interrupted. In this vibration test, I could not break the contact. The connector survived all conditions. I also did a thump test: hit the PCB on a ceramic plate. That didn't break the contact either.

Blog Index

  • Overview: Amphenol / SV Microwave SF2921-61506-1S SMA coaxial connector series
  • Amphenol / SV Microwave SF2921-61506-1S SMA coaxial connector: behavior under vibration
  • Create a custom footprint in KiCad 7 - 1: collect info and component details
  • Create a custom footprint in KiCad 7 - 2a: create the footprint for an SMA coax connector with the editor - initial outline
  • Create a custom footprint in KiCad 7 - 2b: create the footprint for an SMA coax connector with the editor - copper pour, solder mask clearance, holes, pads
  • Use a LibraryLoader Footprint in KiCad 7
  • Sign in to reply
Parents
  • javagoza
    javagoza over 3 years ago

    Is there also a temperature variation in the connector or is it difficult to make this measurement?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to javagoza

    Result:

    image

    data (openoffice format):

    defbuffer1_0306_203554.zip

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to javagoza

    Result:

    image

    data (openoffice format):

    defbuffer1_0306_203554.zip

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    ... and a ramp up / ramp down:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    (collateral: the temperature ramp)

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    Keithley DMM6500 showing both graphs