Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog C++ library for ST Teseo GPS - pt. 8: Initial Raspberry Pi port for UART read
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 18 Aug 2024 12:56 PM Date Created
  • Views 806 views
  • Likes 6 likes
  • Comments 5 comments
  • raspberry_pi
  • Teseo
  • gps
  • OO
  • teseo_c++
Related
Recommended

C++ library for ST Teseo GPS - pt. 8: Initial Raspberry Pi port for UART read

Jan Cumps
Jan Cumps
18 Aug 2024

The Teseo-LIV3 GPS module (as used in shabaz ' GPS / Galileo / BeiDou / GLONASS receiver) talks UART and I2C. I'm writing an OO driver for it, for embedded systems. In this blog, I validate if ST's example fits for UART read.

image

What do I try to test?

My Teseo lib works well on a Raspberry Pico. But it's supposed to be device independent. Here, I'm trying to validate if I can get the UART read on a Raspberry Pi in a controlled way. 
ST published open source examples for reading via I2C and UART. I'll be reusing that UART example, to see if it works in query / response mode.

Here's the adapted UART read example. It 'll print all replies coming from the Teseo's UART channel:

/**
  ******************************************************************************
  * @file       gnss_uart_read.c
  * @author     SRA-SAIL
  * @brief      This file contains application to read the data from GNSS module
  *				over UART
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2021 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */
/*
 ******************************************************************************
 * INCLUDES
 ******************************************************************************
 */
#include <errno.h>
#include <fcntl.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <termios.h>
#include <unistd.h>
#include <linux/gpio.h>
#include <sys/ioctl.h>


/*
 ******************************************************************************
 * DEFINES
 ******************************************************************************
 */
 #define BUFF_LEN 	83
 #define DEBUG 		0
 #define SERIALTERMINAL      "/dev/ttyS0"

#define RESET_CHIP "/dev/gpiochip0"
#define RESET_PIN 23

/*
 ******************************************************************************
 * MAIN FUNCTION
 ******************************************************************************
 */
int set_interface_attribs(int fd, int speed);
static int GNSS_Reset();


int main()
{
    char *portname = SERIALTERMINAL;
    int fd;


    /*Reset The GNSS Device */
    GNSS_Reset();

    /*Open the device file*/
    fd = open(portname, O_RDWR | O_NOCTTY | O_SYNC);
    if (fd < 0) {
        printf("Error opening %s: %s\n", portname, strerror(errno));
        return -1;
    }
    /*for X-NUCLEO-GNSS1A1(Teseo-LIV3F) : baudrate 9600, 8 bits, no parity, 1 stop bit */
    /*for X-NUCLEO-GNSS2A1(Teseo-VIC3DA) : baudrate 115200, 8 bits, no parity, 1 stop bit */
    set_interface_attribs(fd, B9600);

    /* Continously read the data */
    do {
        u_int8_t buf[BUFF_LEN];
        int rdlen;

        rdlen = read(fd, buf, sizeof(buf) - 1);
        if (rdlen > 0) {
            buf[rdlen] = 0;
            #if DEBUG
            /* display as hex numbers  */
            printf("Read %d:", rdlen);
            for (p = buf; rdlen-- > 0; p++) {
                printf(" 0x%x", *p);
                if (*p < ' ')
                    *p = '.';   /* replace any control chars */
            }
            #endif
            printf("%s\n", buf);
        } else if (rdlen < 0) {
            printf("Error from read: %d: %s\n", rdlen, strerror(errno));
        } else {  /* rdlen == 0 */
            printf("Nothing read. EOF?\n");
        }
        /* repeat read */
    } while (1);
}

/*Set Terimal Attributes*/
int set_interface_attribs(int fd, int speed)
{
    struct termios tty;

    if (tcgetattr(fd, &tty) < 0) {
        printf("Error from tcgetattr: %s\n", strerror(errno));
        return -1;
    }

    cfsetospeed(&tty, (speed_t)speed);
    cfsetispeed(&tty, (speed_t)speed);

    tty.c_cflag |= CLOCAL | CREAD;
    tty.c_cflag &= ~CSIZE;
    tty.c_cflag |= CS8;         /* 8-bit characters */
    tty.c_cflag &= ~PARENB;     /* no parity bit */
    tty.c_cflag &= ~CSTOPB;     /* only need 1 stop bit */
    tty.c_cflag &= ~CRTSCTS;    /* no hardware flowcontrol */

    tty.c_lflag |= ICANON | ISIG;  /* canonical input */
    tty.c_lflag &= ~(ECHO | ECHOE | ECHONL | IEXTEN);

    tty.c_iflag &= ~IGNCR;  /* preserve carriage return */
    tty.c_iflag &= ~INPCK;
    tty.c_iflag &= ~(INLCR | ICRNL | IUCLC | IMAXBEL);
    tty.c_iflag &= ~(IXON | IXOFF | IXANY);   /* no SW flowcontrol */

    tty.c_oflag &= ~OPOST;

    tty.c_cc[VEOL] = 0;
    tty.c_cc[VEOL2] = 0;
    tty.c_cc[VEOF] = 0x04;

    if (tcsetattr(fd, TCSANOW, &tty) != 0) {
        printf("Error from tcsetattr: %s\n", strerror(errno));
        return -1;
    }
    return 0;
}

static int GNSS_Reset()
{

  	struct gpiohandle_request req;
  	struct gpiohandle_data data;
  	char chrdev_name[20];
  	int fd, ret;

  	strcpy(chrdev_name, RESET_CHIP);

  	/*  Open device: gpiochip0 for GPIO bank A */
  	fd = open(chrdev_name, 0);
  	if (fd == -1) {
  		ret = -errno;
  		fprintf(stderr, "Failed to open %s\n", chrdev_name);

  		return ret;
  	}

  	/* request GPIO line: GPIO23 */
  	req.lineoffsets[0] = RESET_PIN;
  	req.flags = GPIOHANDLE_REQUEST_OUTPUT;
  	memcpy(req.default_values, &data, sizeof(req.default_values));
  	strcpy(req.consumer_label, "gnss_reset");
  	req.lines  = 1;

  	ret = ioctl(fd, GPIO_GET_LINEHANDLE_IOCTL, &req);
  	if (ret == -1) {
  		ret = -errno;
  		fprintf(stderr, "Failed to issue GET LINEHANDLE IOCTL (%d)\n",
  			ret);
  	}
  	if (close(fd) == -1)
  		perror("Failed to close GPIO character device file");

  	/*  Start led blinking */

          data.values[0] = 0;
  	ret = ioctl(req.fd, GPIOHANDLE_SET_LINE_VALUES_IOCTL, &data);
  	if (ret == -1) {
  		ret = -errno;
  		fprintf(stderr, "Failed to issue %s (%d)\n",
  					"GPIOHANDLE_SET_LINE_VALUES_IOCTL", ret);
  	}
  	sleep(1);
  	ret = ioctl(req.fd, GPIOHANDLE_GET_LINE_VALUES_IOCTL, &data);

  	data.values[0] = 1;
  	ret = ioctl(req.fd, GPIOHANDLE_SET_LINE_VALUES_IOCTL, &data);
  	if (ret == -1) {
  		ret = -errno;
  		fprintf(stderr, "Failed to issue %s (%d)\n",
  					"GPIOHANDLE_SET_LINE_VALUES_IOCTL", ret);
  	}

  	ret = ioctl(req.fd, GPIOHANDLE_GET_LINE_VALUES_IOCTL, &data);

  	/*  release line */
  	ret = close(req.fd);
  	if (ret == -1) {
  		perror("Failed to close GPIO LINEHANDLE device file");
  		ret = -errno;
  	}
  	return ret;
  }

Then, I use (for the moment) the Linux command line to configure the Teseo. I'm submitting the same commands as my Teseo library would:

echo $'$PSTMGPSSUSPEND\r\n' > /dev/ttyS0
echo $'$PSTMCFGMSGL,0,1,0,0\r\n' > /dev/ttyS0
echo $'$PSTMSETPAR,1227,1,2\r\n' > /dev/ttyS0
echo $'$PSTMGPSRESTART\r\n' > /dev/ttyS0

In this state, the Teseo is in query response mode, and will only  spawn output when it gets a command. Here's what happens when I send the GSV command via the Linux command line:

echo $'$PSTMNMEAREQUEST,80000,0\r\n' > /dev/ttyS0

image

The Teseo nicely returns one set of GSV data. That looks promising.

Wiring: 

image image

 

Current version of the reading software: pi_uart_stream.zip.
Unzip, then move it on you Pi,
make it executable : chmod +x ./pi_uart_stream
launch it: ./pi_uart_stream
Keep the terminal open

In another terminal, execute the Linux commands from this post, to interact with the Teseo. You 'll see the output of pi_uart_stream change. And you 'll see that it nicely sends only the response to your queries.

Prereq: UART must be enabled on your Pi. Use the raspi-config tool:
3 - Interface options -> I6 - Serial Port -> No -> Yes 

Link to all posts.

  • Sign in to reply
Parents
  • shabaz
    shabaz over 1 year ago

    This is great news, it will allow for a lot of easy experimentation on Pi+Linux!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 1 year ago

    This is great news, it will allow for a lot of easy experimentation on Pi+Linux!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to shabaz

    yes. The ideal situation, for prototyping, would be, that you could also use the standard Linux commands to read from the Teseo. But I could not get that to work* for the read side, with e.g. the cat command

    *in a request/response way. It does work to just log from a Teseo that's in default configuration