Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog STM32H7B3I - Create a TouchGFX Project with support for the Designer, CubeIDE and Debugger - Pt 2: Touch Works
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 4 Aug 2020 6:36 PM Date Created
  • Views 6924 views
  • Likes 5 likes
  • Comments 16 comments
  • stm32h7b3i
  • rt
  • stm32h7b3i-dk
Related
Recommended

STM32H7B3I - Create a TouchGFX Project with support for the Designer, CubeIDE and Debugger - Pt 2: Touch Works

Jan Cumps
Jan Cumps
4 Aug 2020

Continued from Pt 1: Screen Works.

We left off at the point where the LCD shows out TouchGFX design, but touch screen doesn't work yet.

We'll fix that.

 

5. Add Touch Screen init and handling

 

The two methods in TouchGFX/target/STM32TouchController.cpp aren't implemented by the wizards.

Open the file and implement them as below:

 

#include <stm32h7b3i_discovery_ts.h>
#include <TouchGFXHAL.hpp>
#include <cmsis_os.h>

 

void STM32TouchController::init()
{
    /**
     * Initialize touch controller and driver
     *
     */
    TS_Init_t hTS;

    hTS.Orientation = TS_SWAP_XY;
    hTS.Accuracy = 0;
    hTS.Width = touchgfx::HAL::FRAME_BUFFER_WIDTH;
    hTS.Height = touchgfx::HAL::FRAME_BUFFER_HEIGHT;
    BSP_TS_Init(0, &hTS);
}

 

bool STM32TouchController::sampleTouch(int32_t& x, int32_t& y)
{
    /**
     * By default sampleTouch returns false,
     * return true if a touch has been detected, otherwise false.
     *
     * Coordinates are passed to the caller by reference by x and y.
     *
     * This function is called by the TouchGFX framework.
     * By default sampleTouch is called every tick, this can be adjusted by HAL::setTouchSampleRate(int8_t);
     *
     */
    TS_State_t TS_State = { 0 };

    /* This should never fail !! */
    if (BSP_TS_GetState(0, &TS_State) != BSP_ERROR_NONE)
    {
        configASSERT(0);
    }

    if (TS_State.TouchDetected)
    {
        x = TS_State.TouchX;
        y = TS_State.TouchY;

        return true;
    }

    return false;
}

 

The logic is dependent on the board definition files. We can import them from the firmware support package.

If you don't know where that is installed, check via the IDE  Windows -> Preferences menu

image

 

Right-click on the Drivers folder and select Import -> File System

Navigate to where you installed the firmware - In our case, it's version 1.6.0 because that's the one used in the TouchGFX .ioc file. Look for the folder Drivers and select these:

image

image

 

Then select the project's BSP folder, right-click and select Import

image

 

Rename Drivers/BSP/STM32H7B3I-DK/stm32h7b3i_discovery_conf_template.h to stm32h7b3i_discovery_conf.h.

Rename Drivers/BSP/Components/mx25lm51245g/mx25lm51245g_conf_template.h to mx25lm51245g_template.h.

 

Rename Drivers/BSP/Components/ft5336/ft5336_conf_template.h to ft5336_conf.h.

Then edit it:

#define FT5336_MAX_X_LENGTH                  480U
#define FT5336_MAX_Y_LENGTH                  272U

 

Create a new header file Drivers/STM32H7xx_HAL_Driver/Inc/stm32xxxx_hal.h.

Enter these contents:

#ifndef STM32H7XX_HAL_DRIVER_INC_STM32XXXX_HAL_H_
#define STM32H7XX_HAL_DRIVER_INC_STM32XXXX_HAL_H_

#include "stm32h7xx_hal.h"

#endif /* STM32H7XX_HAL_DRIVER_INC_STM32XXXX_HAL_H_ */

 

 

Adapt the include settings, by right-clicking the project, then select properties:

image

 

Build and Debug again. The touch screen should now work. It does for me image.

Again, the project, now with touch screen working, is attached.

 

Related Posts
First Experience with CubeIDE
Create a TouchGFX Project with support for the Designer, CubeIDE and Debugger - Pt 1: Screen Works
Create a TouchGFX Project with support for the Designer, CubeIDE and Debugger - Pt 2: Touch Works
TouchGFX Simple Example: react on a button click
USB, freeRTOS ,Task Notifications and Interrupts
the Development Kit STMod+ Connector and Using UART2
TouchGFX Application Framework: Model, View, Presentation, Message Queue
TouchGFX Application Framework: A Mock GUI - Show Statuses, Switch Screens
TouchGFX Application Framework: MVP and the ModelListener
Write a CubeIDE MX application: Hardware Cryptography with DMA
Attachments:
STM32H7B3I-DK-roadtest_pt2_touch_works.zip
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago +2
    for the next post: players.brightcove.net/.../index.html
  • jomoenginer
    jomoenginer over 5 years ago in reply to e14 Contributor +2
    With this particular kit, when creating a project for it with TouchGFX, even the latest version, the .project file for STM32CubeIDE does not include the reference to the IOC file for the kit, thus the…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to DAB +1
    It wasn't. For some reason, the current toolset does not include touch functionality. Not easy if it's your first experiene with this paricular family.
Parents
  • e14 Contributor
    e14 Contributor over 5 years ago

    Can't make the touch work. The Graphics according to part1 works fine, but this one ends up with at least 3 errors.

     

    I'm using TouchGFX 4.16 and cubeIDE 1.5.1, and some differences has happened between this example and present time.

     

    It is not clear how to import. It seems like it is 2 different imports one to file system and another to - well that is not clear to me.

    For instance: Drivers/BSP/STM32H7B3I-DK/stm32h7b3i_discovery_conf_template.h to stm32h7b3i_discovery_conf.h. I don't get the folder Drivers/BSP/STM32H7B3I-DK, so either I'm not importing the right way, or the explanation could use a little ekstra details.

     

    And the renaming of the 3 files after import i guess has a fault. Two of the files should have the ..template.. part removed. The third should have the ..conf.. part removed. Does that make sense? shouldn't they all have the ..template.. removed and all 3 be ...conf.h ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to e14 Contributor

    My project is attached. Can you import it and check?

    I don't have the hardware anymore or the software, so  can't reproduce the steps.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 5 years ago in reply to Jan Cumps

    Yes. I found it very difficult to import your existing project, but I succeded now. And I can make it compile and it works on the kit for just about a second, then it freezes. But that aside it is a huge breakthrough.

     

    Now I know it works and I will then have to build my own project again to make it work there as well. That is the important thing to be able to reproduce in my own project, to know the roadmap. I just have to figure out why I can't make it compile errorless. Some files might not be imported the right way.

     

    I just wonder why ST in these new versions of both IDE and TGFX still hasn't come up with a way to handle all this automatically. We want both the fantastic TouchGFX (which is awesome - really), and HAL functionality and the IDE working together. :-)

     

    And for a necomer as me, these tools are fantastic, I love them allready. And your description is really good, only not up-to-date, becausen the tools are constantly changing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to e14 Contributor

    I agree that this should work. I spent the majority of my road test dealing with these difficulties.

    What helped me was a good working example I received fro jomoenginer. That's what I used as a start point for the stable designs later in my road test.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 5 years ago in reply to e14 Contributor

    With this particular kit, when creating a project for it with TouchGFX, even the latest version, the .project file for STM32CubeIDE does not include the reference to the IOC file for the kit, thus the STM32CubeMX stuff does not get imported.  However, once this is included, a change to the clocks is required to get everything working properly.  I'm not sure why it is a thing with this kit, but as far as I know, it has not been corrected. Also, the kit name is not consistent in the TouchGFX/STM32CubeIDE code, so sometimes it is called a '-DISCO' and others a '-DK'.  Again, not sure why this is but it does seem to muck things up at times.

     

    This is the post I added to the STM Community page:

    https://community.st.com/s/question/0D53W00000EHBmpSAH/touchgfx-4140-does-not-include-ioc-file-reference-in-project-file-for-stm32h7b3idk

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 5 years ago in reply to Jan Cumps

    Got it working! And without freezing. I compared your working example from the zipfile provided with my own generated code. And here is my finding:

     

    The second import should be into the folder Drivers/BSP/STM32H7B3I_DK which is not allready there. So make the folder and then import the files mentioned, also with FileSystem.

    I was right about the naming. All the 3 files should be changed from ...conf_template.h to ...conf.h and then one of them should be changed with content as described. :-)

     

    Now I will try to put in some functionality as descibed in the next article. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 5 years ago in reply to Jan Cumps

    Got it working! And without freezing. I compared your working example from the zipfile provided with my own generated code. And here is my finding:

     

    The second import should be into the folder Drivers/BSP/STM32H7B3I_DK which is not allready there. So make the folder and then import the files mentioned, also with FileSystem.

    I was right about the naming. All the 3 files should be changed from ...conf_template.h to ...conf.h and then one of them should be changed with content as described. :-)

     

    Now I will try to put in some functionality as descibed in the next article. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data