<?xml version="1.0" encoding="UTF-8" ?>
<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/" xmlns:atom="http://www.w3.org/2005/Atom"><channel><title>Analogue Design - Recent Threads</title><link>https://community.element14.com/technologies/embedded/f/analogue-design</link><description>Analog and Analogue Design Discussions</description><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><lastBuildDate>Wed, 02 Oct 2024 17:12:15 GMT</lastBuildDate><atom:link rel="self" type="application/rss+xml" href="https://community.element14.com/technologies/embedded/f/analogue-design" /><item><title>9V NiMH charging</title><link>https://community.element14.com/thread/55150?ContentTypeID=0</link><pubDate>Wed, 02 Oct 2024 17:12:15 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:9f5c1243-698f-4b3d-8e4c-f1d888943f38</guid><dc:creator>koudelad</dc:creator><slash:comments>14</slash:comments><comments>https://community.element14.com/thread/55150?ContentTypeID=0</comments><wfw:commentRss>https://community.element14.com/technologies/embedded/f/analogue-design/55150/9v-nimh-charging/rss?ContentTypeId=0</wfw:commentRss><description>&lt;p&gt;Hello,&lt;/p&gt;
&lt;p&gt;9V batteries have always been a pain for me... Expensive, low capacity, almost every DMM / tester needed them.&lt;/p&gt;
&lt;p&gt;I just bought a 9V NiMH battery:&amp;nbsp;&lt;a id="" href="https://www.westinghousebattery.com/Ni-MH-Rechargeable/Premium-Series.html" rel="noopener noreferrer nofollow" target="_blank" data-e14adj="t"&gt;https://www.westinghousebattery.com/Ni-MH-Rechargeable/Premium-Series.html&lt;/a&gt; . To my surprise, it is not made from 6 smaller cells (which would give ca. 7.2-8.4 V), but 7, which has nominal voltage of 8.4, but when charged, can have almost 10 V. This makes it a true primary 9V battery replacement. I am not sure when these became available, but I remember older 6-cell &amp;quot;9 V&amp;quot; NiMH that were kind of useless, because all appliances thought the battery is discharged, due to the lower nominal voltage.&lt;/p&gt;
&lt;p&gt;However, I never really had a charger for this kind of battery. I have heard that cheap chargers only use 12 V DC power supply with in series resistor in series to limit the current to ca 30 mA.&lt;/p&gt;
&lt;p&gt;Do you have any suggestion for a charging circuit? I am open to building something, even using an MCU. I would love it to have a small small charging current (20-30 mA) or slightly higher (50 mA), a safety timer and the delta V detection. There is a famous old MAX713 charger, but according to the features, it offers C/4 to 4C charging and C/16 trickle charging, which is too high. Most commercially available hobby chargers also have a minimum current of 100 mA.&lt;/p&gt;
&lt;p&gt;Thank you,&lt;/p&gt;
&lt;p&gt;David&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;</description></item><item><title>Nice new AD Parts</title><link>https://community.element14.com/thread/54452?ContentTypeID=0</link><pubDate>Wed, 13 Mar 2024 16:12:17 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:a91b32d0-e7b1-4b64-acbd-a7e5f7c25641</guid><dc:creator>michaelkellett</dc:creator><slash:comments>12</slash:comments><comments>https://community.element14.com/thread/54452?ContentTypeID=0</comments><wfw:commentRss>https://community.element14.com/technologies/embedded/f/analogue-design/54452/nice-new-ad-parts/rss?ContentTypeId=0</wfw:commentRss><description>&lt;p&gt;I was going to post this in the Analogue Forum - but there isn&amp;#39;t one, or maybe Audio (nope), or even &amp;quot;Instrumentation &amp;quot;&amp;nbsp; - no.&lt;/p&gt;
&lt;p&gt;So it has to be a blog here.&lt;/p&gt;
&lt;p&gt;Just had a note from ADI about a few rather neat parts:&lt;/p&gt;
&lt;div class="highlight-subheader"&gt;
&lt;h1&gt;ADA4510-2 Op Amp with DigiTrim&lt;span class="emoticon" data-url="https://community.element14.com/cfs-file/__key/system/emoji/2122.svg" title="Tm"&gt;&amp;#x2122;&lt;/span&gt;&lt;/h1&gt;
&lt;h2&gt;Analog Devices&amp;#39; ADA4510-2 precision, 40 V, &amp;plusmn;70 nV/&amp;deg;C, rail-to-rail input and output op amp features DigiTrim&lt;/h2&gt;
&lt;/div&gt;
&lt;p&gt;A very nice low noise, low offset dual op amp remarkably similar to the TO OPA2192.&lt;/p&gt;
&lt;p&gt;Currently only available in 8 pin SOIC.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;div class="highlight-subheader"&gt;
&lt;h1&gt;ADL5960 Analyzer Front End&lt;/h1&gt;
&lt;h2&gt;Analog Devices&amp;#39; ADL5960 10 MHz to 20 GHz integrated vector network analyzer front end supports various LO interface configurations&lt;/h2&gt;
&lt;p&gt;It looks interesting but of course it isn&amp;#39;t a complete VNA - I don&amp;#39;t know enough about the design of such things to tell if its would make a good VNA or just a cheapish one.&lt;/p&gt;
&lt;p&gt;The chip is &amp;pound;133 and the eval board is about &amp;pound;800.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;div class="highlight-subheader"&gt;
&lt;h1&gt;ADG6412/ADG2412 Switches&lt;/h1&gt;
&lt;h2&gt;Analog Devices&amp;#39; ADG6412 and ADG2412 0.5 &amp;Omega; RON quad SPST switches provide high continuous current carrying capability&lt;/h2&gt;
&lt;p&gt;These are nice (if pricey at &amp;pound;6.94 each) quad SPST solid state switches capable of switching serious current and a wide voltage range.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;and finally the:&lt;/p&gt;
&lt;div class="highlight-subheader"&gt;
&lt;h1&gt;MAX17614 Ideal Diodes/Power Source Selector Device&lt;/h1&gt;
&lt;h2&gt;Analog Devices&amp;#39; MAX17614 4.5 V to 60 V, 3 A, ideal diode and power source selector has current limit, UV, and OV protection&lt;/h2&gt;
&lt;p&gt;These look quit nice - I rather wish I had fitted them to my laser controller - it has four buck regulators capable of about 20W each but no easy way to current limit them. If I&amp;#39;d known about these parts I could have used them both for isolation and protection.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;MK&lt;/p&gt;
&lt;/div&gt;
&lt;/div&gt;
&lt;/div&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;</description></item></channel></rss>