Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Pic Microcontrollers Forum Wrong operation when using internally generated negative voltage reference for A/D converter on PIC16F18877
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 201 subscribers
  • Views 1224 views
  • Users 0 members are here
  • pic16
  • reference
  • adc
Related

Wrong operation when using internally generated negative voltage reference for A/D converter on PIC16F18877

Mila_G
Mila_G over 2 years ago

Hello,

please can you help me with the wrong operation when using internally generated negative voltage reference for A/D converter on PIC16F18877?

I would like to use ADC with references 0.416 V and Vdd (5 V).
It works perfectly when I connect 0.416 V to the Vref- pin (RA2) from an external source.

Then I generate 0.416 V on RA2 from FVR and D/A converter as follows:
  FVRCON = 0x84;
  DAC1CON0 = 0xA8;
  DAC1CON1 = 0x0D;
The DAC also works perfectly and there is about 0.416 V on the Vref- pin (RA2).

But now ADC works only if the negative reference is Gnd. If I switch this from Gnd to Vref- (just by changing ADREF from 0 to 0x10), a failure occurs. The voltage on the RA2 pin changes to 2.1 V (and of course the A/D gives bad results).

Workaround attempts:
- 0.416 V output from DAC to RB7, directly conneted to RA2 via a wire, works just as badly as above.
- After interconnecting via an op amp voltage follower instead of the wire, the A/D starts to work properly.

I assumed the PIC analog circuits were designed for internal connections from the VRef- pin, without any external workaround. Please, advise.

Many thanks.

Mila.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago in reply to Mila_G +1
    You explicitly mention in your workaround attempts: Workaround attempts: - 0.416 V output from DAC to RB7, directly conneted to RA2 via a wire, works just as badly as above. I'm merely explaining the…
Parents
  • scottiebabe
    0 scottiebabe over 2 years ago

    You may consider doing the operation digitally. Your increasing the sensitivity 8% or 0.1 bits changing the FSR from 5V to 4.6V. You could subtract 416 mV in software. Sounds like a neat project, best of luck.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • scottiebabe
    0 scottiebabe over 2 years ago

    You may consider doing the operation digitally. Your increasing the sensitivity 8% or 0.1 bits changing the FSR from 5V to 4.6V. You could subtract 416 mV in software. Sounds like a neat project, best of luck.