Experts
  • Technologies
  • More
Experts
Blog EAGLE 6.4.0!! Now available
  • Blog
  • Ask an Expert Forum
  • Documents
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Blog Post Actions
  • Subscribe by email
  • More
  • Cancel
  • Share
  • Subscribe by email
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Richard_H
  • Date Created: 9 Jan 2013 3:48 PM Date Created
  • Views 490 views
  • Likes 0 likes
  • Comments 0 comments
  • ltspice
  • eagle
  • simulation
  • new
  • 6.4.0
  • release
Related
Recommended

EAGLE 6.4.0!! Now available

Richard_H
Richard_H
9 Jan 2013

EAGLE Version 6.4 is now also compatible with MAC 10.8. and includes many bug fixes and new features, such as:

-
Simulation of EAGLE schematics in LTspice IV

- Import of design files from P-CAD, Altium and Protel in ACCEL-ASCII

- Improved user guidance and presetting (tool hints, shortcuts)

- Display and search function of attributes for the ADD- and REPLACE-dialogue

- Search functionality within the control panel tree; display of attributes in the preview for device sets

- Individual properties for DIMENSION command

 

 

Download EAGLE now! ==> http://www.cadsoft.de/download-eagle

 

 

Release notes for EAGLE 6.4.0

=============================

 

* Platforms:

 

  - Added support for MAC OSX 10.8.

 

* Control Panel:

 

  - Added a search bar for searches within the control panel tree.

    Searches can be started via the context menu of a folder or the pulldown menu.

  - Display of attributes in the preview for devicesets.

 

* User Language:

 

  - New ULP constants EAGLE_PATH, EAGLE_DIR, EAGLE_HOME and OS_SIGNATURE.

  - Added the members alwaysvectorfont and verticaltext to UL_BOARD and UL_SCHEMATIC.

  - Added the member UL_TEXT.linedistance.

  - Added new members dtype, extlength, extoffset and extwidth for UL_DIMENSION

    (see DIMENSION section).

 

* ADD command:

 

  - The ADD dialog now has a checkbox that allows to include/exclude packages

    with pads in the search.

  - The ADD dialog of the schematic editor now additionally displays attributes.

    There is also a field for searches within attributes.

 

* DIMENSION command:

 

  - The general settings for dimension objects have been replaced by individual

    properties for each dimension. This includes text size, ratio, unit, precision,

    line width and extension line properties. The properties can be changed by

    CHANGE DUNIT and CHANGE DLINE. That's also available in the CHANGE menu.

    Text properties can be adjusted like for any other text.

    For simplification some parameters like arrow length or text offset

    are no longer offered and internal defaults used.

 

* General GUI improvements:

 

  - Added and adjusted wording, tool tips and status tips of pulldown menus and

    all toolbars.

  - Taken out "Paste from..." from Edit menu in schematic and board editor.

    The identical functionality is available under File/Import.

  - New options "Open Symbol", "Open Package" and "Open Device" available from

    context menu for part instances and elements to open the related library

    entities from schematic or board.

  - Provided a bigger set of default key assignments for frequently used commands

    by extending eagle.scr. The set of internally hardcoded function keys has been

    reduced.

 

* Import/Export:

 

  - Integration of the export of schematic and/or board libraries into EAGLE GUI.

    Now available in File menu under Export/Libraries (a new ULP exp-lbrs.ulp

    is used which replaces the existing exp-project-lbr.ulp).

  - New import-accel.ulp for import of drawings in ACCEL ASCII format. This format

    can be exported from P-CAD, Altium and Protel to import drawings into EAGLE.

  - Under File/Import there are now sub entries for EAGLE drawing (the existing

    "Paste from file" functionality) and the new ACCEL ASCII import.

  - Now dimension objects are handled in the dxf.ulp.

  - A number of further entries have been provided in 'File/Import' and 'File/Export'

    which are handled by existing ULPs. Examples: Export of DXF (dxf.ulp), BOM

    (bom.ulp), Hyperlynx (hyperlynx.ulp), import of bitmaps (import-bmp.ulp).

 

* LTSpice connection on Windows:

 

  - Import of LTSpice schematics into EAGLE and export to LTSpice.

  - LTSpice is a schematic simulation tool for free and available on Windows.

    If installed, a simulation for an existing EAGLE schematic with automatic

    conversion can be started from EAGLE.

  - Possibility to create EAGLE devices from LTSpice library data through import

    of according packages in PADS format, LTSpice symbols and connect lists.

 

* Miscellaneous:

 

  - Now the origins of elements are printed again if their layer is active.

  - If a bus name has a synonym prefix, only that one will be displayed to avoid

    too long labels.

  - Support UNDO/REDO for approval/disapproval of ERC and DRC errors.

  - A number of entries have been added to 'Tools' menu in schematic and layout

    editor. These tools are handled by existing ULPs.

    Examples: Mill outlines (mill-outlines.ulp), drill legend (drillegend-stack.ulp),

    statistics (statistic-brd.ulp, statistic-sch.ulp).

 

* Bugfixes:

 

  - Now the text in the CHANGE TEXT dialog is initially selected again.

  - Fixed DRC clearance calculation for polygons with same rank.

  - Avoiding loss of precision when saving very small grid values.

  - Corrected check for too small grid entries from user.

  - Fixed handling of multiline text objects in polygon calculation.

  - Fix for erroneous ERC warnings in relation to parts of devices

    with predefined value (attribute 'VALUE').

  - Correction in online help: VALUE command only available in default assembly variant.

  - CHANGE PACKAGE/TECHNOLOGY: Ensure update of library attributes if they are displayed

    but haven't been changed in schematic or board.

  - Fixed a crash if a part is replaced by a device without package.

  - Fixed handling of arbitrary pad shapes in the DRC.

  - Avoided a crash if mixing the selection within nearby objects and textual input.

  - Fixed a crash when doing a GATESWAP with an uninvoked gate.

  - Fixed potential crash on MAC related to switching between editor windows, text window

    or CAM processor window.

  - Fixed graphic issues on MAC (display of popup menus).

  - Fixed handling of dimensions in XML regarding extlength and extoffset.

  - Fixed a crash in PRINT command on Windows if a previously used network printer is

    uninstalled and EAGLE restarted.

  - Fixed f/b annotation of attributes when copying parts in the schematic.

  - Fixed displaying the pad names in the device preview of the ADD dialog.

 

Best regards,

Richard Hammerl

Anonymous