Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum CRYDOM 1F25 FILTER Application
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 339 subscribers
  • Views 922 views
  • Users 0 members are here
  • harmonics
  • emi_noise
  • triac
  • triac_dimmers
  • ssr
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

CRYDOM 1F25 FILTER Application

e14 Contributor
e14 Contributor over 10 years ago

Hi.

 

I've been told that this device is what I need for my project.

 

I want to control a triac in phase angle mode to drive a water heater (not more than 2,5KW) similar to a dimmer.

 

I've been advised that this solution can generate undesired harmonics that have to be corrected and this product was pointed as a solution 1F25 - CRYDOM - FILTER, SSR, 1 PHASE | Farnell element14.

 

Is this the correct article for my needs?

Is there a more a appropriate article? (Possibly less expensive)

 

I'm using a simple circuit with a MOC3011 or MOC3021 (without zero crossing sensor) and a triac like BT139 (later I will change to one that can handle higher power).

 

Any advice will be welcome.

 

Cheers.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Anyone, please.

     

    If anyone that is seeing this post know someone that can answer, please ask him.

     

    Cheers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • PeteB
    PeteB over 10 years ago

    Hi Cidi.

     

    I apologize for not seeing your original question.  It didn't pop up in the SSR section where I receive notifications but I trust that the following will provide you with the info on what the 1F25 filter is and does, and it should be of use to you.

     

    It is a correct statement that phase angle control will tend to create varying levels of undesired electrical harmonic noise when operated at phase angles other than full on or full off.  In many of those cases, the harmonic nose may exceed that allowed by the EN standards.  Fortunately, in many of those cases, a bypass filter (like the 1F25) can reduce the noise to an acceptable level.  I've attached here an "ancient" technical paper that Crydom had generated just about 20 years ago on the SSR Filters that should be of use to explain what it does and why it works.  The contact information on this old paper is quite out of date, but the content isn't.  


    You ask about an alternative...    Most "line conditioning" types of filters would be a more thorough solution, (since they pass the full load current through the filter), but they tend to be more expensive than the bypass filter since load current enters into the picture and they are sized accordingly.

     

    Regards,

    Pete B.

    Attachments:
    imageFilter App Notes.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to PeteB

    Hi.

     

    Thank you for your answer.

     

    I've read the document and based on what I've read and what you said this product should be the most cost efective product for my needs.

     

    If you have anything more to add, please, I would appreciate your input.

     

    Cheers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to e14 Contributor

    If you are controlling  a water heater it is a mistake to use phase angle control with its attendant interference problems. You can use zero voltage switching so that you power the heater for complete mains cycles (or half cycles, but full cycles is better). The thermal time constant of  a 2.5kW water heater and the water tank will be quite long so you can supply 1/4 power by (for example) 100 cycles on and 300 cycles off  - which is on for two seconds and off for 6 (at 50Hz). This would be fine for  water heater (but bad for  a light dimmer image).

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelkellett

    Hi.

     

    Thank you for your input.

     

    I've been analyzing that for a while and I don't know if it will work correctly because that way I cannot fixate a constant power consumption.

     

    The objective is to consume the solar energy production that is not being consumed by other devices at home and prevent it from going into the grid and be lost.

     

    The problem is that, I believe that my utility meter (very recent one) has a very small energy packet and with that method I may be allowing power to be lost and at the same time be paying.

     

    The other problem I believe may happen is the flickering caused by the on-off.

     

    I'm divided...

     

    Cheers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to e14 Contributor

    I think you would need to check the specification of the meter very carefully to know if zero voltage switching would work for your meter (and the spec may well not really say).

     

    Probably phase angle control and filtering is the only way.

     

    MK.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelkellett

    Hi.


    I've found a manual of a similar model that I've read most and I think there isn't anything about that there.

     

    And I can not be sure because I've noticed that the impulse led seems to also flash when the energy flow is negative (putting energy to the grid) so it is very hard to know if it is counting or not.

     

    Cheers.