Hello everyone,
I have some questions about voltage regulators (it's the first time I'm dealing with them, so the question are *really* basic - but I wasn't able to find answers anywhere, so I've figured I'll ask).
I have a 6 AA battery pack that I want to get 5 volts out of. First I got this voltage regulator and it seems to be working: https://www.adafruit.com/products/2164
However, it's dropdown can be as high as 2.5V, meaning that once the batteries go below 1.25 V each (which as far as I know is not the end of their lifetime) it may stop working (if I understand correctly. Or will this one do fine?).
Anyway, I've decided to get a regulator with a lower dropdown. I got these two (I expect the output current to be around 1A, so I got ones that support >= 1.5A just in case)
MIC29150-5.0WT - MICREL SEMICONDUCTOR - LDO VOLTAGE REGULATOR, 5V, 1.5A, TO-220 | Newark element14
Now basically my questions are:
- what capacitor should I use on the input? The spec doesn't really specify that. It only marks it as "C In". Does the value of that really matter? Will 10uF work fine (so I'd have 10uF on both input & output)?
- just out of curiosity - what really is the difference between them? Seems like the second one supports higher current and has slightly higher dropdown. Is that really the only thing? Will they pretty much operate the same, or will the second one like get more warm or something? Basically what I'm trying ot ask is - why would anyone want to use the first one over the second one?
Thanks,
Tom