Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is the correct way to replace a 7805 voltage regulator w/ heatsink?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 335 subscribers
  • Views 1647 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is the correct way to replace a 7805 voltage regulator w/ heatsink?

andywest
andywest over 7 years ago

I have an Atari 2600, and I want to replace the 7805 voltage regulator with one that can handle more current so I can power certain devices off the cartridge port. It looks like the stock regulator is screwed down to exposed metal on the board. I assume this is for heat dissipation?

 

If I get a TO-220 package regulator with a clip-on heatsink like this one:

 

https://www.adafruit.com/product/977

 

can I just screw the whole thing down to the board with some fresh thermal paste? The heatsink has a screw hole as well, so I assume it's designed to be used that way?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 7 years ago +9 verified
    Hi Andy! I don't think there is an issue with screwing it down. But, this would be way better than the 7805: Murata DC DC converter Murata DC DC converter or if it fits the space physically, then this…
  • andywest
    andywest over 7 years ago in reply to shabaz +4
    Wow, that's great, shabaz ! I was feeling silly for asking such a simple question, but now I'm glad I did. I will definitely follow your recommendation.
  • shabaz
    0 shabaz over 7 years ago

    Hi Andy!

     

    I don't think there is an issue with screwing it down.

    But, this would be way better than the 7805: Murata DC DC converterMurata DC DC converter

    or if it fits the space physically, then this one is preferred: Recom DC DC converterRecom DC DC converter

     

    Both of these give off far less heat, so no heatsink is needed. The Murata one offers up to 1.5A, the Recom one supports 2A. Your Atari will run cooler with this, and will go a long way toward not being a bottleneck if you need more power for external devices.

     

    They are pin-compatible too, so are drop-in replacements.

    • Cancel
    • Vote Up +9 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • andywest
    0 andywest over 7 years ago in reply to shabaz

    Wow, that's great, shabaz! I was feeling silly for asking such a simple question, but now I'm glad I did. I will definitely follow your recommendation.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer