Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Ideas for changing the color temperature of these LED work lights. Will this work? Or is there a better way?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 311 subscribers
  • Views 4321 views
  • Users 0 members are here
  • led_lighting_strips
  • led
  • led_lighting
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Ideas for changing the color temperature of these LED work lights. Will this work? Or is there a better way?

baldengineer
baldengineer over 2 years ago

image

On my (actual) workbenches, I have overhead LED light bars. I'm very happy with the amount of light they provide. However, their color temperature is warmer than I like. Their temperature is especially annoying when doing video/photo work because it makes everything look gross. (I waste a lot of time color-correcting videos from my bench!)

I'd like to replace the LEDs to get 5700K-6000K lights instead.

First, I checked to see if Global Industrial has another color, but they only sell 4000K lights in this configuration. Bummer.

I took one light bar apart. There are two LED strips inside, each operating off of 45 VDC. There are 135 LEDs on each with a 2835 package size. Doing some clever (lol) measurements, I found there are 15 LEDs in series, and 9 of those groups are in parallel. (There are +/- terminals at either end of the strips.)

Turns out, the description part number spells all of that out: 18c-15x9(2835)1171-v2b. So much for my clever measurements.

Edge of Global Industrial LED Light Bar

I'm not convinced that the LEDs are soldered to an aluminum substrate.

Will this work?

So here is what I'm thinking: replace the SMD LEDs. The strips only have two wire connections to the supply. So removing them from the (aluminum?) enclosure should be relatively easy.

My plan is to use a hot plate to pre-heat a small section of the strip and hot air to hit reflow. This should allow me to remove and re-install LEDs. Quickly, right?

But. Am I overlooking something? Is there a reason the soldering won't go well? Or is there another way to approach this problem?

image

I did consider just using generic "LED Strips." But they all seem to operate off of 12 Vdc. I'm not in the mood to re-design the supply section.

What do you all think? Any other ideas or concerns I should consider?

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 2 years ago +1
    That's a long way to go to get the right colour temperature - and then again, maybe it's also worth paying attention to CRI as well. It will probably work assuming all is well, but prolonged heat will…
  • baldengineer
    baldengineer over 2 years ago in reply to Gough Lui +1
    Gough Lui said: Camera custom white balancing with a grey card generally works as long as you don't then have something active (e.g. an LCD screen) in shot that has its own colour temperature. You mean…
  • shabaz
    shabaz over 2 years ago +1
    Hi James, I too think it could be a partially CRI issue as well. I'll ask a friend tomorrow for his opinion (he's a cameraman for a national broadcaster). I know he's suggested full color LED lights…
Parents
  • Gough Lui
    Gough Lui over 2 years ago

    That's a long way to go to get the right colour temperature - and then again, maybe it's also worth paying attention to CRI as well. It will probably work assuming all is well, but prolonged heat will soften/char the FR4 substrate and doing it in sections may cause warpage that may potentially affect the connection reliability (because the "shape" of the PCB is changing due to differential heating/cooling).

    An optical filter may be possible - but you will cut down on the light quite a bit using something like a cool filter. Camera custom white balancing with a grey card generally works as long as you don't then have something active (e.g. an LCD screen) in shot that has its own colour temperature.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to Gough Lui
    Gough Lui said:
    Camera custom white balancing with a grey card generally works as long as you don't then have something active (e.g. an LCD screen) in shot that has its own colour temperature.

    You mean ... like in every video I shoot? Slight smile

    The ultimate challenge with color correcting is that exposure isn't constant when moving the camera around. I can't shoot the reference card every time. (and I'd like to move towards more inpromtu shooting.)

    But, aside from that, I don't like the warm temperature when soldering or inspecting something anyway. So it's a double dislike.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 2 years ago in reply to Gough Lui
    Gough Lui said:
    Camera custom white balancing with a grey card generally works as long as you don't then have something active (e.g. an LCD screen) in shot that has its own colour temperature.

    You mean ... like in every video I shoot? Slight smile

    The ultimate challenge with color correcting is that exposure isn't constant when moving the camera around. I can't shoot the reference card every time. (and I'd like to move towards more inpromtu shooting.)

    But, aside from that, I don't like the warm temperature when soldering or inspecting something anyway. So it's a double dislike.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Gough Lui
    Gough Lui over 2 years ago in reply to baldengineer
    baldengineer said:
    exposure isn't constant when moving the camera around

    Well, with custom white balance, I set it once for the light I'm using and then it's kept as a setting on the camera. Otherwise, I use white balance corrections in post (in a way, similar to Auto Colour in Premiere Pro).

    Unfortunately, this becomes very problematic when LCD screens are around since many are backlit at about 6500K, so if I correct for my 2700K source, it looks horrible. Alternatively, correcting for the screen means the background is horrible.

    image

    (White balance corrected for LCD, but room lighting 2700K makes everything look orange)

    image

    (Room lit by 2700K source as above, but since no active source of light at any other colour temperature, I custom white balance adjusted on the grey ESD mat and all looks well)

    It's a problem I'm starting to fight with too ... especially since RoadTest sponsors would like to see video ...

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to Gough Lui
    Gough Lui said:
    It's a problem I'm starting to fight with too ... especially since RoadTest sponsors would like to see video ...

    Haha, yeah. To me, it is like learning how to use text formats correctly.