On my (actual) workbenches, I have overhead LED light bars. I'm very happy with the amount of light they provide. However, their color temperature is warmer than I like. Their temperature is especially annoying when doing video/photo work because it makes everything look gross. (I waste a lot of time color-correcting videos from my bench!)
I'd like to replace the LEDs to get 5700K-6000K lights instead.
First, I checked to see if Global Industrial has another color, but they only sell 4000K lights in this configuration. Bummer.
I took one light bar apart. There are two LED strips inside, each operating off of 45 VDC. There are 135 LEDs on each with a 2835 package size. Doing some clever (lol) measurements, I found there are 15 LEDs in series, and 9 of those groups are in parallel. (There are +/- terminals at either end of the strips.)
Turns out, the description part number spells all of that out: 18c-15x9(2835)1171-v2b. So much for my clever measurements.

I'm not convinced that the LEDs are soldered to an aluminum substrate.
Will this work?
So here is what I'm thinking: replace the SMD LEDs. The strips only have two wire connections to the supply. So removing them from the (aluminum?) enclosure should be relatively easy.
My plan is to use a hot plate to pre-heat a small section of the strip and hot air to hit reflow. This should allow me to remove and re-install LEDs. Quickly, right?
But. Am I overlooking something? Is there a reason the soldering won't go well? Or is there another way to approach this problem?

I did consider just using generic "LED Strips." But they all seem to operate off of 12 Vdc. I'm not in the mood to re-design the supply section.
What do you all think? Any other ideas or concerns I should consider?