Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Ideas for changing the color temperature of these LED work lights. Will this work? Or is there a better way?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 311 subscribers
  • Views 4315 views
  • Users 0 members are here
  • led_lighting_strips
  • led
  • led_lighting
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Ideas for changing the color temperature of these LED work lights. Will this work? Or is there a better way?

baldengineer
baldengineer over 2 years ago

image

On my (actual) workbenches, I have overhead LED light bars. I'm very happy with the amount of light they provide. However, their color temperature is warmer than I like. Their temperature is especially annoying when doing video/photo work because it makes everything look gross. (I waste a lot of time color-correcting videos from my bench!)

I'd like to replace the LEDs to get 5700K-6000K lights instead.

First, I checked to see if Global Industrial has another color, but they only sell 4000K lights in this configuration. Bummer.

I took one light bar apart. There are two LED strips inside, each operating off of 45 VDC. There are 135 LEDs on each with a 2835 package size. Doing some clever (lol) measurements, I found there are 15 LEDs in series, and 9 of those groups are in parallel. (There are +/- terminals at either end of the strips.)

Turns out, the description part number spells all of that out: 18c-15x9(2835)1171-v2b. So much for my clever measurements.

Edge of Global Industrial LED Light Bar

I'm not convinced that the LEDs are soldered to an aluminum substrate.

Will this work?

So here is what I'm thinking: replace the SMD LEDs. The strips only have two wire connections to the supply. So removing them from the (aluminum?) enclosure should be relatively easy.

My plan is to use a hot plate to pre-heat a small section of the strip and hot air to hit reflow. This should allow me to remove and re-install LEDs. Quickly, right?

But. Am I overlooking something? Is there a reason the soldering won't go well? Or is there another way to approach this problem?

image

I did consider just using generic "LED Strips." But they all seem to operate off of 12 Vdc. I'm not in the mood to re-design the supply section.

What do you all think? Any other ideas or concerns I should consider?

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 2 years ago +1
    That's a long way to go to get the right colour temperature - and then again, maybe it's also worth paying attention to CRI as well. It will probably work assuming all is well, but prolonged heat will…
  • baldengineer
    baldengineer over 2 years ago in reply to Gough Lui +1
    Gough Lui said: Camera custom white balancing with a grey card generally works as long as you don't then have something active (e.g. an LCD screen) in shot that has its own colour temperature. You mean…
  • shabaz
    shabaz over 2 years ago +1
    Hi James, I too think it could be a partially CRI issue as well. I'll ask a friend tomorrow for his opinion (he's a cameraman for a national broadcaster). I know he's suggested full color LED lights…
Parents
  • shabaz
    shabaz over 2 years ago

    Hi James,

    I too think it could be a partially CRI issue as well. I'll ask a friend tomorrow for his opinion (he's a cameraman for a national broadcaster). I know he's suggested full color LED lights to me in the past, but I didn't ask him about task lighting. In your case it is task lighting as well as video lighting.

    What video tool do you use by the way? It may have an option to do automatic color-correcting. With Davinci Resolve, it is automated. You can use a color test chart (they cost about $60 upward) and as long as you have a snippet of video with that test chart in view, then the software will be able to color-correct, and that will work for a range of colors, since it's more than a simple warm/cold adjustment.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to shabaz

    To expand on my other response, the complication is that the temperature difference between the overhead (spot) and other lights (key/fill) cause a lot of color correction problems. I know most people don't catch it, but it is something I see. E.g., a breadboard's white is completely different from an instrument's front panel white. So I have to either do a bunch of masking or pick an in between.

    But more than that, everything in my lab is very cool white, except the work benches. So even outside of videography, I don't like the temp.

    CRI is something I had not given much attention to before, so I'm quickly understanding how that plays a role!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 2 years ago in reply to shabaz

    To expand on my other response, the complication is that the temperature difference between the overhead (spot) and other lights (key/fill) cause a lot of color correction problems. I know most people don't catch it, but it is something I see. E.g., a breadboard's white is completely different from an instrument's front panel white. So I have to either do a bunch of masking or pick an in between.

    But more than that, everything in my lab is very cool white, except the work benches. So even outside of videography, I don't like the temp.

    CRI is something I had not given much attention to before, so I'm quickly understanding how that plays a role!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 2 years ago in reply to baldengineer

    I see.. that does cause problems, if there is a mix of color temperatures in the room! In that case there's nothing to be done other than modify one or the other to match, or to turn off one of them.

    It looks like it might just be FR4, so that should work to remove the LEDs and attach new ones.

    image

    I tried to make my own LED board too (out of FR4). I had to pause to work on a RoadTest, so it's been in limbo but I should try to solder the LEDs at some point. I too am going to use a pre-heater and hot air tool, but I might use low-temp solder because I've never used hot air for LEDs before and I don't know that I trust myself with it too much. A reflow oven might be safer. I've procrastinated quite a bit, in part because I can't decide how to approach the soldering exercise.

    These panels are for warm and cold LEDs (its for this PicoChroma project I attempted at the start of the year).

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to shabaz

    Hmm, maybe using hot air to solder LEDs is a bad idea, especially when their color output is important.

    Maybe I will use hot air to remove the existing LEDs but pencil solder in the new ones.

    Also, I was planning to test a strip with the various LEDs I bought. Perhaps I could do an A/B test of hot air versus pencil tip.