Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Solder able prototype board for 5A
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 303 subscribers
  • Views 141 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Solder able prototype board for 5A

flows
flows 21 days ago

Hello, 

I need to create an IoT project that will automate something in my life. So i am making a automatic sunscreen controller which will make the screen go up or down based on the weather.

Now im almost finished with the project, it was time to connect the electronics. I am no expert at electronics so i looked up if i can just connect the nema 17 stepper motor to the power supply via the breadboard. As of my knowledge the Nema 17, at its peak, takes 1.7 amps per coil, it has two coils. So thats at most 3.4 amps. I have a power supply to power everything of 12V and 5A. It will melt the plastic of the breadboard with that current. 

So i was thinking maybe i could just put it on a solderable prototype board which makes it more secure, safe, and i will gain some extra points (yes thats something you can score on).

But i have no idea how i can know what prototype board can handle that current. Its also not stated on the sellers page.

On a arduino form someone recommended this prototype board: https://www.amazon.co.uk/Gikfun-Solder-able-Breadboard-Arduino-GK1007U/dp/B07D7PMCG5

But when i ask AI it says the board will also melt. Am i being misled by AI Sob? 

Picture of system:

Note: in this picture i use a expansion board because i though i couldn't directly connect the DRV8825 to the breadboard. 

image

  • Sign in to reply
  • Cancel

Top Replies

  • obones
    obones 21 days ago +2
    Those will take quite a bit of current, the pads are quite large. If you use solder to "bridge" the gaps between the pads, you'll get a quite large metallic junction which should be fine for the current…
  • kmikemoo
    kmikemoo 21 days ago in reply to obones +2
    flows obones was faster than me. ...What he said. If you really want to run that current on the protoboard - for just the driver board, "reinforce" that part of the trace with 18 or 20 AWG. Tack it to…
  • obones
    obones 19 days ago in reply to flows +2
    ESP32 doesn't even come close to 1A, the regulator won't even get hot.
Parents
No Data
Reply
  • Jan Cumps
    0 Jan Cumps 18 days ago in reply to $parentForumReply.Author.DisplayName

    AI generated