Data files for the FlaviaP32 implementation of the Free Logic Array, described in this 'blog entry.
This work is licensed under the Creative Commons Attribution-ShareAlike 3.0 Unported License. To view a copy of this license, visit creativecommons…
Data files for the FlaviaP32 implementation of the Free Logic Array, described in this 'blog entry.
This work is licensed under the Creative Commons Attribution-ShareAlike 3.0 Unported License. To view a copy of this license, visit creativecommons…
Source code and makefiles for XXICC code release 0.0k. You should be able to edit make, .h, and .c files using any text editor. .gal files may contain control characters that confuse your text editor, so you may need to use the XXICC Object Editor (XOE…
This book is a collection of miscellaneous XXICC topics. It supplements "Programming in the GalaxC Language".
For more information on XXICC, see the 'blog post XXICC (21st Century Co-design) release 0.0k and XXICC's home page: xxicc.…
Lancero SGDMA PCI Express IP core with Windows, Linux, QNX drivers.
Faster download with quick configuration of Altera devices will shorten your design cycle and allow you to deliver the products in the market at desired time. SLS BitJet Lite will make this possible. Visit http://www.slscorp.com/pages/usbbitjet_lite.…
SLS recently launched USB 3.0 Development board with Cyclone IV FPGA. Additional peripherals included make the board much more suitable for this age product prototyping. Peripherals include: DDR2 SDRAM, NAND Flash, CFI FLASH, SDRAM, SD Host and many more…
This is a compiled and linked XXICC executable binary "xxicw.exe" for Microsoft Windows on x86 PCs for users who do not want to build it from source code. "xxicw.exe" was built as described in Installing and Running XXICC rev 0.0q
…FlaviaLB60-00r.zip contains data files for the FlaviaLB60 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0r. FlaviaLB60 is for the ValentF(x) LOGI-Bone FPGA board, rev R1.0…
FlaviaLP60-00r.zip contains data files for the FlaviaLP60 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0r. FlaviaLP60 is for the ValentF(x) LOGI-Pi FPGA board, rev R1.2.
…Data files for the FlaviaPD59 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Raspberry Pi 2 meets Papilio DUO. FlaviaPD59 is for the Gadget Factory Papilio DUO. To reduce chances of confusion, I recommend that you…
Data files for the FlaviaP60 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0r. FlaviaP60 is for the Gadget Factory Papilio One 500K FPGA board. To reduce chances of confusion…
Data files for the FlaviaP40 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0r. FlaviaP40 is for the Gadget Factory Papilio One 250K FPGA board. To reduce chances of confusion…
GCHD example files for generating Lattice iCE40 FPGA using IceStorm, as described in Chapter 15 of The XXICC Anthology rev 0.0r. Synthesis targets are Lattice iCEstick or Nandland Go Board.
GCHDis part of XXICC. For more information on GalaxC and XXICC…
These are the .xoe files for "Programming in the GalaxC Language", "The XXICC Anthology", install.pdf, compile.pdf, and TamingWB.pdf. It also includes the .gal files for collecting the individual .xoe chapter files into a book with…
This document contains the source code for XXICC revision 0.0r in PDF for the convenience of users and developers who want to look at GalaxC source code without installing the XXICC Object Editor (XOE). .gal files are ASCII, but may contain control characters…
Source code and makefiles for XXICC code release 0.0r. You should be able to edit make, .h, and .c files using any text editor. .gal files may contain control characters that confuse your text editor, so you may need to use the XXICC Object Editor (XOE…
This book is a collection of miscellaneous XXICC topics. It supplements "Programming in the GalaxC Language".
For more information on GalaxC and XXICC, see the 'blog post XXICC (21st Century Co-design) release 0.0r and XXICC's home page …
Summary of enhancements and bug fixes for XXICC revision 0.0r.
For more information on XXICC and GalaxC, see the ’blog post XXICC (21st Century Co-design) release 0.0r and XXICC’s home page xxicc.org.