This is a compiled and linked XXICC executable binary "xxicw.exe" for Microsoft Windows on x86 PCs for users who do not want to build it from source code. "xxicw.exe" was built as described in Installing and Running XXICC rev 0.0q
…This is a compiled and linked XXICC executable binary "xxicw.exe" for Microsoft Windows on x86 PCs for users who do not want to build it from source code. "xxicw.exe" was built as described in Installing and Running XXICC rev 0.0q
…This document contains the source code for XXICC revision 0.0q in PDF for the convenience of users and developers who want to look at GalaxC source code without installing the XXICC Object Editor (XOE). .gal files are ASCII, but may contain control characters…
Source code and makefiles for XXICC code release 0.0q. You should be able to edit make, .h, and .c files using any text editor. .gal files may contain control characters that confuse your text editor, so you may need to use the XXICC Object Editor (XOE…
This book is a collection of miscellaneous XXICC topics. It supplements "Programming in the GalaxC Language".
For more information on XXICC, see the 'blog post XXICC (21st Century Co-design) release 0.0q and XXICC's home page: xxicc.…
Summary of enhancements and bug fixes for XXICC revision 0.0q.
For more information on XXICC and GalaxC, see the ’blog post XXICC (21st Century Co-design) release 0.0q and XXICC’s home page: xxicc.org.
This document contains the source code for XXICC revision 0.0p in PDF for the convenience of users and developers who want to look at GalaxC source code without installing the XXICC Object Editor (XOE). .gal files are ASCII, but may contain control characters…
Source code and makefiles for XXICC code release 0.0p. You should be able to edit make, .h, and .c files using any text editor. .gal files may contain control characters that confuse your text editor, so you may need to use the XXICC Object Editor (XOE…
Summary of enhancements and bug fixes for XXICC revision 0.0n.
For more information on XXICC and GalaxC, see the 'blog post XXICC (21st Century Co-design) release 0.0n and XXICC's home page: xxicc.org.
0.0n adds two Xilinx Spartan-6 Flavia implementations…
These are the .xoe files for "Programming in the GalaxC Language", "The XXICC Anthology", install.pdf, compile.pdf, and TamingWB.pdf. It also includes the .gal files for collecting the individual .xoe chapter files into a book with…
Data files for the FlaviaLB56 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0n. FlaviaLB56 is for the ValentF(x) LOGI-Bone FPGA board. To reduce chances of confusion, I recommend…
Data files for the FlaviaLP56 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0n. FlaviaLP56 is for the ValentF(x) LOGI-Pi FPGA board. To reduce chances of confusion, I recommend…
Data files for the FlaviaP48 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0n. FlaviaP48 is for the Gadget Factory Papilio One 500K FPGA board. To reduce chances of confusion…
Data files for the FlaviaP32 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0n. FlaviaP32 is for the Gadget Factory Papilio One 250K FPGA board. To reduce chances of confusion…
These are compiled and linked XXICC executable binaries built as described in Installing and Running XXICC rev 0.0n, for users who do not want to build XXICC executables from source code. Includes executables for GNU/Linux on x86 PCs, Raspberry Pi, and…
This document describes how to install and run XXICC on your computer, either by compiling XXICC source code or installing binaries.
This is revision 0.0n, which adds sections 6 and 7 for setting Raspberry Pi and BeagleBone permissions for the ValentF…
This document contains the source code for XXICC revision 0.0n in PDF for the convenience of users and developers who want to look at GalaxC source code without installing the XXICC Object Editor (XOE). .gal files are ASCII, but may contain control characters…
Source code and makefiles for XXICC code release 0.0n. You should be able to edit make, .h, and .c files using any text editor. .gal files may contain control characters that confuse your text editor, so you may need to use the XXICC Object Editor (XOE…
This book is a collection of miscellaneous XXICC topics. It supplements "Programming in the GalaxC Language".
For more information on XXICC, see the 'blog post XXICC (21st Century Co-design) release 0.0n and XXICC's home page: xxicc.…
Data files for the FlaviaP48 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0m. FlaviaP48 is for the Papilio One 500K FPGA board. Only install this file if you want to synthesize…
Data files for the FlaviaP32 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0m. FlaviaP32 is for the Papilio One 250K FPGA board. Only install this file if you want to synthesize…
These are the .xoe files for "Programming in the GalaxC Language", "The XXICC Anthology", install.pdf, compile.pdf, and TamingWB.pdf. It also includes the .gal files for collecting the individual .xoe chapter files into a book with…
These are compiled and linked XXICC executable binaries built as described in Installing and Running XXICC rev 0.0m, for users who do not want to build XXICC executables from source code. Includes executables for GNU/Linux on x86 PCs, Raspberry Pi, and…
This document describes how to install and run XXICC on your computer, either by compiling XXICC source code or installing binaries.
This is revision 0.0m, which is updated for Raspbian 09-09-2014 for RasPi and Debian 05-14-2014 for BeagleBone.
For more…
This document contains the source code for XXICC revision 0.0m in PDF for the convenience of users and developers who want to look at GalaxC source code without installing the XXICC Object Editor (XOE). .gal files are ASCII, but may contain control characters…
Source code and makefiles for XXICC code release 0.0m. You should be able to edit make, .h, and .c files using any text editor. .gal files may contain control characters that confuse your text editor, so you may need to use the XXICC Object Editor (XOE…