I haven't done a poll in a while so I thought it would be fun and instructive to do one about less-expensive FPGA boards. One of the challenges of getting into FPGA design is that the boards are usually a lot more expensive than a Raspberry Pi or…
I haven't done a poll in a while so I thought it would be fun and instructive to do one about less-expensive FPGA boards. One of the challenges of getting into FPGA design is that the boards are usually a lot more expensive than a Raspberry Pi or…
Hi,
I heard that the timing of FPGA signals can be changed via a MS Office Excel file.
The timing of the signals could be designed in an Excel file and then, maybe after conversion, uploaded via RS232 or SPI to the FPGA.
In this way the timing could be changed…
How can I interface external analog signals (from a potentiometer for example) and display the bits on the user LEDs? Is it also possible to apply fourier transform on these analog signals? I have both Cyclone 10 LP evaluation kit and the DE 10 Nano standard…
|
Lancero SGDMA PCI Express IP core with Windows, Linux, QNX drivers.
Faster download with quick configuration of Altera devices will shorten your design cycle and allow you to deliver the products in the market at desired time. SLS BitJet Lite will make this possible. Visit http://www.slscorp.com/pages/usbbitjet_lite.…
SLS recently launched USB 3.0 Development board with Cyclone IV FPGA. Additional peripherals included make the board much more suitable for this age product prototyping. Peripherals include: DDR2 SDRAM, NAND Flash, CFI FLASH, SDRAM, SD Host and many more…
There's been quite a lot of talk in the FPGA group about cheap ways to get started so a couple of weeks ago I decided to forsake the professional setup I use for real work and try one of the cheapest routes I could find. The idea was to try something…
I have developed the following design as the framework for the bus interface of USB2 interfaced FPGA based instruments.
This firmware in intended to aid the design of instrumentation using the Morph-IC-II module and other fpga systems interfaced to the…
FPGA gets its power from the flexibility. The design process can be time-consuming but you can design basically anything. In this project, I will give some examples of the multiplication and flexibility of FPGAs.
Multiplication consumes time and sometimes…
I have been chosen as a roadtester for DEO-NANO P0082 and my kit has arrived. I decided before going roadtest project, it will be nice to give a heartbeat and step into FPGA world. Before you go reading, I want to say I am not an FPGA expert but I want…
Hello.
I had a great opportunity to test and to review the Terasic new flagship, the DE10-Standard FPGA-SoC board.
We will take a look at what this product has to offer, what is its target group and if it is worth its money.
…Hello, i am facing small problem with FPGA programming.
Problem is simple, i have unknown length trigger pulse (1ns-5us) that should start CCD readout. What i need is to be able to make that signal as short as possible, so i don't waste clock cycles to…
If you have an interest in exchanging data between circuitry in an FPGA and a PC, I have written a simple GUI that demonstrates transfers at full USB2 rates to and from an FPGA interfaced with an FTDI FT2232H USB2 interface chip (i.e. the FTDI Morph-IC…
Altera this morning announced Stratix V, their first 28nm FPGA. The new FPGA family provides up to 1.1 million logic elements, 53-Mbits embedded memory, 3,680 18x18 multipliers and integrated transceivers. The full press release can be found in the documents…
I'm still a complete noob with FPGAs, but as part of my digging around I came across ARM's new DesignStart program. It appears to be a royalty free ARM M0 or M3 core for Altera and Xilinx FPGAs. I thought it might interest a few people here.