Internet of Things
  • Technologies
  • More
Internet of Things
Blog Spark Core IoT Controller
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 16 Jan 2015 9:53 PM Date Created
  • Views 989 views
  • Likes 1 like
  • Comments 3 comments
  • core
  • mqtt
  • internet_of_things
  • spark_core
  • spark
  • iot
Related
Recommended

Spark Core IoT Controller

fvan
fvan
16 Jan 2015

  • Introduction
  • Prototype
  • Code
  • Demo
  • Next Steps

 

Introduction

 

Since I got my Spark Core, I've been fiddling without really knowing what I wanted to do with it. Lately, I've also been playing with my Rapiro again, and that's when I got the idea to build a physical controller for the robot, with at its heart a Spark Core.

image

 

The controller would be used to send different MQTT messages depending on which button was pressed. Rapiro (or any other IoT device, really) would be configured with a MQTT client and would be able trigger certain actions based on the received messages.

 

This post is about building the controller and performing some initial tests.

 

 

Prototype

 

Yesterday evening, I started browsing my different bins of parts to find the necessary components to build the controller I had in mind. The list of required components was the following:

  • Spark Core
  • prototyping board
  • pushbuttons (14)
  • 1x12 female header (2)
  • 4xAA battery pack

 

Having found everything I needed, I proceeded by laying out the different components on the prototyping board. Luckily enough, everything fit and I moved on to soldering all the buttons and making the connections.

imageimage

 

The layout is pretty basic:

  • centrally, the Spark Core with the RGB LED used to display status information
  • on the left, five buttons which can be used for movement actions
  • on the right, nine buttons which can be used for various functions

 

Code

 

For the code, I used Chris Howard's port of Nick O'Leary's PubSubClient for Arduino, combined with my sketch below. I've added comments in the code, so it should be clear what I'm trying to achieve, but to summarise:

  • every pin is set as an input which is HIGH by default, using an internal pull-up resistor
  • pressing a button will pull the pin down to ground, setting it LOW
  • the onboard RGB LED is used to display status information:
    • red: not connected to MQTT broker
    • green: connected to MQTT broker
    • blue: button is being pressed
  • check if connected to broker, if not: reconnect
  • check if button is pressed, if yes: publish MQTT message

 

int BTN_A0 = A0;
int BTN_A1 = A1;
int BTN_A2 = A2;
int BTN_A3 = A3;
int BTN_A4 = A4;
int BTN_A5 = A5;
int BTN_A6 = A6;
int BTN_A7 = A7;

int BTN_D0 = D0;
int BTN_D1 = D1;
int BTN_D2 = D2;
int BTN_D3 = D3;
int BTN_D4 = D4;
int BTN_D5 = D5;
int BTN_D6 = D6;
int BTN_D7 = D7;

long lastRetry = 0;

TCPClient tcpClient;
PubSubClient client("iot.eclipse.org", 1883, 0, tcpClient);

void setup() {
    // onboard RGB LED will be used
    RGB.control(true);
  
    // use internal pull-ups, all pins HIGH by default
    pinMode(BTN_A0, INPUT_PULLUP);
    pinMode(BTN_A1, INPUT_PULLUP);
    pinMode(BTN_A2, INPUT_PULLUP);
    pinMode(BTN_A3, INPUT_PULLUP);
    pinMode(BTN_A4, INPUT_PULLUP);
    pinMode(BTN_A5, INPUT_PULLUP);
    pinMode(BTN_A6, INPUT_PULLUP);
    pinMode(BTN_A7, INPUT_PULLUP);

    pinMode(BTN_D0, INPUT_PULLUP);
    pinMode(BTN_D1, INPUT_PULLUP);
    pinMode(BTN_D2, INPUT_PULLUP);
    pinMode(BTN_D3, INPUT_PULLUP);
    pinMode(BTN_D4, INPUT_PULLUP);
    pinMode(BTN_D5, INPUT_PULLUP);
    pinMode(BTN_D6, INPUT_PULLUP);
    pinMode(BTN_D7, INPUT_PULLUP);

    // wait for wifi to be ready
    while( !WiFi.ready() ){
        // wait
    }
}

void loop() {
    // check if connected to MQTT broker
    // only retry every 5 seconds, don't bash the broker
    if(!client.connected() && (millis() - lastRetry) > 5000) {
        // set last retry to now
        lastRetry = millis();
        // not connected, turn LED red
        RGB.color(255, 0, 0);
      
        // connect to MQTT broker
        if (client.connect("SparkCoreController")) {
            // connected, turn LED green
            RGB.color(0, 255, 0);
            // send notification about connection
            client.publish("SparkCoreController/Init", "Connected to broker.");
        }
    } else {
        client.loop();
      
        // check which buttons have been pressed
        buttonPressed(BTN_A0, "SparkCoreController/Command", "DOWN");
        buttonPressed(BTN_A1, "SparkCoreController/Command", "LEFT");
        buttonPressed(BTN_A2, "SparkCoreController/Command", "UP");
        buttonPressed(BTN_A3, "SparkCoreController/Command", "STOP");
        buttonPressed(BTN_A4, "SparkCoreController/Command", "RIGHT");
        buttonPressed(BTN_A5, "SparkCoreController/Command", "F9");
        buttonPressed(BTN_A6, "SparkCoreController/Command", "F8");
        buttonPressed(BTN_A7, "SparkCoreController/Command", "F7");
        buttonPressed(BTN_D0, "SparkCoreController/Command", "0");
        buttonPressed(BTN_D1, "SparkCoreController/Command", "F6");
        buttonPressed(BTN_D2, "SparkCoreController/Command", "F5");
        buttonPressed(BTN_D3, "SparkCoreController/Command", "0");
        buttonPressed(BTN_D4, "SparkCoreController/Command", "F4");
        buttonPressed(BTN_D5, "SparkCoreController/Command", "F3");
        buttonPressed(BTN_D6, "SparkCoreController/Command", "F2");
        buttonPressed(BTN_D7, "SparkCoreController/Command", "F1");
    }
}

void buttonPressed(int button, char topic[], char command[]) {
    // if button has been pressed
    if(digitalRead(button) == LOW) {
        // button pressed, turn LED blue
        RGB.color(0, 0, 255);
        // publish the command to the provided topic
        client.publish(topic, command);
        // wait a little
        delay(250);
        // turn the LED back to green
        RGB.color(0, 255, 0);
    }
}

 

Demo

 

Here's a short video with a brief explanation of the controller, followed by a demo:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Next Steps

 

I'll probably have this circuit made properly by designing a simple PCB for it. And using my 3D printer, I should be able to make a proper enclosure and buttons for it as well.

 

Any suggestions for improvements are welcome!

  • Sign in to reply
Parents
  • mcb1
    mcb1 over 11 years ago

    Nice use.

    I've been deciding what to put mine to as well, rather than simply waste them sitting around or doing something that somethign else could do.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago

    Nice use.

    I've been deciding what to put mine to as well, rather than simply waste them sitting around or doing something that somethign else could do.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fvan
    fvan over 11 years ago in reply to mcb1

    Only ordered one to play around with, until the cheaper Photons arrive image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to fvan

    Photons

    Don't they arrive just before the Klingons attack.?image

     

    Haven't heard about them, I'm missing out.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down